Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum RG1 1.8v regulator
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 231 replies
  • Subscribers 711 subscribers
  • Views 36482 views
  • Users 0 members are here
Related

RG1 1.8v regulator

e14 Contributor
e14 Contributor over 14 years ago

Ok, so in a different thread I threatened to remove RG1 and do some current measurements on it's output after seeing those thermal images that show it's not generating any heat...

 

Well, I did it tonight. Some photos here: https://picasaweb.google.com/selsinork/RPi18v

 

The jumper pins in the output let me either just put a jumper on and verify the Pi boots ok, or wire a multimeter in series to get some current readings.

 

The results were interesting to say the least. I had to go back and check I was reading the multimeter correctly, that it wasn't broken etc.

 

On initial power up I see a negative current for a second or so which then reverses to about 0.5mA (yes half a milliamp, that's not a typo) for a few seconds while we get the first sd-card accesses. Once we're booted and sitting at the login prompt the current reading fluctuates from around 0.001mA to maybe 0.04mA. 

 

I'm using the 40mA range on a decent Fluke multimeter, so I've no reason to doubt the results. There's obviously going to be some inaccuracy down at that level due to length of meter leads etc, but the result is fairly clear.  You'll understand why I was checking the meter was working and I was reading it correctly though image

 

 

So from there onto the next test, lets try completely disconnecting RG1 and see if the Pi boots while using the LAN9512 1.8v 'output'.  Yes it does! 

 

I think that's reasonably good indication that jamodio got it spot on, the lan9512 shouldn't be connected to the 1.8v plane and it's heat problems are going to be largely due to supplying current on it's 1.8v filter pin that it was never designed to do.

 

So anyone willing to pull RG1 off a Pi and verify my results ?

  • Sign in to reply
  • Cancel
Parents
  • electron2
    electron2 over 14 years ago

    As shown in Troy Mackay's post on Jul 28 it seems to me that we could mod our PI's to work more as the chips were designed.

     

    I think that this could make the PI more stable, from the looks of it.

     

    I am not a designer Just an old tech, but I think we need to find a way to FIX what we now know is an error in the board.

     

    So could someone do some practical testing to see if there is something that can be done to easly fix the current board, rather than wait for RPI foundation to fix it by waiting for a board redesign?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to electron2

    i will love to try out the hack Troy mackay has done also and then test again with that fix on the board, but i have looked into this and i most say it is very well done by Troy as i think it is to small for me todo and i done have an microscope as need for this.

     

    so yes if some one can findout where to make an cut to split the LAN9512 1v8 from the lod 1v8 then i will try this also.

     

     

    Tooms

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    The engineering process after initial release is about identifying existing shortcomings and evaluating alternative solutions for future releases, and doing this iteratively for each new version or model.  It is not about pointing fingers at engineers (which is completely irrelevant and unhelpful), and it is not about those engineers reacting defensively when problems are identified.

     

    Reacting defensively makes it hard to analyse technical problems because it personalizes them, and when the defensive reaction is as extreme as on the Foundation forums and leads to messengers being banned, the engineering process is completely stillborn.  We're free of the latter here, but please let's remain free of the former as well.

     

    PeteL wrote:

     

    I do take issue with your final comment - it has been a success so far - with some measure of "success failure" thrown in.

     

    Pi Model B is most definitely not an engineering success.  Engineering success is a fairly measureable quantity related to how much of the engineering involved was actually successful, ie. how much of the product works as expected.  (And "success failure" is not a term any engineer should ever utter.)

     

    If any other computing device had been found to have such a catalogue of compatibility problems when used with totally class-compliant USB devices, it is highly likely that it would have been recalled immediately and withdrawn from sales pending redesign.  The Pi is setting an example of USB incompatibility such as has not been seen since the first year of release of the USB spec and initial devices.

     

    These USB problems appear to be in part fallout from least-cost BCM2835 SoC design and its USB  driver, and in part a consequence of excessively restrictive power design, but the board is a unit and its USB functionality is an extremely important part of its operation.  That key functionality has major faults.  It is not an engineering success (the only kind that concerns us here), because it is failing to operate as expected, and there are countless examples of how it is failing spread across the planet and reported on both RPF and Element 14 forums.

     

    I'm going to assume that the objectively incontrovertible fact of widespread failures is accepted, because anything else would not be a professional engineering response given the evidence.  The big task then becomes to identify the reasons and find solutions, and that is why we are here, in my opinion.

     

    Unless we can get past acceptance of the problems though, there is little prospect of finding solutions.

     

    Regarding how the 1.8V design might affect LAN9512 operation, I have no evidence that they are related either, but I am just hoping that they are related in some way that we cannot currently see because otherwise it seems likely that the Pi's huge USB faults are with us to stay.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jamodio
    jamodio over 14 years ago in reply to e14 Contributor

    Pete anything you are able and wish to share will be very valuable, I can say that so far I've not seen anything being shared yet...

     

    I don't feel qualified to state if the mission of RPF has been or will be a success or not, my comment was referred to situations where people say "we tried hard," "we did our best."

     

    Nobody will deny to acknowledge and appreciate the efforts but what it counts at the end are results.

     

    At one time I had over 100 engineers working in my team and I never accepted that something that was accomplished by "doing their best" couldn't be done better and more efficiently, because as others said engineering is a cumulative process where we constantly learn and apply the new knowledge to do things better, and more efficient, and which will never be perfect.

     

    I'm not a fanboi or a detractor of the R-pi, I still consider that it was a great idea and something worth to create, I'm not angry and I'm still using the 2 boards I purchased and planning to still work on some projects with them, now would I recommend it to local schools?, the answer at this time is NO.

     

    BTW kudos to the UK and London for putting such a great 2012 Olympics.

     

    Regards

    Jorge

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to jamodio

    Everyone doing their best is assumed.  It has no bearing on whether a product works or not, except possibly if the testers are ineffective and hence undermine everyone else on a project.  If anyone else in an engineering team fails, it should be caught at test to within certain limits (not 100%).

     

    But more importantly and relevantly, that issue is not part of the engineering process.  That process at the core of our profession concerns the objects being engineered, not the people.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Here I've assumed that at least since Intel's fdiv bug, hardware

    guys have had the advantage over software guys because they

    use mostly formal verification techniques where we rely mostly

    on ad hoc testing.

    Don't get me wrong, formal verification has it's place and can help a lot. It also leads to two sometimes difficult problems

    1. a simple error early in the design or even in a symbol/footprint supplied by a third party gets propagated through the design resulting in something that may not function at all, or as in this case works but is suboptimal. As the verification passes everyone has a high sense of confidence it'll work.
    2. Over time it leads to a reliance of the verification technology and a de-skilling of the job - beancounters strike again.

    In short there's no substitute for knowledge and experience. Experience of making the stupid mistakes and fixing them usually helps a lot.

     

    If you're a software person, you're probably familiar with unit testing.  IME it suffers from variants of the same problems.

    1. The spec is wrong, unit test to the letter of the spec and the result is wrong, but the test passes.
    2. Often the person who writes the code also writes the unit test for it, if they have some misunderstanding of the requirement, the test will pass but the result is still wrong.

    The same observation that there's no substitute for knowledge and experience holds for software just as much as for hardware.

     

    A dodgy datasheet, or software spec, just means it's even harder to spot the error.

     

    Hardware people do ad-hoc testing too, the tools are different and we literally get our fingers burnt - with a soldering iron image

     

      As technology gets more complex, ambiguity has to be reduced

    so checking can be increased, just to keep reliability from getting worse.

    Agree, but as the complexity grows you're increasingly faced with a datasheet being 1000 pages instead of 50. It's trying to reduce ambiguity, but it's bringing up the needle in a haystack problem.

    Then there's always the problem where increasing complexity gives you 17 different ways to do something, none of them obviously better or worse.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    Since we're talking about testing now, and looking for ways to improve future versions of Pi, let's focus on that a bit since it's clear that testing needs to be revamped to a significant degree.  This observation stems from the fact that testing somehow managed to miss the dramatically widespread incompatibility with common class-compliant USB devices that users have encountered and reported, as well as not catching any USB event or data loss, nor the high operating temperature of some LAN9512 devices.

     

    It seems that USB testing fell short in several respects:

     

    • Sample size.  Even if devices had been chosen at random, with a sufficient sample size it should have become apparent that there is a large incompatibility problem and that data loss is common.
    • Breath of devices tested.  Within the range of devices that fall within Pi's intended application area, a representative selection of device types and most common brands would have raised confidence that Pi works correctly with normal class-compliant devices that use only the generic drivers for their class.  It is very clear that Pi does not.
    • Depth of functional testing.  This refers to performance, overhead and error rate characterisation.  USB supports various different types of data transfer, but the most common and important types are lossless, ie. these USB transfers are meant to be 100% reliable.  Users have found that USB data loss from mouse and keyboard are common, but this is hard for users to quantify.  Given the importance of these HID devices, the error rate should have been characterised at testing time.
    • Physical tests.  Although only laterally related to USB testing, the wide variation in LAN9512 operating temperatures was not caught during Pi testing.  This suggests that either the test sample size was not large enough to reveal the problem or that it wasn't conceived that temperature measurement should be added to the set of tests that were performed.

     

    Everything is a trade-off, and perfection can never be reached through testing.  However, basic correct operation is non-negotiable, so enough testing needs to be performed to guarantee that each of these categories are covered to a satisfactory degree.  That is the only way to have measureable confidence of engineering success upon product release.

     

    Assuming that the premise is agreed, we then have to come up with a way to achieve this within cost and time constraints.  It has to be agreed first though.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 14 years ago in reply to e14 Contributor

    selsinork wrote:

     

    If you're a software person, you're probably familiar with unit testing.  IME it suffers from variants of the same problems.

    1. The spec is wrong, unit test to the letter of the spec and the result is wrong, but the test passes.
    2. Often the person who writes the code also writes the unit test for it, if they have some misunderstanding of the requirement, the test will pass but the result is still wrong.

    Expanding on (2), IMO you should always have different people designing and testing.  A good designer wants to make something work, a good tester wants to break it.  Getting both mind-sets in one person is a rarity, and inevitably leads to a conflict of interest.  Also, humans have difficulty perceiving what's really there versus what they want to see -- you should have someone else proofread your writing, and review your designs.

    selsinork wrote:

     

    Agree, but as the complexity grows you're increasingly faced with a datasheet being 1000 pages instead of 50. It's trying to reduce ambiguity, but it's bringing up the needle in a haystack problem.

    There are good and bad tech reference manuals out there.  It all depends on whether the vendor sees a manual as (1) a way to get more design wins and require less tech support, or (2) an painful burden to be dispatched as cheaply as possible.  A 1000-page TRM isn't a problem if it's well-organized -- I can just print the chapters I need for my particular application.  Many SoCs have all sorts of functions that I don't need, so I can just ignore them provided that the SoC is well designed and there aren't unexpected interactions.  OTOH, some 3000-page TRMs are that way because the writer copied and pasted identical functions and then made small changes to each copy instead of thinking out clearly what would be most helpful to the designer and making one copy with a table of individual differences.

     

    When a manufacturer is dodgy about documentation, it makes me wonder how well their products are designed, since a well-designed product generally starts with a well-written specification, which then provides the basis for a well-written TRM which doesn't cost much to complete.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to johnbeetem

    John Beetem wrote:

     

    When a manufacturer is dodgy about documentation, it makes me wonder how well their products are designed, since a well-designed product generally starts with a well-written specification, which then provides the basis for a well-written TRM which doesn't cost much to complete.

     

    A TRM is written as much for the manufacturer's own staff as for the external audience.  If a company can't be bothered to describe to its own staff how its product works, it doesn't inspire any confidence that its staff actually knows how it works, so you can expect support and the company's support products to be poor or non-existent.

     

    Orthogonal to the above, the days of monolithic TRMs or other large specification documents should have disappeared long ago.  Scalability refers not only to systems but to documentation as well.  Any non-trivial document needs to be hierarchical, distributed, and revisioned at each level of hierarchy, or it has no hope of being maintained to track the thing it describes.  Unfortunately today's prefered format for technical specs favours monolithic documentation.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 14 years ago in reply to morgaine

    Even if the delivery is "monolithic", internally inside the company the separation should take place.


    With "monolithic delivery" I mean: "A single datasheet that describes the whole chip".

     

    With separation I mean that the different chapters are maintained and written separately.

     

    Care must be applied to ensure that when a module is functionally upgraded, the datasheets for the previous versions of that module don't get more complicated.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 14 years ago in reply to rew

    Having now read the last few pages of this thread....


    The LAN chip is not designed to deliver power on the 1.8V. To stick to the specs the two signals need to be decoupled. i.e. a PCB redesign.

     

    In practise the draw on the 1.8V is about 100mA. This means 3.3V-1.8V * 100mA = 150mW of power moves from the LAN chip to the regulator.

     

    In practise, on the total power-draw of almost a Watt, the lan chip will be able to handle the 1/6th of a watt extra power. Maybe not over the full temperature range, so stuffing the 'pi into a mostly-closed enclosure may lead to unneccessary problems.

     

    No recall of existing 'pi boards needs to be done. As said: The lan chip can handle it in practise, it is a question of conforming to the specifications, and being more robust.

     


    If you are comfortable with using chips outside the official specifications, you can save a bit of cost if you leave off RG1. As it seems to work with RG1 removed, or with RG1 there is little current flowing from it. The lan chip seems to be able to cope.

     

    Some people are expressing views that paralleled regulators will have one delivering ALL the current, and the other one none. This is not always the case, This would be the case if they are both ideal voltage sources (with an ideal diode in series). However in practise, both regulators would have a measureable output impedance. So if regulator 1 delivers 1.85V with an impedance of 1 ohm, and the other delivers 1.80V with an impedance of 0.1ohm, the first 50mA will be mostly delivered by the first regulator, but increasing the current draw to 100mA, the second regulator will provide about 50mA of that.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to rew

    Roger Wolff wrote:

     

    Some people are expressing views that paralleled regulators will have one delivering ALL the current, and the other one none. This is not always the case, This would be the case if they are both ideal voltage sources (with an ideal diode in series). However in practise, both regulators would have a measureable output impedance. So if regulator 1 delivers 1.85V with an impedance of 1 ohm, and the other delivers 1.80V with an impedance of 0.1ohm, the first 50mA will be mostly delivered by the first regulator, but increasing the current draw to 100mA, the second regulator will provide about 50mA of that.

    The thing is, that isn't how regulators work, they aren't a voltage source with a resistive output.

     

    Regulators, including the two linear regulators we're dealing with here pretty much always consist of a voltage reference with a feedback circuit controlling a variable resistance between the input power pin and the output power pin provided by either a FET or a bipolar transistor. If the voltage on the output pin is above the reference voltage by more than a tiny amount then the feedback circuit will shut off the output transistor and nearly all the power will be provided by the device with the higher reference voltage. Where it gets funny is when the two reference voltages are very close, both regulators provide part of the power and you can get into oscillations and all sorts of fun and games depending on the impedances around the circuit.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to rew

    Roger Wolff wrote:

     

    Some people are expressing views that paralleled regulators will have one delivering ALL the current, and the other one none. This is not always the case, This would be the case if they are both ideal voltage sources (with an ideal diode in series). However in practise, both regulators would have a measureable output impedance. So if regulator 1 delivers 1.85V with an impedance of 1 ohm, and the other delivers 1.80V with an impedance of 0.1ohm, the first 50mA will be mostly delivered by the first regulator, but increasing the current draw to 100mA, the second regulator will provide about 50mA of that.

    The thing is, that isn't how regulators work, they aren't a voltage source with a resistive output.

     

    Regulators, including the two linear regulators we're dealing with here pretty much always consist of a voltage reference with a feedback circuit controlling a variable resistance between the input power pin and the output power pin provided by either a FET or a bipolar transistor. If the voltage on the output pin is above the reference voltage by more than a tiny amount then the feedback circuit will shut off the output transistor and nearly all the power will be provided by the device with the higher reference voltage. Where it gets funny is when the two reference voltages are very close, both regulators provide part of the power and you can get into oscillations and all sorts of fun and games depending on the impedances around the circuit.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • rew
    rew over 14 years ago in reply to e14 Contributor

    Andrew Warbrick wrote:

    Regulators, including the two linear regulators we're dealing with here pretty much always consist of a voltage reference with a feedback circuit controlling a variable resistance between the input power pin and the output power pin provided by either a FET or a bipolar transistor. If the voltage on the output pin is above the reference voltage by more than a tiny amount then the feedback circuit will shut off the output transistor and nearly all the power will be provided by the device with the higher reference voltage. Where it gets funny is when the two reference voltages are very close, both regulators provide part of the power and you can get into oscillations and all sorts of fun and games depending on the impedances around the circuit.

    Mostly correct.

     

    But if that "tiny amount" is very very small, or equivalently the gain in that feedback circuit is very large, then even with just ONE regulator, the result will be oscilations. So that's why 1) They don't design for inifinite gain in that stage 2) they specify that (usually 100nF) capacitor near the regulator to stabilize the output.

     

    So, as the voltage on the output drops due to increasing load, the difference between the reference voltage and the feedback voltage increases and the output transistor is driven more and more (to a lower resistance as you say).

     

    The end result is that you can measure a real output resistance on regulators.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to rew

    You're absolutely right, but the point I was making is that actually pretty small differences in reference voltage result in one regulator of two connected in parallel providing nearly all the current. Yes, the gain in the feedback circuit isn't infinite but it's high enough that you don't need much difference in the outputs for one regulator to be doing nearly all the work. I won't pick nits over the semantics of resistance versus output impedance, you're right, the output does look like a resistor for small changes in load.