Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum RG1 1.8v regulator
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 231 replies
  • Subscribers 711 subscribers
  • Views 36565 views
  • Users 0 members are here
Related

RG1 1.8v regulator

e14 Contributor
e14 Contributor over 14 years ago

Ok, so in a different thread I threatened to remove RG1 and do some current measurements on it's output after seeing those thermal images that show it's not generating any heat...

 

Well, I did it tonight. Some photos here: https://picasaweb.google.com/selsinork/RPi18v

 

The jumper pins in the output let me either just put a jumper on and verify the Pi boots ok, or wire a multimeter in series to get some current readings.

 

The results were interesting to say the least. I had to go back and check I was reading the multimeter correctly, that it wasn't broken etc.

 

On initial power up I see a negative current for a second or so which then reverses to about 0.5mA (yes half a milliamp, that's not a typo) for a few seconds while we get the first sd-card accesses. Once we're booted and sitting at the login prompt the current reading fluctuates from around 0.001mA to maybe 0.04mA. 

 

I'm using the 40mA range on a decent Fluke multimeter, so I've no reason to doubt the results. There's obviously going to be some inaccuracy down at that level due to length of meter leads etc, but the result is fairly clear.  You'll understand why I was checking the meter was working and I was reading it correctly though image

 

 

So from there onto the next test, lets try completely disconnecting RG1 and see if the Pi boots while using the LAN9512 1.8v 'output'.  Yes it does! 

 

I think that's reasonably good indication that jamodio got it spot on, the lan9512 shouldn't be connected to the 1.8v plane and it's heat problems are going to be largely due to supplying current on it's 1.8v filter pin that it was never designed to do.

 

So anyone willing to pull RG1 off a Pi and verify my results ?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Hi

     

    I have now done the Troy Mackay fix to my test board, it was not easy to cut that small traces and then solder the wires to the board but with an microscope and time it was done and seems to work.

     

    I have also removed the RG1 and RG2, but i was not lucky with the desoldering of the RG2 as i have damage it and it is no longer working so i am using an replacement LF33CV that i have.

     

     

    So guys what testes do you like me to do and what IR images, for now i am thinking some things like this.

     

    Test 1

    Work: idle

    board: as unmodified (execpt i am using the LF33CV as RG2)

     

    Test 2

    Work: CPU is calc Pi, taking images from webcam, copy files via network

    board: as unmodified (execpt i am using the LF33CV as RG2)

     

    Test 3

    Work: Idle

    board: replace RG1 and RG2 with switchmode, disconnect the LAN9512 1V8 rail from RG1

     

    Test 4

    Work: CPU is calc Pi, taking images from webcam, copy files via network
    board: replace RG1 and RG2 with switchmode, disconnect the LAN9512 1V8 rail from RG1

     

    This is the tests i have planned for now, but i will like to hear if your guys like some other ones or changes.
    For the tests i have done see the post 40 in this thread http://www.element14.com/community/message/57800#57800

     


    image

     

     

    Tooms

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    That's very impressive work Tooms, well done.  Your list of tests sounds good.

     

    I wish we had some way of measuring USB data loss directly, such as numbered data injection which we could monitor from the Pi host end.  Networking utilities may help as long as we avoid self-correcting protocols like TCP, but they may exercise only bulk transfers and I'm not sure that observed networking faults will correlate with lost HID events.

     

    Now that RPF has acknowledged the USB data loss and found a likely cause for it, perhaps someone who isn't banned can recommend that they add logging of those dropped split transactions when they occur.  Logging may not catch all faults like direct monitoring for lost data would, but it could certainly help.  Maybe they do that already in their latest driver?

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    That's very impressive work Tooms, well done.  Your list of tests sounds good.

     

    I wish we had some way of measuring USB data loss directly, such as numbered data injection which we could monitor from the Pi host end.  Networking utilities may help as long as we avoid self-correcting protocols like TCP, but they may exercise only bulk transfers and I'm not sure that observed networking faults will correlate with lost HID events.

     

    Now that RPF has acknowledged the USB data loss and found a likely cause for it, perhaps someone who isn't banned can recommend that they add logging of those dropped split transactions when they occur.  Logging may not catch all faults like direct monitoring for lost data would, but it could certainly help.  Maybe they do that already in their latest driver?

     

    Morgaine.