Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum RG1 1.8v regulator
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 231 replies
  • Subscribers 711 subscribers
  • Views 36549 views
  • Users 0 members are here
Related

RG1 1.8v regulator

e14 Contributor
e14 Contributor over 14 years ago

Ok, so in a different thread I threatened to remove RG1 and do some current measurements on it's output after seeing those thermal images that show it's not generating any heat...

 

Well, I did it tonight. Some photos here: https://picasaweb.google.com/selsinork/RPi18v

 

The jumper pins in the output let me either just put a jumper on and verify the Pi boots ok, or wire a multimeter in series to get some current readings.

 

The results were interesting to say the least. I had to go back and check I was reading the multimeter correctly, that it wasn't broken etc.

 

On initial power up I see a negative current for a second or so which then reverses to about 0.5mA (yes half a milliamp, that's not a typo) for a few seconds while we get the first sd-card accesses. Once we're booted and sitting at the login prompt the current reading fluctuates from around 0.001mA to maybe 0.04mA. 

 

I'm using the 40mA range on a decent Fluke multimeter, so I've no reason to doubt the results. There's obviously going to be some inaccuracy down at that level due to length of meter leads etc, but the result is fairly clear.  You'll understand why I was checking the meter was working and I was reading it correctly though image

 

 

So from there onto the next test, lets try completely disconnecting RG1 and see if the Pi boots while using the LAN9512 1.8v 'output'.  Yes it does! 

 

I think that's reasonably good indication that jamodio got it spot on, the lan9512 shouldn't be connected to the 1.8v plane and it's heat problems are going to be largely due to supplying current on it's 1.8v filter pin that it was never designed to do.

 

So anyone willing to pull RG1 off a Pi and verify my results ?

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    selsinork wrote:

     

    Hope this all makes sense.

    Possibly, but everything you say is based on assumption with no actual reference to defined behaviour.

     

    There was a very simple reason for asking that question. If the behaviour is not defined you have no basis to rely on it, you simply don't know if it'll work or not. Saying "It's simply the way that the average linear regulator works" is not an acceptable substitute for actual defined behaviour.  Doesn't anyone question why the behaviour isn't defined ?

     

    The only reference appears to be Figure 31 and that suggests you need 300mV to (reliably?) turn the regulator off. So how does the SoC, RAM etc react 2.1v on it's 1.8v input ?

    On the other hand, if it's only a couple of mV then you'll have lots of fun with oscillations as the voltage measurably changes by a few mV depending on how you load the cpu/gpu.

     

    Without a definition of the behaviour it's only ever going to be a bad engineering decision to use it, rely on it, or expect it to work.

     

    Also we don't know what the 1.8v regulator inside the lan9512 is or what it's defined behaviour is, it could be a 1117 clone, or could be something vastly different in design, we simply don't know. We do have an answer from SMSC saying it's not designed to be used this way.

     

    Very valid points, except perhaps the "fig 31...suggests you need 300mV to (reliably/) turn the regulator off" part. "Yes... and no" is probably the best answer I can give to that.

     

    Who's to say that the nice folks at On Semi ever actually built and tested the circuit, rather than just lifting it from a cookbook and specifying a nice big differential voltage to allow for the vagaries of production tolerances, changes due to ambients and a lump more for safety? And on an unrelated note,  why would a "proper" engineer specify 50R instead of a more sensible (from an inventory POV) 47R? I see this all the time on application notes...

     

    The fact that On specify applications with a resistor in the ground lead demonstrate that (like any other vanilla linear regulator) this one does not rely on a mechanism for dumping current to ground, therefore any overvoltage applied to the output above setpoint will be resisted by the feedback circuitry in the only way it knows how, i.e. by increasing the resistance of the series pass element. How a pair of regulators fight over current supply duties in this real world case will be more complicated (and will require real world analysis), but I'd bet a night's beer money given the output voltage regulation spec that it would take rather less than 300mV output overvoltage to switch one off. The actual setpoint may vary a tad due to the reasons above, but once it's exceeded by even a small amount, the regulator stops working, because there will be a high gain under the feedback loop. It all depends very much on the characteristics of the other reg too, which we're ignoring... image

     

    The bottom line is of course that it's not supposed to work like this and the usual "we'll work around it in software" hacks won't help. I really can't believe that they're still churning these things out at full pelt...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 14 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    coder27 wrote:

     

    ...Amazingly, he hasn't been banned, belittled, or had the thread locked.

    So maybe the RPF is actually considering that.

     

    Don't get your hopes up too high.  While it would be nice to think that RPF have finally woken up to reality and will start being open and honest, precedent doesn't support this possibility very strongly.  Rather more likely is that convincing spin is proving more difficult to manufacture as the evidence accumulates.

    Maybe manufacturing spin is taking too much time and effort, so they decided to outsource it to China.  But it'll take a few months to get the process working. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to johnbeetem

    John Beetem wrote:

     

    Maybe manufacturing spin is taking too much time and effort, so they decided to outsource it to China.  image

     

    Gosh no, we only outsource the productive parts of manufacturing that create jobs, grow native production capability, and increase knowledge of technology among the population.

     

    None of that stuff is needed in the West where the biggest growth industry is litigation, where the USPTO's primary role is chilling innovation, where the media companies treat their audience as criminals, where states block science in education, and where governments' only interest in technology to keep their populations in observational prison.

     

    Spin is a key competency right here at home, and a necessary process in making a dysfunctional board brilliant.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Very valid points, except perhaps the "fig 31...suggests you need 300mV to (reliably/) turn the regulator off" part. "Yes... and no" is probably the best answer I can give to that.

    Well as it's not defined elsewhere, yes and no is about the best answer I'd expect image  Taking a random sampling of datasheets from other manufacturers of equivalent parts, some include that circuit, some don't. I didn't find another one that mentioned the 300mV or defined this behaviour at all.  What is clear is that there must be an original manufacturer and they're all mostly cut&pasting the datasheet from one source. I couldn't easily work out who the original designer was so it's hard to pick any one of the datasheets as being authoritative.

     

    And on an unrelated note,  why would a "proper" engineer specify 50R instead of a more sensible (from an inventory POV) 47R? I see this all the time on application notes...

    I'd probably have picked 51R, but as 50OHM, 0.1W, 1% 50OHM, 0.1W, 1% and all sorts of strange values like 49.9R, 50.5R, 51.1R are available at the same cost as the 'standard' values. I agree though, it's a pain when somthing specifies some odd fractional value that you have to order up specially.

     

    but I'd bet a night's beer money given the output voltage regulation spec that it would take rather less than 300mV output overvoltage to switch one off.

    So would I.. The point was simply that we don't know and as there's no reference we're simply not in a position to judge whether this is suitable behaviour or not. The engineer side of me does things like "specifying a nice big differential voltage to allow for the vagaries of production tolerances, changes due to ambients and a lump more for safety?" as I suspect most of us do, unfortunately that's exactly what brings us to the 'undefined behaviour' vs real world application question.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 14 years ago in reply to e14 Contributor

    The designer of this battery changeover ciruit (ON Semi's fig 31) was intending to set a difference so that one regulator would do all the work if the ac power was present. The 300mV (which is obtained by assuming the nominal 6mA quiescent current flowing through the 50R resistor) gives a margin over the +/-100mV tolerance of the regulators' output voltages. It's not  a good design because the minimum quiescent current is not specified so the intended 300mV might easily be only 200mV and then a worst case pair of regulators would be sharing the load.

     

    What we do know is that the 1117 regulator can be used in pairs but since the SMSC chip makers explicitly say that their part should not the RPi circuit is still uncharted territory (and obviously just a mistake).

     

    I can't believe that they don't just put it right.

     

    Michael Kellett

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to michaelkellett

    which is obtained by assuming

    See, that's the bit I don't like image

     

    I can't believe that they don't just put it right.

    Hopefully they will, but for now all we have is another assumption that theres no quick and easy way to do that.  If there's a pcb respin needed then it makes sense to take some time and fix as many problems as can be identified in one go - alignment of the RJ45 would be quite high on my personal list. 

    There's likely to be some number of bare pcb's in the pipeline, so even an immediate fix could take some time to filter through to customers. We have no details of any of that, nor would I expect to ever see it, so we're left with more of those pesky assumptions image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Hi selsinork and thanks for the reply. You're absolutely right  - no amount of assuming on our part is going to move any copper! Putting on my optimistic to the point of naïveté hat for a moment then if a board revision does come it will take some time to proto and test (properly!) - way longer than the factories' stock of the current boards (which will be pretty skinny). Raspberry Towers may be wary of moving that connector (or doing anything else that isn't absolutely imperative) given the amount of fubar already. Who knows with that lot? They certainly make assuming stuff difficult. I do detect a little more humility on the forums over there lately though. Sometimes. With certain staff. When no-one's looking. Most of the fanbois are just as obnoxious as ever though.

     

    I wonder whether the rollout (if it does happen) will be accompanied by fanfares, or whether it will be a subdued affair...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    selsinork wrote:

     

    If there's a pcb respin needed then it makes sense to take some time and fix as many problems as can be identified in one go - alignment of the RJ45 would be quite high on my personal list.

     

    I'm just incredulous that with so many expert hardware engineers on the various forums, the Foundation's people are so full of themselves that they refuse to do the redesign in open consultation, despite the fact that it is the community that has found all these faults.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    selsinork wrote:

     

    If there's a pcb respin needed then it makes sense to take some time and fix as many problems as can be identified in one go - alignment of the RJ45 would be quite high on my personal list.

     

    You would have hoped that Pete had a bunch of fixes pretty much

    ready to go by now, and that this one would just get added to the list

    without much further delay.

     

    But I don't get the impression that Pete has been very active on RPi

    issues lately, based on him being absent from this forum (not even

    monitoring the hardware flaws and fixups thread that he started)

    and based on his recent comment that this issue was just one on

    his list of board issues to look at.  It sounds to me like the returned

    boards have just been piling up unopened in his office.

     

    Since we aren't getting much help from Pete in understanding how

    the regulators work, is anyone able to attach a scope and measure

    any oscillations?

     

    In post #74, Pete wrote:

    "Of the returns I have for analysis, I have still have not found a real ‘steamer’. These could be in part due to poor underfill or even a short/defect elsewhere on top of what we are asking the chip to do."

     

    I find this interesting in regard to element14's limited warranty, which says:

    "Newark element14 warrants that the Raspberry pi will be free from defects in material or workmanship for a period of 12 months from the date of Newark element14's shipment of the Raspberry pi to you, the Customer."

    http://www.farnell.com/datasheets/1627216.pdf

     

    Notice that "design defects" are not explicitly mentioned.  So I wonder if

    "poor underfill" would be a covered defect in workmanship, but an error in

    the schematics would be an uncovered design defect?  I presume if the

    temperatures are hot enough to be considered a safety issue, that it would

    be covered by law in most jurisdictions regardless of whether it was a

    considered to be a design issue or not.

     

    Hopefully someone from element14 will speak up soon as to how the

    warranty applies to this design error.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    coder27 wrote:

     

    But I don't get the impression that Pete has been very active on RPi

    issues lately, based on him being absent from this forum (not even

    monitoring the hardware flaws and fixups thread that he started)

    and based on his recent comment that this issue was just one on

    his list of board issues to look at.  It sounds to me like the returned

    boards have just been piling up unopened in his office.

     

    Since we aren't getting much help from Pete in understanding how

    the regulators work, is anyone able to attach a scope and measure

    any oscillations?

     

    It's rather likely that we've been guilty of wishful thinking regarding Pete's visits to this forum, sometimes seeing it as vindicating our view that (Foundation minus Pete) is on drugs whereas Pete as their engineer retains his professional standards and distances himself from the shenanigans of the rest of the Foundation.  Unfortunately, that's almost certainly naive in the extreme.  He knows that his toast is buttered on the RPF side, and that being seen as a small hero here does not pay the rent.  His absence and silence probably reflects reality rather than our wishful thinking:  we misjudged his desire to do the right thing for the community.

     

    We still don't have the old gerbers despite countless requests and no rational reason for them to be withheld, we still have no information on whether the first revision is intended to be minimal or extensive, and we still don't  have any engineering feedback about Model A operation despite the continued false advertising of "$25 computer" (it would be valuable to quantify USB faults in the absence of the LAN9512).  If Pete wanted, he could be pushing the Foundation towards being more open about these things, but this has not happened.

     

    While wishful thinking makes all us feel better, the facts are not encouraging:  Pete spent at most a few hours on a number of occasions gathering input from the Element 14 forum, but the information flow has been completely one-way.  I think it's time to put the rose-tinted spectacles aside.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>