Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum Incompatible Self-Powered Hub
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 31 replies
  • Subscribers 709 subscribers
  • Views 8286 views
  • Users 0 members are here
  • raspberry_pi
Related

Incompatible Self-Powered Hub

morgaine
morgaine over 14 years ago

[This thread was split off from an earlier general one about Powered Hubs and has been given a more appropriate subject line.  Note that replies prefix "Re:" to the old subject line.]

 

 

The Pi's very poor power design results in some perfectly good self-powered hubs being incompatible with it.  For example, the cheap little 7-port self-powered Dynamode USB-H70-1A2.0 hub that Farnell advertises as a Pi accessory:

 

  • http://uk.farnell.com/dynamode/usb-h70-1a2-0/hub-usb-2-0-7-port-with-ac-adaptor/dp/2115058

 

is not actually Pi-compatible at all, because in addition to powering its 7 host ports, it also powers the Pi board through its A-B upstream lead yet is incapable of supplying enough power to do that successfully (the Pi's Vcc drops to well below 4V).  As a result, when the micro-USB is powered down but the hub is powered up and connected, the Pi ends up rebooting continuously every couple of seconds, potentially leading to destroyed HDMI displays among other worries.

 

So, buying a self-powered hub is not necessarily the end to your Pi power problems.

 

Really the Pi's power design needs to be nuked from orbit and redesigned from scratch.  It's just plain bad in numerous ways.

 

Morgaine.

  • Sign in to reply
  • Cancel
Parents
  • dharr19
    dharr19 over 14 years ago

    Hi Morgaine,

     

    Thanks and may I say, England ROCKS!!! image  I loved the Olympic openings.  This is the third time the world has been blessed to have England preside over this event.

     

    I'm guessing that although a powered hub will not end my Pi power problems it might be beneficial to have one if I want to power additional peripherals like wifi and bluetooth adapters.

     

    Any peripheral recommendations such chargers, self-powered hubs, or wifi and bluetoothadapters are appreciated.

     

    Thanks

    David

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to dharr19

    actually all the peripherals that do work (and those that don't) are listed here

    http://elinux.org/RPi_VerifiedPeripherals

     

    As for chargers, Nokia's AC-10E seems to be favorable according to some thread I can't find now, 5V and 1200mA. Beware of Chinese fakes though, especially on ebay and amazon.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to dharr19

    actually all the peripherals that do work (and those that don't) are listed here

    http://elinux.org/RPi_VerifiedPeripherals

     

    As for chargers, Nokia's AC-10E seems to be favorable according to some thread I can't find now, 5V and 1200mA. Beware of Chinese fakes though, especially on ebay and amazon.