Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Still unable to Boot my RPi help please
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 21 replies
  • Subscribers 709 subscribers
  • Views 2212 views
  • Users 0 members are here
  • raspberry_pi
Related

Still unable to Boot my RPi help please

quitiri
quitiri over 14 years ago

Hi All

 

I have tried to boot my RPi but without much luck.

I used the win32diskimager to add an o/s to a 4 gig SD card I have tried both the archlinuxarm-13-06-2012 O/S and the 2012-07-15-wheezy-raspbian O/S.

these both gave the same result when i turned on the RPi with the SD card installed i get no video output either on the composite video output or the HDMI output.

I am using a HTC phone PSU charger rated at 5V 1 amp output.

Has anyone got any ideas.

 

Regards Richard

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    This may seem like a stupid question, forgive me for that, but sometimes it's the simplest things that nobody bothers to ask..

     

    The arch and raspbian downloads are zipped. Did you unzip them before writing them to your sd card ?

     

    An easy way to tell is if you put the sd card back into your pc and see if you get a small drive, probably only 100Mb or so, with files like kernel.img, loader.bin, bootcode.bin & start.elf. If you see those then the image on the card should be ok.

     

    With up to date images like the ones you're using, sd-card compatibility is much improved and being on the good/bad lists, or not, is less likely to be an issue.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    Given the target audience of the Pi which is intentionally non-technical, it occurs to me that it would be very useful if the Foundation or the community produced a little program for Windows, Mac and something that runs on all Linux flavours, which just looks at the SD card device after it has been written, ejected, and reinserted and checks that it has been written appropriately for booting as a Pi card.

     

    It would catch the problem that your post suggests, and could be made to catch incomplete writes / premature ejects, and various other ills.  I have little doubt that writing the image is a mystery to many people in what it does (ie. creates two or more partitions), and so inevitably is being messed up by a few.  This would help.

     

    Perhaps more thorough documentation on this initial step of the Pi startup process would help too, but not always.  Unfortunately part of the target audience would probably go totally blank when faced with a highly detailed, point-by-point explanation of image writing from first principles, instead of learning from it.  The post-check utility I suggest would plug that gap.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    Given the target audience of the Pi which is intentionally non-technical, it occurs to me that it would be very useful if the Foundation or the community produced a little program for Windows, Mac and something that runs on all Linux flavours, which just looks at the SD card device after it has been written, ejected, and reinserted and checks that it has been written appropriately for booting as a Pi card.

     

    It would catch the problem that your post suggests, and could be made to catch incomplete writes / premature ejects, and various other ills.  I have little doubt that writing the image is a mystery to many people in what it does (ie. creates two or more partitions), and so inevitably is being messed up by a few.  This would help.

     

    Perhaps more thorough documentation on this initial step of the Pi startup process would help too, but not always.  Unfortunately part of the target audience would probably go totally blank when faced with a highly detailed, point-by-point explanation of image writing from first principles, instead of learning from it.  The post-check utility I suggest would plug that gap.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    Given the target audience of the Pi which is intentionally non-technical,

    As a 'techie' I often find it hard to help non-technical newcomers. Not because I don't want to, but because I always have some inherent assumption that the most basic of things can be taken for granted and don't need to be asked. Often being greeted by that blank faced look.

    Given the target audience and the various issues, limitations, incompatibilities and whatnot that we already know about I can see a lot of frustration from both people in need of help and those trying to offer help.  On my part I know that when that frustration builds all I want to do is elbow them out the way and fix it for them, but as you say nobody learns anything that way..

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    +1

     

    So true.  Coming from the engineering education side, "I can fix this for you, but you would learn nothing" is a really big source of concern.  No matter how strong the desire, how to help people learn is not even close to being a science yet.  Not remotely so, for all the papers published on the topic.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 14 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    No matter how strong the desire, how to help people learn is not even close to being a science yet.  Not remotely so, for all the papers published on the topic.

    As a former academic, here is my experience:

     

    1:  They have to want to learn.  A spark has to be there.

     

    2:  Sparks are easily extinguished.  Successful education is about helping sparks turn into passionate fire.

     

    EDIT:

     

    3:  The best engineers are like Kipling's Elephant Child.  They are full of Insatiable Curiosity, which means they ask ever so many questions.  So they get spanked for asking so many questions, but still they're filled with Insatiable Curiosity.  You can't spell Insatiable Curiosity without IC.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to johnbeetem

    John Beetem wrote:

     

    2:  Sparks are easily extinguished.

     

    That is so sad.