Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Cant save changes to config.txt. Help needed.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 706 subscribers
  • Views 2833 views
  • Users 0 members are here
  • raspberry_pi
Related

Cant save changes to config.txt. Help needed.

hoekeat
hoekeat over 13 years ago

I cant seems to save any changes to my SD card.

 

Plug in my (Wheezy) SD card to my Windows Vista / 7 pc, edit the file, save. Then reopen the file to confirm the changes is saved.

Eject the SD card. Reinsert the SD Card, open the config.txt again and the changes is gone.

 

What happened? what can i do to make changes to the card?

  • Sign in to reply
  • Cancel
Parents
  • johnbeetem
    johnbeetem over 13 years ago

    When you say "Eject the SD card", are you using the Windows command that ejects the card safely?  There's an icon at the bottom of the screen that appears when you plug in the SD card and you should ciick on it, select the option to stop using the SD card, and wait for Windows to say it's safe to remove the SD card.  Otherwise Windows (and Linux for that matter) may save updates in RAM and not write them to SD until it needs the RAM for something else or you explicitly tell the OS to eject the card.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • hoekeat
    hoekeat over 13 years ago in reply to johnbeetem

    i used the "safely remove hardware" option and waited until the message prompt me that it is ready to be removed.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • hoekeat
    hoekeat over 13 years ago in reply to johnbeetem

    i used the "safely remove hardware" option and waited until the message prompt me that it is ready to be removed.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • johnbeetem
    johnbeetem over 13 years ago in reply to hoekeat

    Hoe Keat Lim wrote:

     

    i used the "safely remove hardware" option and waited until the message prompt me that it is ready to be removed.

    It sounds like you're doing the right thing.  Try getting a directory listing using the DOS "dir" command in a Command Window.  Windows sometimes does inscrutable things to file extensions, so it may have stored your "config.txt" as "config.txt.doc" or something equally silly.  The "dir" command gives you a better idea of what's really in a directory.

     

    EDIT: do the "dir" command before and after you save config.txt using your editor to see if the editor is updating the SD card's directory.  It's conceivable that the editor doesn't like the permissions on config.txt, but isn't giving an error message.  Another thing to try is using "Save As" to save config.txt under a new name, and then rename it at the Command Window level.