Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum PiFace Relay  Motor Control Extra
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 19 replies
  • Subscribers 707 subscribers
  • Views 2926 views
  • Users 0 members are here
  • raspberry_pi
  • raspberry_pi_b_plus12vmotor
  • piface
Related

PiFace Relay  Motor Control Extra

e14 Contributor
e14 Contributor over 11 years ago

I want use this board and PiFace Relay+ to drive a 12 V DC motor, is that possible ?

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to balearicdynamics

    I appreciate if you are willing to share the design with me.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to mcb1

    In fact, I find a cheaper circuit board which is L298N, however , I cannot find it in Singapore.As I am using this for my final year project, if I buy from ebay , I need to pay S$30+ shipping fees if I want get it within one week.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago

    If all you need is ON/OFF then any PI compatable relay board will work and you can often have uptp 24V and 5A (PiFace Digital for instance)

    If you need to vary the speed then you need to be able to PWM the supply to the motor or use the PiFace Motor but this also requires the new PiFace Digital card, this is not a bad solution if you want to play with other things. This new digital card has smaller relays on it, hense the limit of 1A rather than 5 on the regular / older card

     

    there are many ways to get this job done as the folks above have already shown / explained

     

    To simply answer your question. Yes it is possible and with this board

    image

    you will have on off control with the relay and this will handle the motor you mention

    with this board

    imagethat plugs into the above board you get the H Bridge control

    and this one

    image

    Gives you more relays instead

     

    Choice depends on what you want to do with the motor... read all the above replies

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to Robert Peter Oakes

    basically the PI Face digital uses a SPI to 16Bit expander chip on the main board, 4 bits are to drive the 4 relays included, the other pins are for the expander (Relay or HBridge) and then a few left for general GPIO stuff

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to Robert Peter Oakes

    Peter, am I wrong or there unused GPIO pins on the pi ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to Robert Peter Oakes

    yeah, I understand what are the function of those 3 parts. However, my concern here is I need 12 v to operate my motor, but where can I plugged in the 12 v battery as rasp only give 5v.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to balearicdynamics

    There are plenty of unused pins on th ePI when you use the PiFace Digital as this device is using a SPI to Parallel GPIO chip (MCP23S17) http://ww1.microchip.com/downloads/en/DeviceDoc/21952b.pdf

     

    so pretty much all the PIFace boards only use the SPI connections leaving all the other GPIO unused

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to Robert Peter Oakes

    Great Peter, it was what I though. So with only one PiFace digital board, as a matter of fact Weng has a bunch of digital pins to do what he needs while for the motor control can be used the standard Pi pins that are free. I have used the PWM anywhere library for the raspberry PI and it works fine as far as I know making tests with micro servos. Connecting them on the GPIO preferred pins.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to balearicdynamics

    That would be correct image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<