Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Will 5,1V    I   850mA smartphone charger work well to power the Pi?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 707 subscribers
  • Views 535 views
  • Users 0 members are here
Related

Will 5,1V    I   850mA smartphone charger work well to power the Pi?

e14 Contributor
e14 Contributor over 14 years ago

Just ordered the Pi when I found out that it doesn't come with an charger. However, I got a pretty new Motorola Smartphone charger which outputs 5,1 volts at 850mA. Will this work with the pi or must the voltage be exactly 5,0?

 

*Think I posted this in the wrong forum, but I can't seem to move it to the Raspberry pi section.

  • Sign in to reply
  • Cancel
  • johnbeetem
    johnbeetem over 14 years ago

    5.1V is fine (sorry about the USA punctuation).  RasPi follows the USB 5V +/- 5% spec so anything from 4.75V to 5.25V complies.  However, because of voltage drops across the micro USB cable and polyfuse F3, it's better to have a bit more than 5.0V, so 5.1V is near-optimal.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to johnbeetem

    Ah, well okay, that's great. Thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnsocm
    johnsocm over 14 years ago

    Yes,

     

    Any cellphone charger or Wallwart adapter will work as long as it is close to 5 volts. You definitely do not want more than 5.5V or less than 4.5V.  The current does not matter as long as it is over 300mA.

     

    I have a ton of posts on the Rasperry Pi and how to get Quake III up and running on my blog at www.engineerdemos.blogspot.com.

     

     

    Thank you and enjoy,

     

     

    Chad Johnson