Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum What to do with a Gertboard?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 13 replies
  • Subscribers 709 subscribers
  • Views 1607 views
  • Users 0 members are here
Related

What to do with a Gertboard?

dharr19
dharr19 over 14 years ago

Hi,

 

If your a programmer but someone with no experience in electronics then would this board be usefull to you?

 

Cheers

David

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Why don't you download the user manaul and have a read. If you're a programmer the programming sections are probably too easy but the manual also tells a bit about the hardware and what it does. It will not replace an electronics course.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    Gert van Loo wrote:

     

    It will not replace an electronics course.

     

    Looking at the board and schematics, it occurs to me that the board could be used quite nicely as the basis of a simple electronics course and provide basic electronics instrumentation at the same time.

     

    For example, while school kids are not too likely to purchase a real oscilloscope, it's not a big stretch to obtain basic waveform display from a buffered A/D, which could greatly enhance an electronic kit's educational value, and then subsequently support further explorations into electronics.

     

    Given the size of the Pi community, it wouldn't surprise me at all to find people capitalizing on your work and taking it in this direction.  It seems to provide a missing link that Arduino doesn't quite fill through lacking a high-level component, which the Pi provides.  Waveform sampling on the Gertboard and display on the Pi seems a perfect combination.

     

    Anyone have a favourite "scope front-end" circuit to fit the 12x7 grid of holes? image

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    Gert van Loo wrote:

     

    It will not replace an electronics course.

     

    Looking at the board and schematics, it occurs to me that the board could be used quite nicely as the basis of a simple electronics course and provide basic electronics instrumentation at the same time.

     

    For example, while school kids are not too likely to purchase a real oscilloscope, it's not a big stretch to obtain basic waveform display from a buffered A/D, which could greatly enhance an electronic kit's educational value, and then subsequently support further explorations into electronics.

     

    Given the size of the Pi community, it wouldn't surprise me at all to find people capitalizing on your work and taking it in this direction.  It seems to provide a missing link that Arduino doesn't quite fill through lacking a high-level component, which the Pi provides.  Waveform sampling on the Gertboard and display on the Pi seems a perfect combination.

     

    Anyone have a favourite "scope front-end" circuit to fit the 12x7 grid of holes? image

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    while school kids are not too likely to purchase a real oscilloscope

    many moons ago when I was at school there were one or two basic scopes available for the science/technology classes. No doubt lots will have changed since then, but I'd be dismayed to learn that wasn't still the case.

    I do agree that few kids are likely to have one available at home though.

     

    Someone over on the other forums was writing a basic logic analyser in software, but I seem to remember he could only get it up to around 1Mhz sample rate. Not entirely useless, but quickly overwhelmed by even a simple mcu these days. I guess the point is to get them hooked though, so some carefully planned stuff that's within range could work.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    It reminds me of our related conversation in another thread about the role of Heathkit in our own educations.  We live in the "age of multicore" and today's systems employ multiple computers at all levels, so I'm pleased to see Gert's interface board having its own CPU and being designed very explicitly as just one half of a 2-processor system.

     

    In addition, I've long been advocating the horses-for-courses approach of using an embedded microcontroller for realtime interfacing, connected to a Unix-type system for non-realtime high level work.  Let them each do what they each do best.  That's what this provides, a way in to system engineering.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to morgaine

    In fact, it's such an "obvious" thing to do that I'm very surprised that none of the ARM board manufacturers has placed an applications processor for Linux AND a bare-metal ARM microcontroller on the same board for this purpose.  A low-end ARM microcontroller can add very little indeed to the overall BOM cost, a fraction of a dollar according to ARM marketing blurb.

     

    Hmmm, where did I put Olimex's email address ... image