Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Gertboard - The Element14 strikes back
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 71 replies
  • Subscribers 718 subscribers
  • Views 8448 views
  • Users 0 members are here
  • raspberry_pi
Related

Gertboard - The Element14 strikes back

e14 Contributor
e14 Contributor over 14 years ago

Oh dear. It seems that If I "Fluke PiStalker" want to obtain a Deathstar beating Gertboard from the Element14 Empire. I have to pay £30 quid and then go all "Hands Solo" from "Solder Wars" fame. (if the farce is with my at the time) Thats a big shame really cos I would have paid £40 willinging for one assemmbled by "R2D2" or some other Solder super Driod.

 

It looks then as if I will have to go remain Fluke PiStalker and wait for a Droid to build me one.

 

Come on Gert please chase the powers that be to get some assembled versions on the go for poor old guys like me whose idea or circuit assemmbly was screwing and fixing a couple of bits a BakerLite together 60 years ago. image

 

Seriously Gert a fantastic job great to see them in the wild but we cant all solder however easy it is, Take Pity Darth Gert and sort it for us.

 

That tale was NOT bought to you by any members of any film companies on the planet Earth. image

 

Just to keep the balls and games rolling ahead is my target.

 

Ray

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Hello All!

    Count me in on the Gert Board. I've purchased one this morning and I've downloaded the comicbook that has the solder lessons. I'm going to give it a go. Sorry to sound so basic - but I find all of the info, projects, lessons, questions and products a blast.

    Best,

    Peg

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Good luck Peg. Hope you have great fun.

     

    OK im Sold-ered. I always believed I am a terrible wielder of the soldering iron. But I have never really given myself a fair test. A few emergency repairs with big blobs of solder is all I have achieved until now. I have done many Arduino projects but always managed to find a way to connect stuff with non perm. connectors,adapters, couplers whatever just to avoid the dreaded iron.

     

    I would like a Gertboard and even though Steve Read kindly offered his services I have decided to bite the bullet and go Hands Soloder. image

     

    I have a good iron and a couple of Maplin bot kits I bought about a year ago (EOL 99p each), I shall tackle those first as a trial. They have a couple of motors a pic socket and a few transistors and resistors etc. If either of them works after my efforts I will order a Gertboard and go for it.

     

    So wish me luck. I type this with 10 unburnt hand digits at this time and these hands were born when WW2 rationing was still on. So I am quite fond of them. image

     

    Who knows maybe I'll surprise myself and be a solder Da Vinci. haha. Night all.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    Thanks Morgaine. Kind words indeed. But to be honest my good days are mainly behind me. I spent a lifetime working with chemistry and computers and making them react safely with each other. I am retired now and decided that hobby electroncics will be my way to keep brain and body nimbleish. image I've had a lot of fun with Arduino over the last couple of years and am loving the Pi. So on to the next project, and the next.....

     

    Ray

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • cityswift
    cityswift over 14 years ago in reply to e14 Contributor

    Hi Ray.  I have been following this discussion and feel that the following may be of some help to you.

     

    In a late eighties I toured the UK with the DTI mobile automated Electronics Factory demonstrating  surface mount techniques and all the other advanced manufacturing in electronics techniques coming to the forefront at that time.  After this I spent some time at the Highbury college in Portsmouth running the surface mount technology workshop.  At that time IBM had a local factory, and it was trying to cross train all its employees and their idea was that if everyone was flexible, then the factory would become more efficient. The factory made hard disk drives and there was a small surface mount board incorporated in that device. The idea was that they could take a storeman or perhaps a fork truck driver and get them to assemble surface mount boards the same way that the young female operators did.  So, without asking me if I thought it was feasible - IBM was always right -  they commissioned me to run a series of workshops to do the training. This just really did not work because the men not only found it very difficult to hold the tools and components steady, but also to see what was going on without powerful magnifiers.  The young females found it easy and produced high quality work. Needless to say, the experiment was abandoned after a short time.

     

    So, everything you have said in this discussion is validated by my experiences. However, I feel sure that the posts I make over the coming weeks will give you hope and enable you to complete a satisfactory kit build. Must stop now as I have run out of time. For the record, I was born before the WW2 rationing started, but still expect to complete a Gertboard kit build which will work first time.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to cityswift

    Very interesting post, cityswift, and inspiring too. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to cityswift

    Thanks for that Cityswift and I look forward to your additional posts. Us old dogs still got a few tricks in us eh? image

     

    Ray

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    About making soldering easier- I recently realized that one reason it's easier to solder at work than at home (apart from the nice binocular microscope) is that we have Metcal MX-500P-11 soldering irons. With that unit, the tip is only 4 cm away from the hand grip, making precision work easier.  I could not spend $500 for my own Metcal, so at home I have a cheap Radio Shack iron with a tip about 8 cm away from the grip, so it is 2x as long. That means any deviation in the angle of my hand is multiplied 2x at the tip relative to the Metcal, and that makes a real difference with accuracy.

     

    Is there any affordable iron with a short hand grip - tip distance? Or is that not practical with a simple, conventional iron (the Metcal uses RF heating right at the tip, so there is no separate heating cartridge to design around).

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    jbeale wrote:

     

    we have Metcal MX-500P-11 soldering irons. With that unit, the tip is only 4 cm away from the hand grip, making precision work easier.

     

    That is an excellent observation.

     

    PS. I have a very old Bausch & Lomb 20X binocular microscope fixed to my worktable, and when I set its 0.7-3.0 zoom to the lowest magnification I get 14X and am able to solder tiny features reasonably effectively.  Good hand control is really difficult though, so your point rings a strong bell.  I'll be looking out for shorter soldering irons.  A pic here for background:

     

    http://www.flickr.com/photos/morgaines/6172845302/in/set-72157627604533547

     

    Morgaine.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Thanks jbeale and Morgaine. Excellent tips (pun intended) about shorter irons  Mine is about 3 or inches from holding point to tip, Perhaps a shorter iron would help steady my wobbles or I need some oven gloves. image

     

    Ray

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 14 years ago in reply to morgaine

    Morgaine Dinova wrote:

    PS. I have a very old Bausch & Lomb 20X binocular microscope...

    If I had a binocular microscope, I'd just use my laser vision!  image  It doesn't work with a magnifier or monocular microscope or video monitor.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to johnbeetem

    There's a joke about sharks and overlords there somewhere, but it refuses to materialize. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • cityswift
    cityswift over 14 years ago in reply to morgaine

    I have looked at the Gertboard assembly manual and the soldering instructions are basically

    1. Solder iron in

    2. Solder in

    3. Solder out

    4. Solder iron out.

    I think the process deserves more coverage than that, as if you have an understanding of what is happening, then you have much better chance of doing it correctly.

     

    This is what happens when you make a joint using 60/40 tin lead solder wire with a rosin flux core and an iron tip temperature of around 270 degrees C.

    1. All surfaces must be bright and shiny to start with.

    2. The tip is applied to the surfaces being soldered to bring them up to its temperature.

    3, The solder is fed into the joint and it melts a 185 C releasing the now molten flux into the joint. The flux is inert at room temperature but becomes molten at 120 C and mildly acidic so that it dissolves the thin layer of oxide on the surfaces allowing the formation of a pure alloy. This is the process known as wetting, and the flux is the key to its achievement. The solder is then withdrawn.

    4. The tip is removed and the temperature drops rapidly and the solder solidifies at 185 C and the flux residue solidifies around 100 C and reverts to its inert state. The components must not be moved during the freezing process so some method of achieving that needs to be implemented.

     

    I am sure that many of you will already know this, but I thought it worth repeating so that you start on a solid foundation.

    I have ordered bits to test out some ideas and more will follow.

    Dave Tedd

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • cityswift
    cityswift over 14 years ago in reply to morgaine

    I have looked at the Gertboard assembly manual and the soldering instructions are basically

    1. Solder iron in

    2. Solder in

    3. Solder out

    4. Solder iron out.

    I think the process deserves more coverage than that, as if you have an understanding of what is happening, then you have much better chance of doing it correctly.

     

    This is what happens when you make a joint using 60/40 tin lead solder wire with a rosin flux core and an iron tip temperature of around 270 degrees C.

    1. All surfaces must be bright and shiny to start with.

    2. The tip is applied to the surfaces being soldered to bring them up to its temperature.

    3, The solder is fed into the joint and it melts a 185 C releasing the now molten flux into the joint. The flux is inert at room temperature but becomes molten at 120 C and mildly acidic so that it dissolves the thin layer of oxide on the surfaces allowing the formation of a pure alloy. This is the process known as wetting, and the flux is the key to its achievement. The solder is then withdrawn.

    4. The tip is removed and the temperature drops rapidly and the solder solidifies at 185 C and the flux residue solidifies around 100 C and reverts to its inert state. The components must not be moved during the freezing process so some method of achieving that needs to be implemented.

     

    I am sure that many of you will already know this, but I thought it worth repeating so that you start on a solid foundation.

    I have ordered bits to test out some ideas and more will follow.

    Dave Tedd

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to cityswift

    This is what happens when you make a joint using 60/40 tin lead solder

    Lead free solder is somewhat different.. I still struggle with it, and as someone with long history of tin/lead soldering I always think I've done it wrong when I don't get the shiny surface I'm used to seeing image