Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum USB discussions getting a bit heated
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 87 replies
  • Subscribers 710 subscribers
  • Views 16428 views
  • Users 0 members are here
Related

USB discussions getting a bit heated

e14 Contributor
e14 Contributor over 14 years ago

On the other forum, discussions of USB and networking problems have been

getting a bit heated recently, with one user, Sulge, banned yesterday by abishur

for a 1-week cooling off period.  Maybe we will see him here soon.

 

http://www.raspberrypi.org/phpBB3/viewtopic.php?f=28&t=12097&start=177

http://www.raspberrypi.org/phpBB3/viewtopic.php?f=24&t=14151

http://www.raspberrypi.org/phpBB3/viewtopic.php?f=28&t=5249

 

Some of the USB issues are being blamed on Linux latency, which

doesn't sound easy to fix.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Those threads are terrible image They downplay most of the problems people have encountered and add confusion.

     

    But it's a timebomb waiting to go off...

    I guess user Kernel sums it up pretty nicely http://www.raspberrypi.org/phpBB3/viewtopic.php?f=28&t=12097&start=197

     

     

    Frankly even though the Foundation people are not making profit on Raspi, I think it doesn't make them any less responsible for the quality of the device they designed and have been (indirectly) selling.

     

    Regardless of the cause (software, power, design) of Pi's problems, they are frustrating to deal with and are likely to cause many to lose interest at some point (even children, or perhaps especially them).

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Those threads are terrible image They downplay most of the problems people have encountered and add confusion.

    Thing is, the issues are complex. A lot of the confusion is being caused by people who mostly don't have a grasp of either the hardware or software problems.  Lets face it, with a usb IP block that nobody seems to have much information about, we're all in the dark and what makes it tick may as well be black magic image

     

    Still, at this point the Pi really is a development board - there's lots of development happening and various people working on fixing issues. Unfortunately due to all the hype there's lots of them landing in the hands of people who are used to a device that's been in development for years with budgets in the billions and expect everything to 'just work' instantly, instead they have a device that was designed to a strict budget with all the compromises that entails. This was bound to cause some friction.

     

    I suspect the RPF was very much unprepared for the amount of destructive stress testing a couple of hundred thousand users can do in such a short time with devices that were never thought of during the design.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    selsinork wrote:

     

    Time may provide a solution, would certainly be disappointing if it didn't, and a software fix would be the best outcome..

     

    A software fix is quite likely to be able to resolve the problem, no matter how broken the controller core, just by working within its limitations.  In the same way that USB drivers reserve bandwidth for audio channels for example (and reject connections which they know cannot work), a driver that understands the controller's limits could allow only such devices that can work together to connect.

     

    This could limit the choices, but we would at least have a 100% working platform within well defined constraints, and that is crucial.  Flakey operation has no place in USB.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dharr19
    dharr19 over 14 years ago in reply to morgaine

    Hi Morgaine,

     

    You seem good at explaining things to non-engineer types.  My question to you is this.  I attached an Abe Bluetooth dongle directly to my Pi.  On the dongle there are to light diodes (I think) one turns and stays red the other green and it flashes during data transmissions.  During bootup I saw that the system did pick up the bluetooth and the generic bluetooth driver was loaded.  So is it possible that a system can pick up a device that is connected to its usb ports but not have enough to power it?  Or is it possible for the bluetooth to be broken but still be recognized. I ask this because no lights appeared at all and given the conversation regarding usb ports ...

     

    Cheers

    David

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to dharr19

    @David: I'll try to answer. image

     

    All of the fault scenarios that you mention are feasible as a combination of Pi power constraints, Pi USB faults, and ARM driver non-working.  I don't know whether your particular Bluetooth dongle is known to work with ARM using class-compliant drivers, but let's assume that it does otherwise there is little point in further analysis.

     

    (Eg. if it only works with a binary x86 driver blob then obviously there is no chance of it working on ARM, and if it is not class-complaint and hence requires its own bespoke Linux driver which hasn't yet been ported to ARM then again, there is little a non-developer can do.  Therefore let's assume that it works with ARM, so we're just trying to get an ARM-capable device to work with Pi.)

     

    Your first question can be answered even without any testing:

     

    David Harrison wrote:

     

    During bootup I saw that the system did pick up the bluetooth and the generic bluetooth driver was loaded.  So is it possible that a system can pick up a device that is connected to its usb ports but not have enough to power it?

     

    Yes, it is possible, because before a USB Bluetooth dongle transmits RF, it will attempt to get connected into the USB device chain.  That involves only the USB interface circuitry on the dongle and not its RF circuits, which would normally be quiescent at this stage and hence not consuming much power.  (Significantly more power is consumed by the dongle when it transmits Bluetooth RF than when it is not transmitting.)  So, the dongle could in principle need only a little current during the connect phase, well within the Pi's capabilities, but then later require in excess of the Pi's power limits when transmitting.

     

    USB has a way of dealing with this "I need more current" situation because it is quite common.  Host ports are required to be able to deliver an initial unit of current, and then additional units are negotiated between the USB host and the power-hungry device.  Unfortunately I don't think we know exactly how this negotiation works on Pi, because although the LAN9512 chip contains a hub and is (presumably) USB-compliant, that hub is not self-powered but takes power from the Pi board under SoC control, which has some idiosyncracies.

     

    The Pi has polyfuses with high on-resistances in series with its USB power lines, so the current available to devices that request more is limited by the voltage dropping as more current is provided, until eventually the voltage drops below USB spec or the polyfuse trips and pretty much turns it off altogether.  What's more, we have no idea whether the Pi's highly broken USB driver understands that there are polyfuses in those lines and hence that it cannot just offer additional units up to the USB maximum if it does grant such requests.  Even if it does or could, the wide variation in polyfuses on-resistance would make this very hit-or-miss.  I hope that is not happening.

     

    The best we can hope for is that the Pi's driver has been set up to refuse to grant additional units of current above 100mA.  We could then have the situation that a Bluetooth dongle gets enough power from the USB port to allow the Pi's USB driver to enumerate it and to commence the power negotiation.  The extra power request would then be rejected, and if the dongle has the smarts to recognize the rejection, then the dongle's RF transmitters would never be enabled.  The device would be inoperative as you hypothesized, but recognized as a USB device.

     

    I hope that answers your first question and explains the reasoning behind the answer.

     

    To get some more info on what actually happens within Pi we would have to read the USB driver source to see whether it handles power negotiation and whether requests are granted or rejected, and we'd have to look for messages that would be logged if a power request were refused.  You would then have to look for such refusal messages in your error messages log.

     

    Your second question (separate from the power question) isn't easy to answer in any detail:

    Or is it possible for the bluetooth to be broken but still be recognized. I ask this because no lights appeared at all and given the conversation regarding usb ports ...

     

    Because the USB interface circuitry is generally separate from the rest of a device, that is certainly possible in principle.  However, assuming that we're talking about class-compliant devices that are known to work on ARM, I would think that it's unlikely for the non-USB part of the device to be totally inoperative on Pi unless it's caused by the generally broken state of Pi's USB system.  It's very hard to say.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dharr19
    dharr19 over 14 years ago in reply to morgaine

    Thank you so much for all your helpimageimageimage

     

    Cheers

    David

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    ah ha Morgaine!  We may be "clueless" and walking around in the dark - - - but we sure know how to find someone with a lightimage

     

    great explanation to @David.

    Best

    peg

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    Funny comment, Peg, but I hope the references to 'clueless' weren't misunderstood. image

     

    The 'clueless' aren't those who don't know --- the more you know, the more you realize that you don't know, so not knowing is not the defining property.  It's only those who don't wish to know and don't wish to think, or cannot think.

     

    Walking around in the dark is what we all do, but the desire for illumination is what takes us to the nearby planets today, and one day to the stars.  Civilization is all about riding on the shoulders of those who went before, so if you know how to find someone with a light then you're helping to carry that torch forward and build that pyramid of knowledge and capability.

     

    Welcome to the dark.  But as you said so well, we sure know how to find someone with a light.image

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jamodio
    jamodio over 14 years ago in reply to morgaine

    Let me clarify the context related to my "clueless" comment.

     

    I have no issue or problems with people that don't have a clue and are asking the right questions and in a proper manner. I've been clueless and I'm clueless in many many things and we all at sometime are "newbies." That's not the issue.

     

    The issue is with a forum where moderators are supposed to, among other things "moderate" some comments so wrong information doesn't get widespread.

     

    In the case of the R-Pi forum if somebody states something like "The chips in the RPi are supposed to run hot, they are designed to operate safely to 120 degrees C," I've not seen any moderator or anybody from RPF to reply to that comment so the clueless person that made it can get un-clueless, or even providing the right information about what is the correct operating temperature range for the R-Pi and its parts.

     

    On the other hand people reporting real problems, and providing valuable information, get bashed, harassed, called names and banned.

     

    This is from where my "clueless" comment came from.

     

    -J


    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to jamodio

    All,

    I got a kick out of the clueless thing!! Hope you didn't misunderstand my compliment!

    I have learned so much in the last few months - and it's from reading then researching, then doing after you have explained or discussed something. . .

    My thanks to you all - keep the light comingimage

    peg

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    Morgaine. . . I've become a fan of yours...please see my reply to jamodio

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    Peg Wagner wrote:

     

    Morgaine. . . I've become a fan of yours...please see my reply to jamodio

     

    Yay, I have a fan!  I'm not sure what to do now, I've never had one before. image

     

    PS. I can't improve on your last line to jamodio --- "keep the light coming".  That's glorious! image image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    Peg Wagner wrote:

     

    Morgaine. . . I've become a fan of yours...please see my reply to jamodio

     

    Yay, I have a fan!  I'm not sure what to do now, I've never had one before. image

     

    PS. I can't improve on your last line to jamodio --- "keep the light coming".  That's glorious! image image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    One light that stays off is that of the backfeeding usb hubs. If the Pi is powered from the a downstream port of the same hub, wouldn't that basically ensure that the Pi receives the full voltage, and shouldn't it boot normally, besided getting some voltage as well on one of it's usb ports? This would basically just short the main and usb polyfuse on the board. But reading from reports, people say that keyboard and mouse behavour is bad with a hub providing power to it's upstream port. This doesn't make sense.

     

    Considering the power negotiation of usb ports. When you run into issues on a windoze pc, it simply shows a warning message that a device needs more power and should be connected to a self powered hub. Since the driver is not loaded, the device can't start to consume the power it needs. The usb port will keep providing current untill a Polyfuse trips (or some other protection turns on.) On cheap mobo's, they will even provide just one 1Amp fuse for 2 usb ports. It will have a lower resistance under normal operating conditions, and power hungry usb harddisks will work as long as the second usb port isn't badly loaded as well. Maybe it's an idea to improve the price on the Pi2.