Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum USB discussions getting a bit heated
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 87 replies
  • Subscribers 710 subscribers
  • Views 16428 views
  • Users 0 members are here
Related

USB discussions getting a bit heated

e14 Contributor
e14 Contributor over 14 years ago

On the other forum, discussions of USB and networking problems have been

getting a bit heated recently, with one user, Sulge, banned yesterday by abishur

for a 1-week cooling off period.  Maybe we will see him here soon.

 

http://www.raspberrypi.org/phpBB3/viewtopic.php?f=28&t=12097&start=177

http://www.raspberrypi.org/phpBB3/viewtopic.php?f=24&t=14151

http://www.raspberrypi.org/phpBB3/viewtopic.php?f=28&t=5249

 

Some of the USB issues are being blamed on Linux latency, which

doesn't sound easy to fix.

  • Sign in to reply
  • Cancel
Parents
  • johnbeetem
    johnbeetem over 14 years ago

    From what I've read, it seems that the fundamental problem is that the BCM2835 SoC has a bare-bones USB host controller which requres a lot of the ARM processor.  Such a USB host controller works fine in BCM2835 intended applications, such as Roku, but if you try to use the ARM11 as a high-performance GNU/Linux engine talking to dozens of USB devices you will run into limitations.  It also sounds like documentation for the SoC's USB host controller is not available and that the low-level "open source" software suffers from "security through obscure code".  If this is indeed the case, it will be hard to improve things.

     

    Please let me know if my impressions are incorrect.  I would be delighted to hear that open documentation for the USB host controller is available (link?) and that the low-level driver is perfectly understandable and well-documented (link?).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to johnbeetem

    John Beetem wrote:

     

    From what I've read, it seems that the fundamental problem is that the BCM2835 SoC has a bare-bones USB host controller which requres a lot of the ARM processor.  Such a USB host controller works fine in BCM2835 intended applications, such as Roku, but if you try to use the ARM11 as a high-performance GNU/Linux engine talking to dozens of USB devices you will run into limitations.  It also sounds like documentation for the SoC's USB host controller is not available and that the low-level "open source" software suffers from "security through obscure code".  If this is indeed the case, it will be hard to improve things.

     

    This is EXACTLY the same conclusion that I have reached.

     

    The Pi is in reality not a general purpose computer.  It's half a computer, with the ARM being used to fill in the hardware gaps that let the SoC be designed at the lowest possible cost.  If you try to use the ARM at the same time for normal computing, you can kiss your SoC's correct functioning goodbye.

     

    It's this that is wreaking havoc when you attach a correctly-working self-powered hub with added devices downstream.  Linux accepts it, because it doesn't realize what the purpose of the ARM is within the BCM2835.  In reality it should say "Sorry Dave, I don't have the CPU headroom for that" and refuse to attach.

     

    Morgaine.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    it should say "Sorry Dave, I don't have the CPU headroom for that" and refuse to attach.

    LOL...  but does sound work well enough for it to sing the song ?

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    it should say "Sorry Dave, I don't have the CPU headroom for that" and refuse to attach.

    LOL...  but does sound work well enough for it to sing the song ?