Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum USB discussions getting a bit heated
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 87 replies
  • Subscribers 710 subscribers
  • Views 16502 views
  • Users 0 members are here
Related

USB discussions getting a bit heated

e14 Contributor
e14 Contributor over 14 years ago

On the other forum, discussions of USB and networking problems have been

getting a bit heated recently, with one user, Sulge, banned yesterday by abishur

for a 1-week cooling off period.  Maybe we will see him here soon.

 

http://www.raspberrypi.org/phpBB3/viewtopic.php?f=28&t=12097&start=177

http://www.raspberrypi.org/phpBB3/viewtopic.php?f=24&t=14151

http://www.raspberrypi.org/phpBB3/viewtopic.php?f=28&t=5249

 

Some of the USB issues are being blamed on Linux latency, which

doesn't sound easy to fix.

  • Sign in to reply
  • Cancel
Parents
  • yvanttt
    yvanttt over 14 years ago

    Here are some results i ran into when using cheap powered hub.

     

    Initialy they may seem incompatible with th PI, but it could be due to some compromise in the design/production run to cut pricr down.

     

    I ordered some cheap 7 port power USB hub (like 3 for $12) with the power supply included.

     

    on my 1rst attempt i connected my PI to the hub for both power, keyboard and mouse on the hub.

    The PI would start to boot and then keept on rebooting.

    I removed the keyboard and mouse, no change.

     

    The supplied power supply was rated for 5v 1A only, clearly insuficient current rating. so i used a 5v 2A supply i had left over.

     

    I reconnected everything back, then the PI booted till it got to the USB port detection and then it was looping into the USB detection sequence. Then i noticed the micro usb plug was NOT connected on the PI ????? The PI was receiving power from the normal USB jack instead.

     

    I then connected the micro USB plug and reapplied power, now the PI booted normaly. But the keyboard and mouse where erratics.

     

    I decided to look inside the USB hub case and i found a jumper that connected the external power supply to the +5v side on the incoming usb connector from the PI.

     

    Then i proceded to remove said jumper. Now the PI would not power on from the hub, good.

    So i connected the micro usb cable to the powered hub along the keyboard and mouse.

    now they are all behaving properly.

     

    So my theory is that when the jumper wire was installed in the hub and you use the same hub for both power and expansions some current loops may be created inside the PI and cause some undesirable behaviour.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • yvanttt
    yvanttt over 14 years ago

    Here are some results i ran into when using cheap powered hub.

     

    Initialy they may seem incompatible with th PI, but it could be due to some compromise in the design/production run to cut pricr down.

     

    I ordered some cheap 7 port power USB hub (like 3 for $12) with the power supply included.

     

    on my 1rst attempt i connected my PI to the hub for both power, keyboard and mouse on the hub.

    The PI would start to boot and then keept on rebooting.

    I removed the keyboard and mouse, no change.

     

    The supplied power supply was rated for 5v 1A only, clearly insuficient current rating. so i used a 5v 2A supply i had left over.

     

    I reconnected everything back, then the PI booted till it got to the USB port detection and then it was looping into the USB detection sequence. Then i noticed the micro usb plug was NOT connected on the PI ????? The PI was receiving power from the normal USB jack instead.

     

    I then connected the micro USB plug and reapplied power, now the PI booted normaly. But the keyboard and mouse where erratics.

     

    I decided to look inside the USB hub case and i found a jumper that connected the external power supply to the +5v side on the incoming usb connector from the PI.

     

    Then i proceded to remove said jumper. Now the PI would not power on from the hub, good.

    So i connected the micro usb cable to the powered hub along the keyboard and mouse.

    now they are all behaving properly.

     

    So my theory is that when the jumper wire was installed in the hub and you use the same hub for both power and expansions some current loops may be created inside the PI and cause some undesirable behaviour.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • morgaine
    morgaine over 14 years ago in reply to yvanttt

    The USB upstream A-B backfeed that you describe is what causes the official "Pi Accessory" 7-port Dynamode hub to fail with the Pi, as I described in this thread ---  http://www.element14.com/community/thread/19316?tstart=30  .

     

    I'll probably hack out the backfeed path or insert a diode some day, but for now it's working fine with Intel PCs.

     

    Unfortunately the Pi's USB problems go far beyond just being succeptible to backfeed from cheap hubs.