Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum USB discussions getting a bit heated
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 87 replies
  • Subscribers 710 subscribers
  • Views 16499 views
  • Users 0 members are here
Related

USB discussions getting a bit heated

e14 Contributor
e14 Contributor over 14 years ago

On the other forum, discussions of USB and networking problems have been

getting a bit heated recently, with one user, Sulge, banned yesterday by abishur

for a 1-week cooling off period.  Maybe we will see him here soon.

 

http://www.raspberrypi.org/phpBB3/viewtopic.php?f=28&t=12097&start=177

http://www.raspberrypi.org/phpBB3/viewtopic.php?f=24&t=14151

http://www.raspberrypi.org/phpBB3/viewtopic.php?f=28&t=5249

 

Some of the USB issues are being blamed on Linux latency, which

doesn't sound easy to fix.

  • Sign in to reply
  • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    selsinork wrote:

     

    If the BCM2835 is still the best multimedia device available, fine, use it,

    I'm still uncertain how that matters. Right now all that potential still hasn't found an outlet. Lack of codecs prevents serious multimedia use and lack of accelerated X driver means you get no benefit elsewhere. Those things are being worked on, but without a timetable. So it could still be the best unused multimedia device in 5 years.

     

    +1.

     

    Reminds me of another unrelated discussion I was having, about hidden costs and liabilities.

     

    The BCM2835's closed nature is proving a liability to the Pi community already, and the USB core's closed nature is proving a liability to Broadcom already, as well as to the community.  It's somewhat incredible that the Pi is being marketted on the multimedia strengths of the BCM, yet neither X11 nor open media players like mplayer are accelerated yet just because it's closed tight as a drum.

     

    Well I suppose I'm "reaching out" to Broadcom/RPF and throwing them a crumb (not that they deserve it) by suggesting to continue using their device to handle the graphics at least, but in reality you're right.  Designing in a liability is not sensible.

     

    Morgaine.

     

     

    [Addendum:  It's worth pointing out that chucking out the BCM2835 wouldn't leave us without graphics.  The TI AM3358/9 contains a PowerVR SGX530 GPU, and it's no slouch.  Of course it's nearly as closed as the Broadcom so it's still a liability, but it comes for free with a Cortex-A8 and proper USB and Ethernet controllers.  Oh and <shock horror>, documentation.]

     

    PS. I've  just discovered that the Ethernet MAC on the TI AM 3358/9 is 10/100/1000 !!  It's only the PHY on the BeagleBone that limits it to 100Mbps.  So it's even more "proper" than I thought. :-)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago

    I wonder what Farnell and RS's reaction is to all this.  I suspect that no other computer-like product they sell is so badly broken and incompatible with common USB devices.  They can't be pleased, and their high-level talks with RPF must be "interesting".

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 14 years ago in reply to morgaine

    Morgaine Dinova wrote:

    PS. I've  just discovered that the Ethernet MAC on the TI AM 3358/9 is 10/100/1000 !!  It's only the PHY on the BeagleBone that limits it to 100Mbps.  So it's even more "proper" than I thought. :-)

    Actually, the AM3358/9 have versions with two 10/100/1G Ethernet ports which can be coupled to make a three port Ethernet switch (the third port being the CPU).  It also has support for IEEE 1588 Precision Time Protocol, if you really want to know what time it is image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to johnbeetem

    John Beetem wrote:

     

    Actually, the AM3358/9 have versions with two 10/100/1G Ethernet ports which can be coupled to make a three port Ethernet switch (the third port being the CPU).  It also has support for IEEE 1588 Precision Time Protocol, if you really want to know what time it is image

     

    Awesome chip.  It needs someone to make a rock-bottom board using it to compete at the Pi price niche.

     

    There are quite a few things that could be whittled off the BeagleBone to bring the BOM cost down from $89:

     

    • The PMIC expansion header and LCD/backlight interface are not essential.
    • The PMIC itself has a lot of extra features outside of power management that may be superfluous in a bottom-end board so a cheaper PMIC may be available.
    • The front-end USB hub is not essential.
    • The front-end FT2232H that connects to the USB hub is not essential.
    • The BeagleBone's USB device/host flexibility could be reduced by routing the SoC's two USB OTG ports to a combined host USB connector for lower cost.
    • The reset button is not essential.
    • The two large expansion headers provide good physical support for daughterboards, but could be shortened to reduce cost.
    • If one must play RPF-type marketing tricks, don't supply the micro-SD card with the board.
    • It must be remembered that in addition to BOM reductions, there will be at least one increase:  HDMI socket and associated circuitry, which must be on-board..

     

    I bet that such reductions could get the BOM cost down down to the Pi price niche for Pi-type volumes.  BeagleBone is made in much smaller volumes than Pi, so their volume price breaks are probably not very good currently, but with volume sales that would change dramatically.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 14 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    I bet that such reductions could get the BOM cost down down to the Pi price niche for Pi-type volumes.  BeagleBone is made in much smaller volumes than Pi, so their volume price breaks are probably not very good currently, but with volume sales that would change dramatically.

    I think the key here is volume.  In large volumns BB could probably come down to under US$50 even with the current BOM, and the DVI cape could come down to US$15 instead of US$50.  Another cost factor is USA manufacturing, but I'm happy to pay a bit more and not wonder about quality.

     

    I like having a separate video cape so you have the choice of VGA (coming soon!) or LCD.  But à la carte is always going to be more expensive.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to johnbeetem

    True, the flexibility of BeagleBone is very high, but unfortunately price is king.

     

    Sadly, the board is priced above the point on the budget radar where price is no barrier for the average pocket in the "West" (often said to be the price of an evening out).  But the board is also so well specified that there is ample room for a bottom-end product of that line created through feature reduction.

     

    The Beagle family would be rounded off beautifully with a "BeagleBite" (to stay within their naming meme), where everything except reliability is sacrificed at the altar of BOM cost.  And when sales rocket in reverse exponential proportion to price, the team would find itself with a whole product line ready to cater for different use cases, unlike Pi.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to johnbeetem

    Actually, the AM3358/9 have versions with two 10/100/1G Ethernet ports

    Doesn't take a lot of imagination to realise that a lot of people would be interested in a cheap device with two decent ethernet ports.  Different target market, but still.  With three configurations, one with usb only for all the weird wifi lovers, then single wired port and dual wired port versions you have an interesting device.

     

    Only question is whether the Arm is fast enough to deal with two 1G ports. I've come across a fair few of those little nas enclosures that do have 1G ports but barely manage 100M speeds on them.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    And when sales rocket in reverse exponential proportion to price, the team would find itself with a whole product line ready to cater for different use cases, unlike Pi.

    If nothing else the Pi has proved there's a market for a cheap device. Hopefully another device will rise to that challenge and some healthy competition gives us some interesting devices to use.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jamodio
    jamodio over 14 years ago in reply to e14 Contributor

    Probably right, but remember that the R-Pi has been always promoted as a cheap linux "computer," many people realize that to make it work as a computer there is other stuff and extra expenditure associated with it.

     

    I wonder when Eben will stop saying that the R-pi can do "what other computers do."

     

    -J

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dharr19
    dharr19 over 14 years ago in reply to morgaine

    Hi Morgaine,

     

    You seem good at explaining things to non-engineer types.  My question to you is this.  I attached an Abe Bluetooth dongle directly to my Pi.  On the dongle there are to light diodes (I think) one turns and stays red the other green and it flashes during data transmissions.  During bootup I saw that the system did pick up the bluetooth and the generic bluetooth driver was loaded.  So is it possible that a system can pick up a device that is connected to its usb ports but not have enough to power it?  Or is it possible for the bluetooth to be broken but still be recognized. I ask this because no lights appeared at all and given the conversation regarding usb ports ...

     

    Cheers

    David

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>