Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Per-seat codec licensing for Raspberry Pi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 706 subscribers
  • Views 2033 views
  • Users 0 members are here
  • raspberry_pi
Related

Per-seat codec licensing for Raspberry Pi

morgaine
morgaine over 14 years ago

I was quite disappointed by the news of additional optional licensing costs for Pi, announced in this  RPF blog article, "New video features! MPEG-2 and VC-1 decode, H.264 encode, CEC support"  -- http://www.raspberrypi.org/archives/1839 .  The costs are not high, but the principles involved are worrying.

 

These optional codec licenses are being sold tied to an individual Pi's serial number, so this is what's known as "per-seat licensing" in the education and commercial worlds.  Not only does it inflate the effective cost of Pi by some additional amount, but it is not portable from Pi to Pi.  That is especially bad news for hardware enthusiasts who inevitably take risks with their Pi, since it would appear that they will not be able to move this license to another Pi board.

 

The whole idea of adding restricted codec licenses to an educational product seems very misguided to me.  It's not contributing to the Pi's goal of education in the slightest, and it introduces the horrid issue of software patents which have a very chilling effect on innovation, education, and research.

 

Summary view:  the Pi is becoming more closed instead of more open.

 

Morgaine.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    I actually see this as positive thing and disagree with the comment "... Not only does it inflate the effective cost of Pi by some additional amount,". It only increases the cost of the Pi for those that want native support for these decoders and not the base cost of the Pi for those who do not want it e.g. education. Also its only £2.40, its less than the cost of a pint of beer and if the Pi dies and I have to but another one, hey its only £2.40, less than the cost of a pint of beer .... thats something I can accept.

     

    The only slightly annoying thing out of this is that Liz has closed one of the most interesting threads on the Pi forums, the mpeg2 thread. It would have probably died anyway but I don't see any need to close it as what those guys were doing was really interesting to a bystander like me.

     

    Rob

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    welshblob wrote:

     

    It only increases the cost of the Pi for those that want native support for these decoders and not the base cost of the Pi for those who do not want it e.g. education.

     

    While that is certainly true because the extra cost is purely optional (as I clearly noted above), it doesn't recognize a few issues:

     

    • Some schools will inevitably purchase the licenses to have "a fully working Pi".
    • The schools that purchase only a few licenses will pay the price of platform divergence.
    • The schools that don't purchase licenses on principle will not be able to run all Pi software.
    • The extra amount would not be visible at all if it had been covered in the Pi BOM cost.

     

    In other words, this does not appear to have been the most sensible course of action at all.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    OK you stated it was optional in one sentence then condradicted that by saying that the effective cost of the Pi had increased! Make your mind up!

     

    In my opinion schools won't care about mpeg2 licenses. I assume most will be focussed on basic programming on the Pi and any video processing is likely to be with h264 especially as the encoder is now also available and will be used with the soon to be released camera module. h264 appears to be the future codec given its wide adoption which I expect is partly due to its low licensing cost.

     

    You do seem to be tilting at windmills here.

     

    Rob

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    I'm pretty philosophical about this. They've managed to deliver MPEG-2 handling to the people who bought the board for media duties - and without making them shell out for the camera module (which was to act as a dongle). They've also managed to convince MPEG LA that they have a robust C/R mechanism. Fair play. I hate C/R because it's a fact of life here (as in "Jesus, I paid a fortune for this software, what if I go to reauthorise after changing a motherboard and find the company has gone bust and there's no C/R server..."). Such is life in the world of "there's no freeware option". image

     

    No educational establishment explicitly needs MPEG-2 support. If the I.T. guy buys it just "because it's there" then that probably speaks volumes about the quality of training that those poor kids are going to get...

     

    I'm happy to cut the Foundation a break on this one. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    I'm pretty philosophical about this. They've managed to deliver MPEG-2 handling to the people who bought the board for media duties - and without making them shell out for the camera module (which was to act as a dongle). They've also managed to convince MPEG LA that they have a robust C/R mechanism. Fair play. I hate C/R because it's a fact of life here (as in "Jesus, I paid a fortune for this software, what if I go to reauthorise after changing a motherboard and find the company has gone bust and there's no C/R server..."). Such is life in the world of "there's no freeware option". image

     

    No educational establishment explicitly needs MPEG-2 support. If the I.T. guy buys it just "because it's there" then that probably speaks volumes about the quality of training that those poor kids are going to get...

     

    I'm happy to cut the Foundation a break on this one. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    Jonathan Garrish wrote:

     

    "and without making them shell out for the camera module (which was to act as a dongle)."

     

    That's good news for a change!  Dongles would have balkanized the Pi as a common platform even further.  But it's not all positive --- notice that the camera module would have been portable to another Pi board, whereas these licences cannot be moved between Pi boards.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    Jonathan Garrish wrote:

     

    "and without making them shell out for the camera module (which was to act as a dongle)."

     

    That's good news for a change!  Dongles would have balkanized the Pi as a common platform even further.  But it's not all positive --- notice that the camera module would have been portable to another Pi board, whereas these licences cannot be moved between Pi boards.

     

    It happens - it's a commercial product. One criticism often levelled at education is that it fails to prepare them's what's doing it for the rigours of real life. The whole Pi thing so far has been a window on the world of having an idea and putting it out there. The Good, the Bad and the Ugly. One day someone will hopfully write a paper on the Foundation's rather bizarre roadtrip and use it as teaching material!

     

    Regarding dongles. We use them too. Great if you want to run that s/w on more than one computer, but the possibility of loss or theft gives me the heebies.I hate paying for them as well, because they're supposed to be raising extra revenue for the software vendor! Why aren't they free? And why are there different formats? Agh!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jdavidgea
    jdavidgea over 14 years ago in reply to e14 Contributor

    It's not  a commercial product... Well it shouldn't be a commercial product:

     

    - If it's a commercial product is a low quality one with lots of problems not being solved.

     

    - If it's not a commercial product a lot of effort is being made to make profit from it.

     

    I'm waiting any copy of this made with an AllWinner chip or similar. Even if it's made as a commercial product I bet it would be 10 times better than what the RaspberryPi Foundation is offering.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to jdavidgea

    I'm not sure that there's much of an argument to be made either way, since it's clearly both at the same time.

     

    It's a commercial product with a very low profit margin for the manufacturing partners --- their main "profit" is in gaining colossal exposure and exclusive standing far beyond anything that they could have dreamed or paid for.  Nobody else can gain entry to this exclusive club.  Opportunities like this are more rare than hens' teeth, and their competitors in the distribution industry have been left in the dust.  It's a wonderful feather in their cap.

     

    But on the other hand it's not a commercial product in the normal sense.  The partners are not free to set their own price points, and they are not free to modify the design independently and still call it "Raspberry Pi" to remain on the gravy train, and they are getting a mountain of flak stemming from the design and community relations issues.  These things have to be subtracted from the previous plus points, and their ability to influence them is far less than for a normal commercial product which they could drop instantly without much angst.

     

    Plus of course the whole purpose of Pi is to open the doors of technical interest to a whole new generation of budding engineers, a highly worthwhile goal but not exactly a balance sheet item.  The latter must be really hard to justify to the beancounters, yet for those who can look beyond current ledger pages, it's clearly the right thing to do.

     

    So ... "it's complicated". image

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jdavidgea
    jdavidgea over 13 years ago in reply to jdavidgea

    I

    José David Gea Esteban wrote:

    I'm waiting any copy of this made with an AllWinner chip or similar. Even if it's made as a commercial product I bet it would be 10 times better than what the RaspberryPi Foundation is offering.

     

    I've been following the Cubieboard project. It's nice and seems to cover much of the holes the RaspberryPi isn't kind to fullfil. It's a step in the direction to have better commercial products to really learn or use.