Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum 7" monitor cabling conundrum
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 705 subscribers
  • Views 881 views
  • Users 0 members are here
  • raspberry_pi
Related

7" monitor cabling conundrum

recantha
recantha over 14 years ago

Just a quick repost from something I posted on the Foundation forum as I reckon there's more technical knowledge over here!

 

 

I need some help with adapting some wiring.


I bought an item off eBay http://www.ebay.co.uk/itm/110940093247.


Now, I probably should have known better when I saw the HDMI label on it... I'm hoping that it is still decent definition, but I have a bit of a cable problem.


Here's a picture of the whole package:

Image


Here's a couple of close-ups of the cable that attaches to the cable that comes out of the bottom of the screen. It's got 6 pins and looks a bit like a PS/2 cable. I _think_ it's a 6-pin DIN, but I could be talking out of my bum.

Image

Image


and one of the cable pack that comes with it.

Image


I know, I know... Doesn't look promising.


So, there's a ground wire (black) and a 12V wire. Now, obviously it's a car rear view screen, so it's expected that the 12V wire is supposed to be connected to the rear tail light and then another wire goes back to power the tail light.


What I really want it to run it off the mains.


I have another screen that is _very_ similar, but has an adapter on the end for a 12V mains power supply (which I've got). Here's the display:

Image

Another similar one:

Image

And a close-up of the cable ends that I want to have for the new screen:

Image

And this shows what the whole cable looks like on mine - note the little gadget that is on the live wire (which has a fuse inside it):

Image



What I've done so far is to take the connector off the end of the 3.5" cable (the end that goes into the screen box) to reveal a red (live) wire, a ground and a yellow and a white (which must be the two composite inputs).


Now, what I think I have to do is to cut open the new input cable (with the 6 pin male connector), separate the wires and solder them to their equivalents on the 3.5" cable.


Does this sound right? I'd rather not a) blow the mains b) blow my head off c) blow the screen up d) blow the Pi up.


Hope someone can help.

--

Mike

  • Sign in to reply
  • Cancel
Parents
  • cityswift
    cityswift over 14 years ago

    Hi Mike I have looked at the original ebay listing and the display box says that the unit is VGA - not HDMI - so the listing was innaccurate. Pi will not feed a VGA monitor - it outputs only composite video (CSV) or HDMI. The second smaller unit is CSV and can be fed from the Pi RCA output. I have the same unit and it works fine from the Pi, although the text is small. Hope this helps.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • cityswift
    cityswift over 14 years ago

    Hi Mike I have looked at the original ebay listing and the display box says that the unit is VGA - not HDMI - so the listing was innaccurate. Pi will not feed a VGA monitor - it outputs only composite video (CSV) or HDMI. The second smaller unit is CSV and can be fed from the Pi RCA output. I have the same unit and it works fine from the Pi, although the text is small. Hope this helps.