I just found this: http://au.element14.com/raspberry-pi/raspbrry-modb-512m/sbc-raspberry-pi-model-b-512mb/dp/2191863
Is this a raspberry pi with 512Mb RAM or is this a joke.
I just found this: http://au.element14.com/raspberry-pi/raspbrry-modb-512m/sbc-raspberry-pi-model-b-512mb/dp/2191863
Is this a raspberry pi with 512Mb RAM or is this a joke.
Now it's official. A 512MB Pi, and we certainly as more often than not heard it here first.
Thank you all deep miners of the Pi caverns to keep us all on the forefront of knowledge.
Ray
P.S. Dear Distro maintainers please do not suddenly make all your Pi OS distros twice as big and only suitable for the larger memory machines.
Ray Hughes wrote:
Now it's official. A 512MB Pi, and we certainly as more often than not heard it here first.
Thank you all deep miners of the Pi caverns to keep us all on the forefront of knowledge.
Ray
P.S. Dear Distro maintainers please do not suddenly make all your Pi OS distros twice as big and only suitable for the larger memory machines.
Pretty sure that the people here had no more idea that a 512 was imminently on the way than anywhere else. Lots of people predicting it eventually (well, obvious it was going to happen at some point), but not sure anyone predicted it so soon. Anyone can make Pi in the the sky predictions, its getting the timing right that's the important bit, and I don't reckon anyone saw this one coming so soon.
Making a distro twice as 'big' doesn't mean you need twice the memory - the kernel stays the same size (within reason) on any platform. Linux uses swap, so lower memory system will still work, but slower.
Bill.
Billy Thornton wrote:
Pretty sure that the people here had no more idea that a 512 was imminently on the way than anywhere else. Lots of people predicting it eventually (well, obvious it was going to happen at some point), but not sure anyone predicted it so soon. Anyone can make Pi in the the sky predictions, its getting the timing right that's the important bit, and I don't reckon anyone saw this one coming so soon.
Bill.
Fegus started this thread on 02-Sep-2012, based on evidence he had found on the Australian site. I don't think this counts as a pie in the sky prediction?
So your claiming an accidental website entry as evidence? Did he predict when? Like I said, any one could have predicted there was going to be a 512 version -I saw posts on the other forum well before September about that. No-one predicted when. Just do a seach on 512MB - mentioned all over the place. Everyone assumed it was coming, no-one knew when. I read somewhere over there that these things have been in production since the move to Wales manufacturing so obviously planned for some time. They still managed to keep it mostly secret, to keep Osbourne happy! That pretty cool!
My prediction now; there will never be a 1GB version. You heard it here first! (Citation : no one makes 1GB ddr2 PoP ram, and its an old technology, so no-one ever will).
Bill
So it looks like there are already instructions on how to configure the Pi to make use of the extra memory over on the RasPi forum.
Now I just need the Pi to arrive :-)
One of my old ones will be consigned as a permanent Air print server - any thoughts on where the 512 Meg version will most show improvement over the 256 Meg version ?
Steve, I would guess the most improvement would be in multitasking. Say a multi-user webserver. In 'normal use', though, I'd expect X windows to improve markedly with multiple windows.
Overall video performance is likely to improve also as at the moment the memory allocation has to be played with to get the balance right.
jamodio wrote:
Instead being a moron contesting anything that anybody says (starting with your useless comment about version numbers,) you should do more due diligence about what is going on, and who is working on what. It was not difficult to envision that sooner or later the Rpi was going to have 512MB RAM since RPF was already working and testing preliminary images of Android 4.0.
BTW, your citation and assumed authoritative answer from one of the moderators on the RPi forum is not valid ...
http://omapworld.com/4430_8Gb__DDR_PoP_111_1003122.pdf
I don't know what is your mission here but so far the only thing you are contributing is noise and additional fuel for flame wars.
Actually, forgot to ask something here - despite your inability to be polite, what's Android got to do with 512MB, and I don't remember talking about version numbers- what's up there dude?
My mission? To provide an antidote to the bitter vitriol and bile spouting from some of the posters on this site, who have an over exagerated sense of thier own importance, just 'cos they got banned from the other one. or something like that. Don't actually have a official mission statement, so I make it up as I go along. And it's the middle of the night, I'm tired aftyer working 14 hours straight, so it might change at short notice.
jamodio wrote:
Well you are failing in your mission and even if you were in front of my face I'll still call you a moron, I don't feel the need to be polite with people like you that seems to have every intent to create flame wars.
Good luck with that. Next time you are in the Far East give me a shout.
ps. See my previous comment.
Since my original reply stating that the 1GB ram package quoted by Jamodio has been deleted, presumably because he didnt like to be shown to be wrong, I'll reiterate. That package will not work on a Raspberry Pi. It's the right physical size, and the right sort of DDR2, but it's interface is different and it has a different number of balls in its BGA array to find on the Raspberry Pi SoC. I leave it as an exercise for the reader to compare the datasheet with those of the current 256 RAM chips used on the Rasberry Pi for the exact reason.
I didn't delete anything and BTW my reply to you was also deleted. I never said that that particular part would work with the RPi, just a proof that somebody out there is actually working on 1GB DDR2 PoP memory.
jamodio wrote:
I didn't delete anything and BTW my reply to you was also deleted. I never said that that particular part would work with the RPi, just a proof that somebody out there is actually working on 1GB DDR2 PoP memory.
You certainly implied it. Although I have realised that in my posts I omitted to say there I was refereing to the Raspberry Pi SoC, not 1Gb Pop in general. I just assuemd that's what we were talking about. Sorry for not being clear - there are quite a few 1GB PoP already out there in devices being sold - but none that fit on the 2835, and none, as far as I know, in the pipeline. It's old tech, and modern SoC have more channels and more chip selects, so that pipline ain't gonna be filled up.