Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Is this the first Pi supercomputer ?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 708 subscribers
  • Views 907 views
  • Users 0 members are here
  • raspberry_pi
Related

Is this the first Pi supercomputer ?

mgt6910
mgt6910 over 13 years ago

 

http://arstechnica.com/information-technology/2012/09/university-builds-cheap-supercomputer-with-raspberry-pi-and-legos/

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    Virginia Polytechnic University in the U.S. made, the cheapest supercomputer to date (in 2000) using a few handfuls of powermac g4's. I think it was the third or fourth fastest supercomputer at the time, at a small fraction of the cost

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mgt6910
    mgt6910 over 13 years ago in reply to e14 Contributor

    With reference to the Virginia Polytechnic system,the lead designer says " With dual 64-bit, 2.3GHz G5 processors in each of its 1,100 Xserve G5 units, the new cluster operates at 12.25 teraflops".

     

    Is there some confusion betwen clusters and supercomputers ?

     

    (See http://www.apple.com/science/profiles/vatech2/)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • mgt6910
    mgt6910 over 13 years ago in reply to e14 Contributor

    With reference to the Virginia Polytechnic system,the lead designer says " With dual 64-bit, 2.3GHz G5 processors in each of its 1,100 Xserve G5 units, the new cluster operates at 12.25 teraflops".

     

    Is there some confusion betwen clusters and supercomputers ?

     

    (See http://www.apple.com/science/profiles/vatech2/)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to mgt6910

    > Is there some confusion betwen clusters and supercomputers ?

     

    Wikipedia defines a supercomputer as:

     

    "A supercomputer is a computer at the frontline of current processing capacity, particularly speed of calculation." http://en.wikipedia.org/wiki/Supercomputer

     

    The Virginia Polytechnic system was ranked #3 on the list of the world's

    top 500 supercomputers in 2003, #7 in 2004, #14 in 2005 with a rating of

    12.25 teraflops, and #280 in 2008, so there's no ambiguity there.

     

    In contrast, the Pi cluster has no FLOPS rating, no high-speed

    interconnect, and a very small ram, and is clearly not at the frontline of

    current processing capacity.   So no ambiguity there either.

     

    The benchmark that was run to calculate pi is designed to show

    the speedup from running multiple nodes in parallel, but they only

    showed it running on two nodes, and deleted the timing information.

    The RPi has been measured at about 40MFLOPS under Raspbian,

    so a two-node RPi cluster is clearly not a supercomputer.

     

    For teaching purposes, with the budget they used, they actually could

    have made an instructional cluster that also had impressive performance,

    but not with RPi's.