Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum model a usb expansion
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 707 subscribers
  • Views 1069 views
  • Users 0 members are here
  • raspberry_pi
Related

model a usb expansion

e14 Contributor
e14 Contributor over 13 years ago

Can anyone tell me if the model a lacks the controller for more than one usb port or if it simply lacks the port itself? I would like to integrate a wireless card into a pi. I don't think it would be too difficult to crack open a small wireless n usb adapter and permanently attach its insides to the usb tx and rx lines while attaching the power leads directly to the power inlet connector.

 

It looks pretty silly to have an entire usb hub hanging off just to attach a wireless adapter.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    Brandon,

      The model A, if and when it appears, is expected to lack

    the controller chip, the 2nd usb port, and the ethernet jack.

    If you are using a hub just to power the wifi, then you might

    be able to plug that directly into one of the recent model B's,

    either the recent rev 1.0 ones with 0 ohm resistors in place of

    the USB polyfuses, or the rev 2.0 ones.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 13 years ago in reply to e14 Contributor

    With the new F1 and F2 fuses in place (or not - as be the case in rev2), does that mean that the new maximum draw for the USB port is 500mA (the rating of the tracks)?

     

    And that would mean that you could power any usb device provided that it would not draw above 500mA? (for model A)

     

    On model B it would be 1000mA - 700mA = 300mA, the maximum current availble through the 1.1A capacitor/provided by the power supply.

     

    Could you confirm this?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • wallarug
    wallarug over 13 years ago in reply to e14 Contributor

    With the new F1 and F2 fuses in place (or not - as be the case in rev2), does that mean that the new maximum draw for the USB port is 500mA (the rating of the tracks)?

     

    And that would mean that you could power any usb device provided that it would not draw above 500mA? (for model A)

     

    On model B it would be 1000mA - 700mA = 300mA, the maximum current availble through the 1.1A capacitor/provided by the power supply.

     

    Could you confirm this?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to wallarug

    I don't think there is any hard and fast 500mA limit on the tracks.

    I think both the model A and B have a 700mA polyfuse connected

    to the microusb input, so you would be limited by that, unless you

    use an alternate source of power, such as the GPIO pins, which

    bypass the 700mA polyfuse.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 13 years ago in reply to e14 Contributor

    I think both the model A and B have a 700mA polyfuse connected

    I thought that that was a 1.1A polyfuse. ??

    John Beetem wrote:

    ...you are limited to 1A by polyfuse F3...

                                  on a differnet thread. http://www.element14.com/community/thread/19819?tstart=0

    I will look into powering though GPIO pins.  This sounds like a good idea for a portable application.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 13 years ago in reply to wallarug

    Fergus Byrne wrote:

     

    I think both the model A and B have a 700mA polyfuse connected

    I thought that that was a 1.1A polyfuse. ??

    John Beetem wrote:

    ...you are limited to 1A by polyfuse F3...

    According to the RasPi 1.0 schematic, F3 is 1.1A.  This is one of the standard sizes offered by the Littelfuse 2016L series, which I would guess is a possible vendor for F3.  OTOH, we don't know what part is actually is populated on a given board, and I don't think we've ever seen a formal bill of materials (BOM) for RasPi with approved vendors.

     

    Assuming F3 is indeed 1.1A and the RasPi SoC + P1 consume no more than 500 mA, that leaves you 500 mA for a wireless dongle with 100 mA margin.  However, the micro USB cable and F3 both have resistance so as you draw more current through them RasPi's 5V0 voltage may drop to the point that your HDMI and/or USB device(s) become sad.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to johnbeetem

    There is a lot of confusion about F3.  I think the 700mA (or in some cases

    750mA) comes from the marking on the actual fuse.  Apparently 700mA

    is the "hold" current, and 1.1mA is the "trip" current, where the fuse starts

    to heat up somewhere between the hold and the trip.  So you wouldn't want

    to use more than the hold current.

     

    http://www.raspberrypi.org/phpBB3/viewtopic.php?f=2&t=5068&start=22

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 13 years ago in reply to e14 Contributor

    coder27 wrote:

     

    There is a lot of confusion about F3.  I think the 700mA (or in some cases

    750mA) comes from the marking on the actual fuse.  Apparently 700mA

    is the "hold" current, and 1.1mA is the "trip" current, where the fuse starts

    to heat up somewhere between the hold and the trip.  So you wouldn't want

    to use more than the hold current.

     

    http://www.raspberrypi.org/phpBB3/viewtopic.php?f=2&t=5068&start=22

    Yes, this sounds right.  It would really help things if RasPi would list a BOM.