Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Interesting "Competitors" for the Raspberry Pi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 196 replies
  • Subscribers 716 subscribers
  • Views 25078 views
  • Users 0 members are here
  • single_board_computer
  • single_board_computers
  • raspberry_pi
Related

Interesting "Competitors" for the Raspberry Pi

wallarug
wallarug over 13 years ago

It is interesting to see what people are comparing to the "An ARM GNU/Linux box for $25. Take a byte!" to these days.

 

http://arstechnica.com/information-technology/2012/09/99-raspberry-pi-sized-supercomputer-touted-in-kickstarter-project/

This article is talking about a $99 dollar supercomputer that has 16 cores @ 700MHz each.

 

http://www.electronicsweekly.com/Articles/28/09/2012/54676/raspberry-pi-gets-a-competitor.htm

This article is about an ARM board, not that different to the Raspberry Pi but with more power and RAM.

  • Sign in to reply
  • Cancel
Parents
  • GregC
    GregC over 13 years ago

    Hello

    Have you heard about the Sabre-Lite board based on a Freescale i.MX6Q (Cortex-A9, Quad-Core, 1GHz) ?

    i.MX6 is really a powerfull processor considering its 4x Cores @1GHz, its Graphical Unit Vivante for 2/3D, its Video Unit allowing 1080p multi-Encoding/Decoding and its Image Unit for multi-camera input/display outputs.

    The IC was announced few months before but the launch is imminent (November 15th during Electronica) with samples available.

    Sabre-Lite will be sold (with an aggressive resale price) and supported by Element14.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jamodio
    jamodio over 13 years ago in reply to GregC

    I've seen it, but $199 will be too high for my pocket.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to jamodio

    ouch for $200 I'd rather go all the way and just do a full fledge computer using a pico-itx board.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to jamodio

    ouch for $200 I'd rather go all the way and just do a full fledge computer using a pico-itx board.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • GregC
    GregC over 13 years ago in reply to e14 Contributor

    Jim, I understand your position.

    Just keep in mind that board will come with i.MX6 will be in Quad Core version @1GHz with a dedicated VPU for multi-video decoding and encoding capabilities up to 1080p or 3D HD, 1GB of DDR3, a camera input and up to 3x video output (1x HDMI, 1x LVDS and 1x Parallele)

    In terme of multimedia performances, i.MX6Q might outperform the NVidia Tegra3 with its dedicated Video Processing Unit.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to GregC

    First off, it having an LVDS is pretty awesome, I keep hoping (probably in vain) that the Pi will either get an LVDS or someone will make an interface for it using something like the DSI bus.

     

    That said, I don't mean to discourage anyone else from getting the board.  I think these ARM based boards are quite amazing, but for me graphics and camera input aren't high priorities so if I'm going to dish out the extra cash it's going to be for significantly more processing power, or a lot more RAM.  For me, personally, there's also a limit where ARM compatibility with some obscure piece of software hit a price ceiling I'm not willing to go past.  Shoot, if it weren't for the support that exists for the Pi in the 2 forums, I probably wouldn't have gotten a pi.

     

    But that's why they make more than one flavour of tea, right?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to GregC

    Greg C wrote:

     

    Jim, I understand your position.

    Just keep in mind that board will come with i.MX6 will be in Quad Core version @1GHz with a dedicated VPU for multi-video decoding and encoding capabilities up to 1080p or 3D HD, 1GB of DDR3, a camera input and up to 3x video output (1x HDMI, 1x LVDS and 1x Parallele)

    In terme of multimedia performances, i.MX6Q might outperform the NVidia Tegra3 with its dedicated Video Processing Unit.

    All in all, looks like a nice board and the i.MX6 series certainly look as if they'll provide a good starting point for some interesting boards. But onto the akward questions.. 

     

    Accelerated X drivers ? (no point in a fancy VPU if you can't use it for more than a dumb frame buffer).

    Why only 1GB ?

    Where's the mainline kernel integration effort ? Or is it stuck at 3.0.x ? (even the Pi manages 3.2.x and realistically you want 3.4+ with devicetree)

     

    Realistically, outperforming the Tegra3 only matters if there's actually a useable accelerated 3D driver. Nvidia will likely have a closed binary blob of a driver for the Tegra, but if it works....