Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Interesting "Competitors" for the Raspberry Pi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 196 replies
  • Subscribers 715 subscribers
  • Views 24748 views
  • Users 0 members are here
  • single_board_computer
  • single_board_computers
  • raspberry_pi
Related

Interesting "Competitors" for the Raspberry Pi

wallarug
wallarug over 13 years ago

It is interesting to see what people are comparing to the "An ARM GNU/Linux box for $25. Take a byte!" to these days.

 

http://arstechnica.com/information-technology/2012/09/99-raspberry-pi-sized-supercomputer-touted-in-kickstarter-project/

This article is talking about a $99 dollar supercomputer that has 16 cores @ 700MHz each.

 

http://www.electronicsweekly.com/Articles/28/09/2012/54676/raspberry-pi-gets-a-competitor.htm

This article is about an ARM board, not that different to the Raspberry Pi but with more power and RAM.

  • Sign in to reply
  • Cancel
Parents
  • jamodio
    jamodio over 13 years ago

    The parallela sounds and looks cool but we are talking about a major project that includes sillicon rebake and that probably is 6-12months away from mass production.

     

    Meanwhile while there are other developments that are not exactly comparable to the R-Pi, they are slowly but steady making progress, like the OLinuXino boards from Olimex. I'm testing both the micro and maxi using the Freescale iMX233 application processor SoC (fully documented by the way,) waiting for the A13 one and they also have under development one using the A10. The iMX233 Maxi uses also the LAN9512 and I didn't find any issues with it yet (and BTW the connectors are properly aligned and it has a nice swtiching power supply, the board is slightly bigger than the R-pi, no HDMI/VGA tough.)

     

    I also recently got a TI AM335x Starter Kit, you will start to see more stuff based on the AM335x and TI will get more agressive to dettach the OMAP from some applications and put it on boards similar to the R-Pi.

     

    Still the R-pi continues to be a good idea, unfortunatelly with an associated plan badly executed and with more focus on hype and promotion than really make it a strong and solid "product" with the participation of a community that is eager and able to contribute.

     

    No schematics, no Gerbers, major concern is "cloning" .... I'd not clone something that is not working properly ...

     

    -J

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to jamodio

    At least it looks like Olimex is taking the problems from people using their boards seriously.

    Their Forum is an example of what a forum should be like.

     

    The supply dip when you connect an usb device is a known fact. It might be hard to notice it on a scope, unless you have a good memory scope and are able to trigger it properly. The issue happens more frequently on the newer boards with the usb polyfuses removed. If you look at the Pi schematics, there aren't much buffer capacitors on the 5V supply rail. (just 1 small capacitor). I guess we get what we payed for.

    It looks like a lot of the Pi usb issues are caused by timing.

    As linux isn't a real time OS, and as stated before that the cpu can become heavy loaded, I doubt they will ever be able to fully fix the issue.

    Besides the usb, there are other dissapointing things. One mentionned already is the fact that X11 isn't hardware accelerated.

    Another one is the poor quality of the analog audio output. A third one is the fact that you need to properly shutdown the system to avoid sd card corruption. This makes it difficult to use the Pi as an embedded solution. A fourth one is the critical power requirement of the board.

    Some of those can be resolved, but all solutions make your cheap solution (not so cheap) anymore.

    I know it's a little off topic, but these points are worth checking when seeking for "Competitors" and might rectify a higher price.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to GeorgeIoak

    Looks interesting, the iMX6 series of SoC holds promise. I continually wonder about the compromises though - why do I have to buy useless (to me) wifi and bluetooth in order to get dual core and 1Gb ram ?

     

    I see from their google group that someone has already asked the 'accelerated X ?' question, I wonder if he has an RPi image

     

    So $69, but what isn't really clear is whether that includes the 'interface board' or if the interface board is a seperate $150 item.

     

    Also at 314 pins I expect the unspecified 'EDM' connector is going to be fairly fine pitch.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jamodio
    jamodio over 13 years ago in reply to e14 Contributor

    The iMX6 will be quite an interesting series of SoC, among other things integrated 1Gbps Ethernet and 3Gbps SATA, etc.

    Expect other boards starting to pop up here and there.

     

    -J

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 13 years ago in reply to GeorgeIoak

    George Ioakimedes wrote:

     

    Hey Everyone, I just saw this, http://wandboard.org, at first glance it's looking pretty good but I haven't read the details...

    Shipping at end of November 2012 and they don't have photos of prototype boards?  Not a good sign IMO.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jamodio
    jamodio over 13 years ago in reply to johnbeetem

    Well we had plenty of photos of the Raspberry Pi, even X-Rays, and it took them some time to start shipping.

     

    -J

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jamodio
    jamodio over 13 years ago in reply to johnbeetem

    FYI, one of the producers of EDM modules ... Most probably the wanboard will be just another "mainboard" for the compact modules.

     

    http://www.technexion.com/index.php/products/edm/compact/edm-cf-imx6

     

    -J

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to morgaine

    Earlier in this thread I mentioned that if you're intending to create an open board, it is helpful if you can encourage an ecosystem to develop around it so that the concept doesn't wither and die through disinterest, and that one way of achieving this is by riding on the backs of existing open hardware companies so that you are broadening the audience for their product lines.  They often like that, and it may even result in some direct support for your cause.

     

    I mention this because on Olimex's blog I found this recent post which describes their very inexpensive MOD-IO2, an "Input Output expandable board with UEXT".  This nice stackable design is the kind of approach to I/O  that I think should feature in all open hardware ARM boards, since its inherent expandability would allow a single community board to address a very diverse range of requirements that naturally appear in a large community.

     

    Indeed, any computer board is made more flexible when it features a generic I/O connector, as Olimex described in their reason for UEXT ,which covers I2C, SPI and RS232.  Without generic I/O, you would have to offer different computer boards for different I/O requirements, which makes little sense.  This is obviously preaching to the converted here, but while it's normal to have expandible I/O connectors on the PC, it's far less common in the ARM world, other than through user-level USB.

     

    I like what Olimex is doing in that area for microcontrollers, and it's very notable that they are continuing that flexible I/O concept on their application processor boards as well:  their A13-OLinuXino-WIFI-DEV features a UEXT connector.

     

    Among application processor boards, TI's BeagleBone and Olimex's A13-OLinuXino seem to be in the lead for good I/O design.

     

    Morgaine.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jamodio
    jamodio over 13 years ago in reply to morgaine

    So far I'm happy with some of the tests using the iMX233 OLinuXino Maxi and Micro. I just added the headers to the Micro to set it on a protoboard, I'll post some pics later. Wating for the A13 that is expected to start shipping around Oct 20, and they are already testing the first prototypes for an A10 based board.

     

    Not doing much yet with the iMX233 boards, just making sure the basic stuff works, that they don't crash, the Arch Linux images still need some work.

     

    I agee with your assesment that BeagleBone and the OLinuXino have good I/O design.

     

    -J

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • GeorgeIoak
    GeorgeIoak over 13 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    I mention this because on Olimex's blog I found this recent post which describes their very inexpensive MOD-IO2, an "Input Output expandable board with UEXT".  This nice stackable design is the kind of approach to I/O  that I think should feature in all open hardware ARM boards, since its inherent expandability would allow a single community board to address a very diverse range of requirements that naturally appear in a large community.

     

    Indeed, any computer board is made more flexible when it features a generic I/O connector, as Olimex noted here as their reason for UEXT ,which covers I2C, SPI and RS232.  Without generic I/O, you would have to offer different computer boards for different I/O requirements, which makes little sense.  This is obviously preaching to the converted here, but while it's normal to have expandible I/O connectors on the PC, it's far less common in the ARM world other than through user-level USB.

     

    I like what Olimex is doing in that area for microcontrollers, and it's very notable that they are continuing that flexible I/O concept on their application processor boards as well:  their A13-OLinuXino-WIFI-DEV features a UEXT connector.

     

    Among application processor boards, TI's BeagleBone and Olimex's A13-OLinuXino seem to be in the lead for good I/O design.

     

    Morgaine.

     

    That looks similar to Digilent's (sp?) module. I think you need something a little more generic with more I/O defined on the interface. Then the bigger issue comes in getting a driver written and supported. If that could be done then you are really talking about something that would be useful for all of us.

     

    I'm not worried about not seeing any pictures of boards from Freescale because we're talking about a "major" company with the funds and engineers to get things done. What Olimex is doing looks very promising too but I don't think they've been around as long as Freescale. If I had to sum up what I'm looking for it would be an embedded board with the processing power of a computer (i.e. dual core Arm), community supported OS and drivers, and the flexibility of an embedded board that provides direct access to GPIO and buses.

     

    It seems that almost all of the current boards are leveraging off of the mobile phone markets and that ends up limiting the flexibilty

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to GeorgeIoak

    Sounds good, but put a microcontroller on the board alongside the applications processor.  Except for the most trivial of slow-speed applications, expecting Linux to handle low-level I/O without high response latency and jitter is a design mistake.

     

    Microcontrollers cost next to nothing.  Use one, or indeed several.  The Linux kernel has better things to do.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 13 years ago in reply to GeorgeIoak

    George Ioakimedes wrote:

     

    I'm not worried about not seeing any pictures of boards from Freescale because we're talking about a "major" company with the funds and engineers to get things done.

    I wouldn't be worried about a Freescale board other than Freescale's habitual tardiness in delivering new ICs, a tradition they inherited from Motorola.  But I haven't seen any indication that Wandboard has any official relationship with Freescale other than as a customer for Freescale ICs.  For example, if I do a search at https://community.freescale.com for "Wandboard" I get no results.  (Plenty of results for i.MX6 Sabre.)  Just sayin'.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • johnbeetem
    johnbeetem over 13 years ago in reply to GeorgeIoak

    George Ioakimedes wrote:

     

    I'm not worried about not seeing any pictures of boards from Freescale because we're talking about a "major" company with the funds and engineers to get things done.

    I wouldn't be worried about a Freescale board other than Freescale's habitual tardiness in delivering new ICs, a tradition they inherited from Motorola.  But I haven't seen any indication that Wandboard has any official relationship with Freescale other than as a customer for Freescale ICs.  For example, if I do a search at https://community.freescale.com for "Wandboard" I get no results.  (Plenty of results for i.MX6 Sabre.)  Just sayin'.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • jamodio
    jamodio over 13 years ago in reply to johnbeetem

    The Wandboard is not a child of Freescale. Check the company I posted the link before ...

     

    And if you are smart enough and a good observer you will notice the names of the other main boards they produce: fairy, elf, druid, seer, wizard ...

     

     

    -J

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • GeorgeIoak
    GeorgeIoak over 13 years ago in reply to jamodio

    Yeah, I just noticed that this wasn't a Freescale project, in fact I can't even find any company name on that Wandboard web site which is odd...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to GeorgeIoak

    I just posted this link in another mega-conversation about clusters, but also thought it might be appropriate to the conversation at hand here:

     

    http://www.kickstarter.com/projects/adapteva/parallella-a-supercomputer-for-everyone?ref=category

     

    Neil.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jamodio
    jamodio over 13 years ago in reply to e14 Contributor

    I think we mentioned Adapteva's Parallela before, it really looks promising. I'm glad they god funded (I'm a backer) at kickstarter, I exchange few messages with Andreas and they released more documentation and demos through the funding period.

     

    Looking forward to see how they execute and the Parallela board comes out next year.

     

    Similar to Kickstarter I recently contributed to cubieboard on indiegogo http://www.indiegogo.com/cubieboard?a=1678910

     

    I did register for the Wandboard but didn't get any confirmation yet, on their blog they posted that the first batch of validation samples last week. http://www.wandboard.org/index.php/blog

     

    And there are several others on the works, so we'll have plenty of ARM based boards to play with under the $100 price mark and I'm not sure we can compare some of the vis-a-vis with the Rpi.

     

    I'm putting together a table, but there is already an interesting one on-line with the same idea

    http://socialcompare.com/en/comparison/low-cost-arm-boards

     

    -J

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to jamodio

    Yeah, my bad, I went back a few pages and realized I was late to the party... :-)

     

    N.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 13 years ago in reply to jamodio

    jamodio wrote:

     

    I did register for the Wandboard but didn't get any confirmation yet, on their blog they posted that the first batch of validation samples last week. http://www.wandboard.org/index.php/blog

    Thank you for posting the Wandboard link.  Impressive that they can price the two boards at US$69 solo and US$89 dual for the two-board sandwich.  I'll be watching that one.

     

    You know, I keep reading Wandboard as Wandaboard, as in "a board called Wanda".  Probably just me -- I once named a board Wamba after the court jester in Ivanhoe.  His full name: "Wamba, son of Witless".

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jamodio
    jamodio over 13 years ago in reply to johnbeetem

    My pleasure. It also happens to me all the time, but if you checked the link I posted some time ago ( http://www.technexion.com/index.php/products/edm/compact/edm-cf-imx6 ) looks like these guys like to brand their base boards with names related to magic (Fairy, Elf, Druid, Seer, Wizard ...) so Wand makes sense and it looks like a new addition to their product portfolio.

     

    Yup, pricing looks very aggresive for the amount of stuff that they have on both boards looking at the pictures.

     

    I didn't check if Freescale released to the public additional info iMX6 yet, as far as I remember these guys are planning to release more documentation as soon as Freescale opens the door. Meanwhile you can take a peak a the Gerber plots for both boards and expansion pinouts, very large and nice number of GPIOs and interfaces to play with.

     

    -J

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to johnbeetem

    John Beetem wrote:

     

    I wouldn't be worried about a Freescale board other than Freescale's habitual tardiness in delivering new ICs, a tradition they inherited from Motorola.

     

    On past precedent, how are Freescale on the documentation front?  I've never looked closely at Freescale's publications record in this area (nor Motorola's), but I always prefer to back companies that embrace open documentation and support the open software movement.

     

    It would be wonderful if i.MX6 turns out to be friendly to the open hardware/software community.  I'm greatly looking forward to the date of official release when the NDAs are dropped.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 13 years ago in reply to morgaine

    It's been a while (ColdFire days) since I've had to look into their documentation, but personally I think they always had quite good documentation, such as for their DSP chips. And they have a forum, so that's a good thing. For their other processors, the CodeWarrior IDE and compiler was quite nice (but again my information is quite old), but was not free unfortunately (nowadays they have free code-size-restricted versions,

    so that is very good). Of course, for ARM we have gcc however.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • GeorgeIoak
    GeorgeIoak over 13 years ago in reply to morgaine

    I started looking into the i.MX6 a little more today and am becoming more and more interested in it. Enough that I'm considering taking up our suggestions and trying to create the board we all want. Before I go much further in this quest though I wanted to see if anyone knew of someone already working on this. I'd hate to put the time and effort in this only to be outdown by someone else with a larger team to tackle this. I have all the means to design and build but I'm by no means a software guru.

     

    Thoughts?