On May 11, 2012, SImon initially wrote:
"One thing to bear in mind is that if I reply [replace] all my acceleration hooks with no-ops, working with things like gedit and gtkperf still aren't super fast. I have a feeling that system bottlenecks may lie elsewhere."
http://www.raspberrypi.org/phpBB3/viewtopic.php?f=63&t=4649&start=58
On October 05, 2012, he confirmed his initial findings:
> b. acceleration is working
"Yes. However in the process of writing this, I've discovered that X is rarely the bottleneck. Since I doubt people will believe me I've added a mode where X runs as absolutely fast as possible (the display is completely corrupt) but you can still make out how slow the actual applications are functioning through the corruption."
http://www.raspberrypi.org/phpBB3/viewtopic.php?f=63&t=4649&start=190