Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Does config.txt do anything?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 710 subscribers
  • Views 2207 views
  • Users 0 members are here
  • raspberry_pi
Related

Does config.txt do anything?

cityswift
cityswift over 13 years ago

Since I received my Pi 2 months ago I have been trying at intervals to get a decent display on my 15" LCD monitor on CVS. The screen is 4:3 and is 1024*768 pixels and the display I get is 14:9 with a black border at top and bottom and is a few pixels too wide.

 

I can succesfully edit  config.txt, except for  the overscan which does not accept a negative number such as -20, but when I reboot the picture is just the same. Can anyone help?

 

On HDMI the picture is fine.

 

I am perservering because the Pi is a tool with great potential and spending a few months getting to really make it hum will be time well spent.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    Hi CitySwift. Its good that you are continuing to learn with your Pi.

     

    This link should give all the information you need to sort out the overscan on your monitor.

     

    http://elinux.org/RPi_config.txt

     

    Don't forget to use sudo nano /boot/config.txt or you wont be able to save the changes. ( or insert your text editor instead of nano)

     

    Good luck

    Ray

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • GreenYamo
    GreenYamo over 13 years ago in reply to e14 Contributor

    Hello Cityswift, I have a vague feeling that Config.txt only works for HDMI connections, hopefully someone will be along with a better memory than me to confirm or otherwise.

    Ray also makes a great point about making sure you use Sudo. I tried Vi once but still bear the scars, I'd stick with Nano :-)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • cityswift
    cityswift over 13 years ago in reply to GreenYamo

    Hi Steve  I am using nano as Ray suggests and have no trouble with it. I am beginning to think you are right about config.txt only working on HDMI as the CVS is an analogue signal - but surely this point would be made somewhere in the many RPi dialogues and tutorials?  imageimage

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 13 years ago in reply to cityswift

    According to the RasPi wiki, config.txt does have settings for composite video.   I've never used RasPi composite video -- I find the RCA jack makes a dandy alignment peg for vertically mounting RasPi to improve air flow.  The wiki says that the default settings are "sdtv_mode=0" (Normal NTSC) and "sdtv_aspect=1" (4:3).  I assume you have your monitor set to the correct aspect ratio.  You probably want postive values for "overscan_left" and "overscan_right" to compensate for overscan, or else just adjust the monitor's own settings.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • johnbeetem
    johnbeetem over 13 years ago in reply to cityswift

    According to the RasPi wiki, config.txt does have settings for composite video.   I've never used RasPi composite video -- I find the RCA jack makes a dandy alignment peg for vertically mounting RasPi to improve air flow.  The wiki says that the default settings are "sdtv_mode=0" (Normal NTSC) and "sdtv_aspect=1" (4:3).  I assume you have your monitor set to the correct aspect ratio.  You probably want postive values for "overscan_left" and "overscan_right" to compensate for overscan, or else just adjust the monitor's own settings.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • cityswift
    cityswift over 13 years ago in reply to johnbeetem

    Hi John thanks for that link as I managed to get the answer from a link it contained.

     

    What the RPi config.txt file DOES NOT SAY at its start is that the # symbol has to be removed from the front of any function which you want to use. I have now got the screen size and position exactly as I want it but the text is size is too small for easy reading and I wondered if there is any way to increase it by reducing the number of lines on the screen?

     

    Cancel that - the answer is  http://elinux.org/RPi_Command_line_font_size