Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum USB update from Gordon, new direction
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 17 replies
  • Subscribers 708 subscribers
  • Views 1858 views
  • Users 0 members are here
Related

USB update from Gordon, new direction

e14 Contributor
e14 Contributor over 13 years ago

"Unfortunately I've been unable to create a more credible improvement for the USB issues we currently have. Improvements to latency actually have a detrimetal effect to some types of transport (split transactions) which isn't going to be fixed any time soon.

 

So instead I've been spending a little time horsing around with the EHCI interface to see if I can create a software implementation of the EHCI host interface for the DWC_OTG hardware, this would solve our problems because then we can push this code onto the VPU which has a very low interrupt latency and interrupt overhead.

 

But unfortunately it is going to take time and I could probably do with some volunteers to help do the EHCI interface. I'm hoping to get a simple one in place first (that works with most simple transactions) then people can begin helping in the spirit of open software!"

 

http://www.raspberrypi.org/phpBB3/viewtopic.php?f=28&t=12097&start=556

  • Sign in to reply
  • Cancel
Parents
  • jamodio
    jamodio over 13 years ago

    USB will work when they find the formula to create milk out of a rock. I believe I mentioned it long time ago, but the piece of IP that Broacdom got from Synopsys for the BCM2835 is an implementation of USB OTG, it will be very challenging to pretend make it work as a full featured USB HOST.

     

    Can you do some workaround to get some limited functionality working properly for some devices, probably yes, but it will never reach Eben's promise that you can do with the Pi what you can do with any other computer, that has been a misleading statement since day way as it is the permanent tag message on the Blog header.

     

    Still the Rpi is a cool gadget to thinker with Linux.

     

    -J

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to jamodio

    jamodio wrote:

     

    ...Still the Rpi is a cool gadget to thinker with Linux.

     

    -J

     

    I would venture to say that ~most~ people don't have a computer in order just to "tinker" with it's operating system - although some of us will doubtless have spent far too much time poking about in the innards because something doesn't work, or just out of curiosity... image

     

    Nope, for most a computer is a box for doing stuff - interfacing with a sensor, browsing, coding, playing media, writing that novel and all the other wonderful / mundane things. "Tinkering is fine, so long as it's not compulsory!" It shouldn't be compulsory either - not everyone wants to be a dentist, or a lion tamer - even though they are doubtless noble professions.

     

    Ironically, for those folks that are keen on destruction testing an operating system then the best choice of hardware IMO is something absolutely bulletproof. Then, when the rainbow / blue screen / spinning beachball of abject misery appears one know's it's directly related to one's own input and not some random hardware / driver burp that one has no control over. That's why that with hindsight the original choice of Fedora for the Pi seems a bit ...umm... foolhardy. Beta hardware + alpha software = debugging purgatory.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jamodio
    jamodio over 13 years ago in reply to e14 Contributor

    Noticed that I said "gadget" not "computer" ...

     

    Jonathan Garrish wrote:

    Beta hardware + alpha software = debugging purgatory.

     

    Amen

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jamodio
    jamodio over 13 years ago in reply to e14 Contributor

    Noticed that I said "gadget" not "computer" ...

     

    Jonathan Garrish wrote:

    Beta hardware + alpha software = debugging purgatory.

     

    Amen

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to jamodio

    jamodio wrote:

     

    Noticed that I said "gadget" not "computer" ...

     

     

    Noted and understood!