Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum GPIO simple safe interface
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 705 subscribers
  • Views 431 views
  • Users 0 members are here
  • raspberry_pi
Related

GPIO simple safe interface

cityswift
cityswift over 13 years ago

With the gpio pins being so vulnerable:-

 

An input will fail if you apply 3.3v without any limiting resistor  -  an output if set at 1 will fail if shorted to gnd     - on output set at 0 will fail if you apply 3.3v without any limiting resistor

 

then I thought it worthwhile to set up safe insulated access to the pins as in attached pic. The pi is held in position with terminal blocks which are bolted to a piece of 4mm ply, and the connections are made to 3 @ 5A 12 way terminal blocks

(EBAY NO 150493789204)image

which are clearly labelled to reduce

errors and are also bolted to the ply. The connection to the blocks is made with a 26 way socket FARNELL NO 381-5730 and a ribbon cable.

  • Sign in to reply
  • Cancel
  • johnbeetem
    johnbeetem over 13 years ago

    Nice set of tentacles there.   You might want to see if they'll stock it at the HP Lovecraft Historical Society store: http://www.cthulhulives.org/store/store.lasso image