Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Open Source ARM Userland
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 31 replies
  • Subscribers 710 subscribers
  • Views 4729 views
  • Users 0 members are here
  • videocore
  • open_source
  • drivers
  • github
  • userland
  • raspberry_pi
  • gpu
  • news
Related

Open Source ARM Userland

jealderson1
jealderson1 over 13 years ago

It has been announced today on the Raspberry Pi site that the userland libraries have been made open-source. This makes the BCM2835 on the Raspberry Pi the "first ARM-based multimedia SoC with fully-functional, vendor-provided (as opposed to partial, reverse engineered) fully open-source drivers" (in the words of Alex Bradbury - the lead Linux developer at the Raspberry Pi foundation).

 

This should make life much easier for anyone looking to port different operating systems on to the Pi. With the GPU drivers opened up, it will mean that you can take advantage of the full hardware accelerated graphical capabilities of the BCM2835.

 

According to Alex, Broadcom are the first vendor of mobile phone SoCs to open up their drivers this way.

 

You can read the full announcement on RaspberryPi.org

 

Does this help anyone with their plans, or give them an idea? You can find the userland source on GitHub

 


  • Sign in to reply
  • Cancel
Parents
  • johnbeetem
    johnbeetem over 13 years ago

    I took a quick look at github but I didn't see any "doc" subdirectory.  Is there any documentation of the interface, or is it all a bunch of undocumented source code with unhelpful symbolic constants and function names?  I hope the former, but a comment at the RasPi 'blog post suggests it could be the latter.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 13 years ago in reply to johnbeetem

    John Beetem wrote:

     

    I took a quick look at github but I didn't see any "doc" subdirectory.  Is there any documentation of the interface, or is it all a bunch of undocumented source code with unhelpful symbolic constants and function names?  I hope the former, but a comment at the RasPi 'blog post suggests it could be the latter.

    Eben Upton answered my question at Slashdot:

    Eben Upton wrote:

     

    To help people get the most out of this, we hope to sponsor some efforts to formally document the interface exposed by the GPU over the next few months.

    Works for me.  I have plenty to do in the mean time.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to johnbeetem

    What's the point of documenting the GPU interface?  Are applications supposed to use the GPU interface now instead of using GL_ES?  Looking at the code, most of the functions are simple shims, so there would be no gain from bypassing them.

     

    https://github.com/raspberrypi/userland/blob/master/interface/khronos/glxx/glxx_client.c

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 13 years ago in reply to e14 Contributor

    free.quark wrote:

     

    What's the point of documenting the GPU interface?  Are applications supposed to use the GPU interface now instead of using GL_ES?  Looking at the code, most of the functions are simple shims, so there would be no gain from bypassing them.

     

    https://github.com/raspberrypi/userland/blob/master/interface/khronos/glxx/glxx_client.c

    It means you don't have to be running Linux (whether it's GNU/Linux, Android/Linux, MeeGo/Linux, ...) in order to use the GPU.  You can write a bare metal application that boots off an SD Card and talks to the GPU with binary calls.

     

    Running a mainframe operating system like GNU/Linux gives you lots of services, but it comes with lots of baggage.  There are times when you want an 18-wheel trunk but other times when you want a bicycle, and the extra wheels just get in the way.  An excellent example is a real-time application where the Linux scheduler could present problems.  Opening up the GPU interface gives you that flexibility.  JMO/YMMV

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to johnbeetem

    John Beetem wrote:

     

    free.quark wrote:

     

    What's the point of documenting the GPU interface?  Are applications supposed to use the GPU interface now instead of using GL_ES?  Looking at the code, most of the functions are simple shims, so there would be no gain from bypassing them.

     

    https://github.com/raspberrypi/userland/blob/master/interface/khronos/glxx/glxx_client.c

    It means you don't have to be running Linux (whether it's GNU/Linux, Android/Linux, MeeGo/Linux, ...) in order to use the GPU.  You can write a bare metal application that boots off an SD Card and talks to the GPU with binary calls.  ...

     

     

     

    I still don't understand.  Does linking with this shim pull in Linux modules?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 13 years ago in reply to e14 Contributor

    coder27 wrote:

     

    John Beetem wrote:

     

    free.quark wrote:

     

    What's the point of documenting the GPU interface?  Are applications supposed to use the GPU interface now instead of using GL_ES?  Looking at the code, most of the functions are simple shims, so there would be no gain from bypassing them.

     

    https://github.com/raspberrypi/userland/blob/master/interface/khronos/glxx/glxx_client.c

    It means you don't have to be running Linux (whether it's GNU/Linux, Android/Linux, MeeGo/Linux, ...) in order to use the GPU.  You can write a bare metal application that boots off an SD Card and talks to the GPU with binary calls.  ...

     

     

     

    I still don't understand.  Does linking with this shim pull in Linux modules?

    Here's my understanding: free.quark is saying that the newly-opened userland code is basically just a bunch of shims that take user-level OpenGL calls and convert them into binary messages which are sent to the GPU.  Without the open source and future documentation, it's hard to know what the message format is so you have to use the GNU/Linux modules.

     

    With the open source and future documentation, we should be able to find out how to pass these messages directly to the GPU without having to use GNU/Linux modules.  This permits non-Linux operating systems or bare metal programs to talk to the GPU.  They're still using the same OpenGL functions, but calling them with messages instead of function calls that prepare messages.  At least that's my understanding.

     

    If you're writing an OpenGL application for GNU/Linux, you might as well continue to use the GNU library and Linux driver.  You might be able to save some function call overhead by talking to the message interface directly, but it's probably not worth the trouble.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to johnbeetem

    There isn't really much of "message format".  The same parameters are passed in the same order,

    and RPC_CALL4 means there were 4 parameters.

     

    For example on line 488:

     

    GL_API void GL_APIENTRY glClearColor (GLclampf red, GLclampf green, GLclampf blue, GLclampf alpha)

    {  

        CLIENT_THREAD_STATE_T *thread = CLIENT_GET_THREAD_STATE();  

        if (IS_OPENGLES_11_OR_20(thread)) {     

             RPC_CALL4(glClearColor_impl,

                    thread,

                    GLCLEARCOLOR_ID,

                    RPC_FLOAT(red),              

                    RPC_FLOAT(green),               

                    RPC_FLOAT(blue),               

                    RPC_FLOAT(alpha));

            }

    }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    It could have some use under linux to figure out what functions are implemented.

    It's usefull for the development of other os, as they don't need the linux libraries anymore.

    But it's definite not like wow, we have a truly open hardware platform now.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Luc Cool wrote:

     

    It could have some use under linux to figure out what functions are implemented.

    It's usefull for the development of other os, as they don't need the linux libraries anymore.

    But it's definite not like wow, we have a truly open hardware platform now.

    And my reading of the announcment doesnt say that is IS a completely open platform - I don't reckong I ever seem them claim that. As I see it the GPU is still closed, which is to be expected I reckon. I look on it as just a block of hardware attached to a Arm, and now all th Arm code is available,

     

    Dunno how they did it though - getting stuff out of Broadcom is like getting a baby out of a dingos mouth, so Kudo to them.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Luc Cool wrote:

     

    It could have some use under linux to figure out what functions are implemented.

    It's usefull for the development of other os, as they don't need the linux libraries anymore.

    But it's definite not like wow, we have a truly open hardware platform now.

    And my reading of the announcment doesnt say that is IS a completely open platform - I don't reckong I ever seem them claim that. As I see it the GPU is still closed, which is to be expected I reckon. I look on it as just a block of hardware attached to a Arm, and now all th Arm code is available,

     

    Dunno how they did it though - getting stuff out of Broadcom is like getting a baby out of a dingos mouth, so Kudo to them.