Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Open Source ARM Userland
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 31 replies
  • Subscribers 710 subscribers
  • Views 4649 views
  • Users 0 members are here
  • videocore
  • open_source
  • drivers
  • github
  • userland
  • raspberry_pi
  • gpu
  • news
Related

Open Source ARM Userland

jealderson1
jealderson1 over 13 years ago

It has been announced today on the Raspberry Pi site that the userland libraries have been made open-source. This makes the BCM2835 on the Raspberry Pi the "first ARM-based multimedia SoC with fully-functional, vendor-provided (as opposed to partial, reverse engineered) fully open-source drivers" (in the words of Alex Bradbury - the lead Linux developer at the Raspberry Pi foundation).

 

This should make life much easier for anyone looking to port different operating systems on to the Pi. With the GPU drivers opened up, it will mean that you can take advantage of the full hardware accelerated graphical capabilities of the BCM2835.

 

According to Alex, Broadcom are the first vendor of mobile phone SoCs to open up their drivers this way.

 

You can read the full announcement on RaspberryPi.org

 

Does this help anyone with their plans, or give them an idea? You can find the userland source on GitHub

 


  • Sign in to reply
  • Cancel
Parents
  • morgaine
    morgaine over 13 years ago

    I've just seen this (thanks John for the Slashdot link, interesting comments and responses there), and on the whole I welcome it as a move in the right direction.  Something being open sourced is better than nothing being open sourced.

     

    However, it's most definitely not what the PR on the blog describes, because RPF's diagram of Raspberry Pi Software Architecture clearly shows OpenGL ES as being open sourced under the BSD license but that is not the case.  OpenGL ES runs on the VideoCore, so it has not been open sourced.  Too much is being claimed, and the claims are not accurate.

     

    It's easy to give such PR statements an acid test.  Does this open sourcing mean that OpenGL ES can be hacked and modified and improved and bugs fixed by the community?  No it doesn't, because only the API or interface to it has been open sourced (what people are calling the "shim"), and having open source access to this shim does not enable you to modify OpenGL ES itself.  The acid test shows that claim to be false.

     

    In typical fashion, RPF is overstating the merits of what it has done.  Nevertheless, I welcome the shims being open sourced.  I have been calling for at least the APIs to the closed hardware to be opened and documented for a long time, so this is a start.  Next comes the documentation phase.

     

    Unfortunately, developers who thought that the news meant that the GPU is now directly programmable or that OpenGL ES is now open source will be very disappointed.

     

    Morgaine.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    I've just seen this (thanks John for the Slashdot link, interesting comments and responses there), and on the whole I welcome it as a move in the right direction.  Something being open sourced is better than nothing being open sourced.

     

    However, it's most definitely not what the PR on the blog describes, because RPF's diagram of Raspberry Pi Software Architecture clearly shows OpenGL ES as being open sourced under the BSD license but that is not the case.  OpenGL ES runs on the VideoCore, so it has not been open sourced.  Too much is being claimed, and the claims are not accurate.

     

    It's easy to give such PR statements an acid test.  Does this open sourcing mean that OpenGL ES can be hacked and modified and improved and bugs fixed by the community?  No it doesn't, because only the API or interface to it has been open sourced (what people are calling the "shim"), and having open source access to this shim does not enable you to modify OpenGL ES itself.  The acid test shows that claim to be false.

     

    In typical fashion, RPF is overstating the merits of what it has done.  Nevertheless, I welcome the shims being open sourced.  I have been calling for at least the APIs to the closed hardware to be opened and documented for a long time, so this is a start.  Next comes the documentation phase.

     

    Unfortunately, developers who thought that the news meant that the GPU is now directly programmable or that OpenGL ES is now open source will be very disappointed.

     

    Morgaine.

    Once again a deliberately misleading post from Ms Divona.

     

    I've read the release, and checked out the diagram carefully, they have now released the source to the OGLES library running on the Arm (and all the other Arm side libraries). This appears to be a shim/wrappper layer to convert GLES calls to GPU api calls, and therefor is correctly refered to as a driver. This means that anyone can no recompile/modify those libraries easily and use OpenGLES calls from their baremetal code, or their homegrown OS etc. At no point have they claimed any code on the GPU iteself has been open sourced, that would indeed be incorrect, and in fact checking slashdot, the Eben bloke has been quite specific in what has been released.

     

    Why is it that ANY good news from these people is immediately slagged here? Do you people want them to fail? Are you really that vindictive as to want a charity to fail, one set up to improve the teaching of children? Sometimes you lot are unbelievable.

     

    Bill

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to e14 Contributor

    Stick to facts please, fanboyism doesn't get you anywhere on a site where engineering facts are considerably more important than PR.

     

    RPF's own diagram shows the Pi's OpenGL ES running on ARM and licensed under BSD.  The Pi's OpenGL ES does not run on the ARM and is not licensed under BSD nor under any other open source license.  It is implemented as firmware on the VideoCore, so the diagram is completely misleading, and has led to non-technical people misunderstanding what was open-sourced.  Only the shim was open-sourced, which contains nothing of OpenGL ES's implementation that people could usefully fix or improve.

     

    Your reply is doubly misplaced because I welcomed even just the shim being opened.  But of course you wouldn't care about the facts here.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    Stick to facts please, fanboyism doesn't get you anywhere on a site where engineering facts are considerably more important than PR.

     

    RPF's own diagram shows the Pi's OpenGL ES running on ARM and licensed under BSD.  The Pi's OpenGL ES does not run on the ARM and is not licensed under BSD nor under any other open source license.  It is implemented as firmware on the VideoCore, so the diagram is completely misleading, and has led to non-technical people misunderstanding what was open-sourced.  Only the shim was open-sourced, which contains nothing of OpenGL ES's implementation that people could usefully fix or improve.

     

    Your reply is doubly misplaced because I welcomed even just the shim being opened.  But of course you wouldn't care about the facts here.

    It appears I know more facts that you do, but then I spend a lot of time in the real world doing a real job with real engineers. The diagram shows the Linux libraries for EGL, OGES and VG now as OSS, along with the GPL VCHIQ kernel driver (which IIRC has always been GPL'd). These are all on the Arm side, as the diagram states. These are the libraries that they have been talking about, and at no point that I can see have the Raspberry Pi foundation ever stated the GPU code was being made OSS. The fact that these libraries are shims to translate the LInux standard API's to whatever the GPU does is irrelevent, since they are, to all intents and purposes the implementation of the API.

     

    And there is an interesting post on the Raspberry Pi forums which says something about the lines of code running on the GPU - over 5 million! If you think any person unfamilar with the code woudl be able to make improvements or fix bugs without spending a hell of a lot of time on, then your engineering skills are not of this world. And that coming from someone who has experience in a similar area. I'll leave the bug fixing to the experts thanks mate!

     

    As an aside, anyone found any bugs on the GPU yet? Or anyone think they could make the implementation better than the team that designed the hardware and wrote the software? Or have a go at writing their own 5m lines of code?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to e14 Contributor

    You appear to be willfully or accidentally disregarding the words shown on the diagram, so I'll enumerate the newly BSD-licensed blocks for you.  For reference, the diagram is here .  Please read carefully the words on each of the BSD-licensed blocks.  To help you avoid confusing implementations with interfaces, I'll provide the Wikipedia references as well so that you can see what the block labelled with each of these words is supposed to do.

     

    • OpenMAX --- http://en.wikipedia.org/wiki/OpenMAX
    • OpenGL ES  --- http://en.wikipedia.org/wiki/OpenGL_ES
    • OpenVG --- http://en.wikipedia.org/wiki/OpenVG
    • EGL --- http://en.wikipedia.org/wiki/EGL_%28OpenGL%29

     

    Now that you know what each block is supposed to do, let's see what the evidence is that OpenGL ES (one of the blocks in question) runs on the ARM in any shape or form, in libraries or in daemons or in any other form of executing entity that you prefer:

     

    • Eben Upton has very clearly stated (link referenced earlier in this thread) that OpenGL ES runs on the VideoCore and presents a high-level messaging interface to the ARM side.  OpenGL ES itself does not run on the ARM in any shape or form.  Since you appear to disregard technical facts, perhaps giving you Eben's description here first will convince you even if you ignore the facts that follow.
    • The RPF blog announcement thread about this open sourcing contains code listings showing that the userland code that has been open sourced is merely a shim passing messages to the VideoCore.  Very clear to see (probably even to non-programmers) is that the released code does nothing at all except pass arguments through to VideoCore using RPC messages.  It is clearly nothing but an API, almost worthless to any open source developer wishing to fix or improve OpenGL ES, as actually open sourcing ARM-based OpenGL ES would have allowed.
    • The diagram does not show OpenGL ES implemented on the VideoCore at all, so people who don't know the details of BCM2835 architecture could be forgiven for thinking that the orange block labelled "OpenGL ES" is the implementation of OpenGL ES for the Pi.  I doubt that it was deliberate, but it's a very unfortunate omission which has led many non-technical people into thinking that OpenGL ES resides in the block called "OpenGL ES", and has been magnanimously open-sourced.  It does not, and it has not.
    • Developers of the open-source Lima driver for ARM's MALI-400 GPU and of *BSD have explained clearly that OpenGL ES has not been open sourced, and that only some small shims interfacing to the OpenGL ES on the VideoCore have been released under the BSD license..

     

    So, I don't know how you can argue that the diagram which clearly show OpenGL ES as BSD-licensed is accurate.  It's not.  Only small interface libraries (the API which hides the messaging to OpenGL ES which runs on the VideoCore) have been open sourced, not OpenGL ES itself, neither in the form of libraries nor in any other form.

     

    If this had been stated clearly on the blog, and especially if the diagram had been labelled correctly on the blog (because non-technical people just look at the diagram), then much of the confusion suffered by non-programmers would have been avoided, and so many non-programmers would not be thinking that Broadcom is the first ARM company to have made OpenGL ES open source.  Broadcom has not done this, despite many people now thinking that they did.

     

    Morgaine.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • recantha
    recantha over 13 years ago in reply to morgaine

    Play nicely, people.

    At least, play nicer than this thread over on the Foundation's original post:

    http://www.raspberrypi.org/archives/2221#comment-34981

     

    I think the main problem people are having is that the press release and original headline are a bit misleading as to what has been released. i.e. people have mistakenly taken it as 'Everything has been open sourced, hurrah!' whereas there's plenty of smaller print saying 'But not this bit - way too difficult to release at the moment'.

     

    I think we should be grateful for what we've got and see what we can do with it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • recantha
    recantha over 13 years ago in reply to morgaine

    Play nicely, people.

    At least, play nicer than this thread over on the Foundation's original post:

    http://www.raspberrypi.org/archives/2221#comment-34981

     

    I think the main problem people are having is that the press release and original headline are a bit misleading as to what has been released. i.e. people have mistakenly taken it as 'Everything has been open sourced, hurrah!' whereas there's plenty of smaller print saying 'But not this bit - way too difficult to release at the moment'.

     

    I think we should be grateful for what we've got and see what we can do with it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to recantha

    > I think we should be grateful for what we've got and see what we can do with it.

     

    I think if you realized how little was opened up, compared to what was advertised:

    "Today we have some really big news, which is going to mean a lot to many programmers"

    you might agree with the experts who are showing their extreme disgust.

     

    Liz said at the link you give: "There's some microcode in the videocore."

    Abishur similarly said "there is still just a small amount of GPU stuff in the GPU that is closed".

    http://www.raspberrypi.org/phpBB3/viewtopic.php?f=63&t=20900&start=28

     

    But it turns out that essentially *all* the functionality is in the closed videocore,

    which JamesH says is more than 5M lines of code, not some miniscule amount.

     

    This is not even a step on the way to opening up the rest.

    As was explained, the shim was opened up because it didn't

    contain the crown jewels, not as a first step in opening up the

    crown jewels.

     

    It may in fact be possible for some people to get some benefit from

    the shim, but the OpenBSD guys who supposedly were going to benefit

    the most, were the most vocal against it.

    http://www.mail-archive.com/misc@openbsd.org/msg116656.html

    http://www.mail-archive.com/misc@openbsd.org/msg116657.html