Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Open Source ARM Userland
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 31 replies
  • Subscribers 710 subscribers
  • Views 4669 views
  • Users 0 members are here
  • videocore
  • open_source
  • drivers
  • github
  • userland
  • raspberry_pi
  • gpu
  • news
Related

Open Source ARM Userland

jealderson1
jealderson1 over 13 years ago

It has been announced today on the Raspberry Pi site that the userland libraries have been made open-source. This makes the BCM2835 on the Raspberry Pi the "first ARM-based multimedia SoC with fully-functional, vendor-provided (as opposed to partial, reverse engineered) fully open-source drivers" (in the words of Alex Bradbury - the lead Linux developer at the Raspberry Pi foundation).

 

This should make life much easier for anyone looking to port different operating systems on to the Pi. With the GPU drivers opened up, it will mean that you can take advantage of the full hardware accelerated graphical capabilities of the BCM2835.

 

According to Alex, Broadcom are the first vendor of mobile phone SoCs to open up their drivers this way.

 

You can read the full announcement on RaspberryPi.org

 

Does this help anyone with their plans, or give them an idea? You can find the userland source on GitHub

 


  • Sign in to reply
  • Cancel
Parents
  • morgaine
    morgaine over 13 years ago

    I've just seen this (thanks John for the Slashdot link, interesting comments and responses there), and on the whole I welcome it as a move in the right direction.  Something being open sourced is better than nothing being open sourced.

     

    However, it's most definitely not what the PR on the blog describes, because RPF's diagram of Raspberry Pi Software Architecture clearly shows OpenGL ES as being open sourced under the BSD license but that is not the case.  OpenGL ES runs on the VideoCore, so it has not been open sourced.  Too much is being claimed, and the claims are not accurate.

     

    It's easy to give such PR statements an acid test.  Does this open sourcing mean that OpenGL ES can be hacked and modified and improved and bugs fixed by the community?  No it doesn't, because only the API or interface to it has been open sourced (what people are calling the "shim"), and having open source access to this shim does not enable you to modify OpenGL ES itself.  The acid test shows that claim to be false.

     

    In typical fashion, RPF is overstating the merits of what it has done.  Nevertheless, I welcome the shims being open sourced.  I have been calling for at least the APIs to the closed hardware to be opened and documented for a long time, so this is a start.  Next comes the documentation phase.

     

    Unfortunately, developers who thought that the news meant that the GPU is now directly programmable or that OpenGL ES is now open source will be very disappointed.

     

    Morgaine.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    I've just seen this (thanks John for the Slashdot link, interesting comments and responses there), and on the whole I welcome it as a move in the right direction.  Something being open sourced is better than nothing being open sourced.

     

    However, it's most definitely not what the PR on the blog describes, because RPF's diagram of Raspberry Pi Software Architecture clearly shows OpenGL ES as being open sourced under the BSD license but that is not the case.  OpenGL ES runs on the VideoCore, so it has not been open sourced.  Too much is being claimed, and the claims are not accurate.

     

    It's easy to give such PR statements an acid test.  Does this open sourcing mean that OpenGL ES can be hacked and modified and improved and bugs fixed by the community?  No it doesn't, because only the API or interface to it has been open sourced (what people are calling the "shim"), and having open source access to this shim does not enable you to modify OpenGL ES itself.  The acid test shows that claim to be false.

     

    In typical fashion, RPF is overstating the merits of what it has done.  Nevertheless, I welcome the shims being open sourced.  I have been calling for at least the APIs to the closed hardware to be opened and documented for a long time, so this is a start.  Next comes the documentation phase.

     

    Unfortunately, developers who thought that the news meant that the GPU is now directly programmable or that OpenGL ES is now open source will be very disappointed.

     

    Morgaine.

    Once again a deliberately misleading post from Ms Divona.

     

    I've read the release, and checked out the diagram carefully, they have now released the source to the OGLES library running on the Arm (and all the other Arm side libraries). This appears to be a shim/wrappper layer to convert GLES calls to GPU api calls, and therefor is correctly refered to as a driver. This means that anyone can no recompile/modify those libraries easily and use OpenGLES calls from their baremetal code, or their homegrown OS etc. At no point have they claimed any code on the GPU iteself has been open sourced, that would indeed be incorrect, and in fact checking slashdot, the Eben bloke has been quite specific in what has been released.

     

    Why is it that ANY good news from these people is immediately slagged here? Do you people want them to fail? Are you really that vindictive as to want a charity to fail, one set up to improve the teaching of children? Sometimes you lot are unbelievable.

     

    Bill

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine

    ~If~ the announcement had been something like "GPU interfacing SDK released - documentation to come (subject to manpower)" then it would have saved a lot of traffic.Using a word as emotive as "open" might have been a touch foolhardy. Oh well. image

     

    Eben was pretty straightforward about it all in the Slashdot comments that John Beetem linked to. Perhaps he should have written the blog post in the first place...

     

    Anyway, free (as in beer) stuff never hurts - I'm sure that it will find a use with folks writing their own applications, or minimalist embedded types. Someone may even figure out how to migrate the USB traffic into the GPU, or use it to number crunch a discrete Fourier transform etc, but I don't think it's anything for "ordinary" users to get too excited about just yet.

     

    "Pi blog headline writer to my office immediately..."

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Does anybody knows what compiler and compression algoritm they use at broadcom?

     

    5M lines of code...

    Is it?

    loader.bin 269KB

    start.elf    2401KB

    bootcode.bin 17KB

     

    the start.elf for the 240MB memory split is even only 600 - 700KB.

    I know Dom throw some stuff out, not sure if it's the gpu code.

     

    Isn't it amazing? 2 lines of code produce one byte in the final binary.

     

    Maybe employees are payed based upon the number of codelines they produce? image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Luc Cool wrote:

     

    ...Maybe employees are payed based upon the number of codelines they produce? image

     

    I think that only happens at Microsoft! [/shooting fish in a barrel mode] image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 13 years ago in reply to e14 Contributor

    Luc Cool wrote:

     

    Does anybody knows what compiler and compression algorithm they use at Broadcom?

     

    5M lines of code...

    Is it?

    loader.bin 269KB

    start.elf    2401KB

    bootcode.bin 17KB

     

    the start.elf for the 240MB memory split is even only 600 - 700KB.

    I know Dom throw some stuff out, not sure if it's the gpu code.

     

    Isn't it amazing? 2 lines of code produce one byte in the final binary.

    I've never seen any of VideoCore's 5 MLOC* and given jamesh's various comments chez RasPi I don't think I want see it, but here are some general comments about how 5 MLOC gets down to 2 MB of binary, or whatever it is.

     

    First, compression: general-purpose compression algorithms can usually get you a factor of 2 for typical binaries.  If the binary is sparse, like an FPGA image or VLIW instructions you can get 3-4.

     

    Second, SLOC usually includes comments.  Well-documented code will have higher KLOC per KB of binary.  This is particularly true if it's clever code that uses tricks to save instructions.  They say that every time you remove a line of code by doing something clever, you should add 5-10 comment lines to explain what you did so the code can be maintained.  Performance-sensitive video/graphics code should fall into this category.

     

    Third, VideoCore may have a standard coding style which increases the number of lines of code.  For example, one place I worked forbid having single-line conditionals and loops.  Instead of "if (condition) consequent else alternative" you had to write:

     

    if (condition)

    {

       consequent

    }

    else

    {

       alternative

    }

     

    There's a factor of 6 increase in SLOC right there.

     

    Fourth, there may be lots of conditional compilation so that the same code supports different VideoCore versions and configurations.  Code that gets omitted by conditional compilation adds to the SLOC count but don't add to the binary.

     

    Fifth, we don't know what's encompassed by jamesh's 5 MLOC.  It might be the code that goes into the standard RasPi binary blob, or it might include other VideoCore code such as diagnostics and codecs.  I would hope the basic video and graphics processing is pretty clean and simple and is 10's of KLOC and not MLOC.  When I hear of 5 MLOC complexity, I hear C.A.R. Hoare saying:

    There are two ways of constructing a software design: One way is to make it so simple that there are obviously no deficiencies, and the other way is to make it so complicated that there are no obvious deficiencies.  The first method is far more difficult.

    OTOH, jamesh's comments on VideoCore suggest that they did it the easy way.

     

    *Glossary:

    SLOC/KLOC/MLOC: Source/Kilo/Mega Lines of Code.

    VLIW: Very Long Instruction Word.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to johnbeetem

    John Beetem wrote:

     

    Luc Cool wrote:

     

    Does anybody knows what compiler and compression algorithm they use at Broadcom?

     

    5M lines of code...

    Is it?

    loader.bin 269KB

    start.elf    2401KB

    bootcode.bin 17KB

     

    the start.elf for the 240MB memory split is even only 600 - 700KB.

    I know Dom throw some stuff out, not sure if it's the gpu code.

     

    Isn't it amazing? 2 lines of code produce one byte in the final binary.

    I've never seen any of VideoCore's 5 MLOC* and given jamesh's various comments chez RasPi I don't think I want see it, but here are some general comments about how 5 MLOC gets down to 2 MB of binary, or whatever it is.

     

    First, compression: general-purpose compression algorithms can usually get you a factor of 2 for typical binaries.  If the binary is sparse, like an FPGA image or VLIW instructions you can get 3-4.

     

    Second, SLOC usually includes comments.  Well-documented code will have higher KLOC per KB of binary.  This is particularly true if it's clever code that uses tricks to save instructions.  They say that every time you remove a line of code by doing something clever, you should add 5-10 comment lines to explain what you did so the code can be maintained.  Performance-sensitive video/graphics code should fall into this category.

     

    Third, VideoCore may have a standard coding style which increases the number of lines of code.  For example, one place I worked forbid having single-line conditionals and loops.  Instead of "if (condition) consequent else alternative" you had to write:

     

    if (condition)

    {

       consequent

    }

    else

    {

       alternative

    }

     

    There's a factor of 6 increase in SLOC right there.

     

    Fourth, there may be lots of conditional compilation so that the same code supports different VideoCore versions and configurations.  Code that gets omitted by conditional compilation adds to the SLOC count but don't add to the binary.

     

    Fifth, we don't know what's encompassed by jamesh's 5 MLOC.  It might be the code that goes into the standard RasPi binary blob, or it might include other VideoCore code such as diagnostics and codecs.  I would hope the basic video and graphics processing is pretty clean and simple and is 10's of KLOC and not MLOC.  When I hear of 5 MLOC complexity, I hear C.A.R. Hoare saying:

    There are two ways of constructing a software design: One way is to make it so simple that there are obviously no deficiencies, and the other way is to make it so complicated that there are no obvious deficiencies.  The first method is far more difficult.

    OTOH, jamesh's comments on VideoCore suggest that they did it the easy way.

     

    *Glossary:

    SLOC/KLOC/MLOC: Source/Kilo/Mega Lines of Code.

    VLIW: Very Long Instruction Word.

     

    What a good post. Not vitriolic, pretty sensible assumptions, no whinging. Are you sure youa re in the right place? Only thing I'd say is the GPU's are now very very complicated, and need a lot of code to make them work - if I rememebr right this has 3D units, 2D, video stuff in many differetn formats, a camera interface, LCD control, HDMI, i2c, i2s and probably other stuff not made public. And even an implementation of OpenGLES is a *** load of code - try a line compare with the MESA librearies.

     

    As to the compiler, a quick google find you its a custom job, so presumably the CPU is a custom design.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • recantha
    recantha over 13 years ago in reply to e14 Contributor

    Billy Thornton wrote:

     

    What a good post. Not vitriolic, pretty sensible assumptions, no whinging.

    What a pity you couldn't have resisted the temptation... Give it a rest, Billy.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 13 years ago in reply to e14 Contributor

    Billy Thornton wrote:

    Only thing I'd say is the GPU's are now very very complicated, and need a lot of code to make them work - if I rememebr right this has 3D units, 2D, video stuff in many differetn formats, a camera interface, LCD control, HDMI, i2c, i2s and probably other stuff not made public.

    Billy, as far as I know, the code for the  CSI and DSI interfaces is not yet distributed with the firmware images, as it hasn't been written yet.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to rew

    Argh, been away on business, so had my rest, now back for more fun.

     

    Roger Wolff wrote:

     

    Billy Thornton wrote:

    Only thing I'd say is the GPU's are now very very complicated, and need a lot of code to make them work - if I rememebr right this has 3D units, 2D, video stuff in many differetn formats, a camera interface, LCD control, HDMI, i2c, i2s and probably other stuff not made public.

    Billy, as far as I know, the code for the  CSI and DSI interfaces is not yet distributed with the firmware images, as it hasn't been written yet.

     

    So, bearing in mind the GPU in the Pi is the same as that in the latest Nokia Symbian phones, you know, the ones with the best camera phones in the world, and with LCD panels on the front, what make you think the software hasnt been written yet? I reckon all the GPU software is there, it's the Linux shim that needs doing, and that stuffs a PITA. Since I rememebr seeing some images from a camera attached to the board, I guess it takes pictures already.

     

    Bill

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 13 years ago in reply to e14 Contributor

    Yeah, in theory the code is "somewhere", but in practise the guys at broadcom have to configure their source tree to make a "start.elf" that runs on the 'pi. And there might be code to write to make the "can take a picture" code talk to Linux, not just the linux code to take advantage of it, but also the code on the GPU that talks to Linux.

     

    On the other hand, even if there is a Nokia phone with broadcom support, maybe nokia said: "We've heard that Nikon makes good video processing software".... -- "but that'll add $3 to the price of the SOC!"... -- "It's important to us to have the best video processing available, NOW, so we'll pay for it".

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to rew

    Roger Wolff wrote:

     

    Yeah, in theory the code is "somewhere", but in practise the guys at broadcom have to configure their source tree to make a "start.elf" that runs on the 'pi. And there might be code to write to make the "can take a picture" code talk to Linux, not just the linux code to take advantage of it, but also the code on the GPU that talks to Linux.

     

    On the other hand, even if there is a Nokia phone with broadcom support, maybe nokia said: "We've heard that Nikon makes good video processing software".... -- "but that'll add $3 to the price of the SOC!"... -- "It's important to us to have the best video processing available, NOW, so we'll pay for it".

    I read on the Pi website that they were writing the Linux side code to communicate with the camera driver, although was already available using something called OpenMAX.

     

    From what I've read around, the broadcomm GPU does all the camera work in the Nokia smartphones, even the 808.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to rew

    Roger Wolff wrote:

     

    Yeah, in theory the code is "somewhere", but in practise the guys at broadcom have to configure their source tree to make a "start.elf" that runs on the 'pi. And there might be code to write to make the "can take a picture" code talk to Linux, not just the linux code to take advantage of it, but also the code on the GPU that talks to Linux.

     

    On the other hand, even if there is a Nokia phone with broadcom support, maybe nokia said: "We've heard that Nikon makes good video processing software".... -- "but that'll add $3 to the price of the SOC!"... -- "It's important to us to have the best video processing available, NOW, so we'll pay for it".

    I read on the Pi website that they were writing the Linux side code to communicate with the camera driver, although was already available using something called OpenMAX.

     

    From what I've read around, the broadcomm GPU does all the camera work in the Nokia smartphones, even the 808.