Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum USB device connect resets 512M Raspberry Pi (most USB devices).
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 22 replies
  • Subscribers 708 subscribers
  • Views 5634 views
  • Users 0 members are here
Related

USB device connect resets 512M Raspberry Pi (most USB devices).

e14 Contributor
e14 Contributor over 13 years ago

Hi,

 

I got my batch of 3 brand-new 512M Raspberry Pi-s today (hardware revision "000f" according to /proc/cpuinfo). Every single one of them exhibits the same instability: They reset when I connect certain USB devices. If I have such an offending USB device connected on power-on and leave it in, it will work just fine. Which means that hot-plugging USB devices does not work - a critical bug.

 

I have a couple of USB devices that I can connect without resetting a running 512M Pi:

 

* A SanDisk Cruzer Micro 16 GB memory stick.

* A handful of non-descript memory sticks (give-away advertising gifts from various vendors).

* My USB keyboard.

 

But every single time that I plug any of the following devices into a 512M Pi it resets:

 

* D-Link N Nano Wi-Fi dongle DWA-131.

* Kingston Data Traveller II, 2 GB memory stick.

* An old IBM 64 MB memory stick.

* A pair of USB-powered loudspeakers (speakers with a mini-jack and an analog built-in amplifier powered by 5V USB).

 

I suspect that the USB power surge when an offending device is connected and powers up, is causing the Pi to reset. This did not happen on a previous revision of the Pi - I have three older 256M Pi's and they can all have all of the above USB devices hot-plugged without resetting (as you would expect).

 

The power rail on the 512M Pi's USB port is quite dirty. If I power my USB loudspeakers from a 512M Pi's USB port then I have just as much background noise as I have sound. The noise sounds like power supply switching noise, a 2-4 kHz steady tone with high-frequent chirps as soon as there is activity, e.g. the SD card is active. This leaves the audio output completely unusable. If I do the same setup on a 256M Pi there is still too much background noise for comfort but it is clearly less than on a 512M Pi. If I power the USB loudspeakers from elsewhere, e.g. my laptop, and connect the loudspeakers to the Pi's audio jack then the sound is fine - the noise level is at least low enough for casual listening.

 

I have two different types of 1000 mA 5V power supplies that I have tested with. There is no difference in behavior. I have even tried to buffer the on-board 5V by connecting a flat-ribbon cable to the P1 connector and then, via the ribbon cable wires, connect a 4700 uF capacitor across 5V and GND (pin 2 -> pin 6). No effect.

 

I have seen a report on thermal instability with the new 512M Pi's [1] but that issue is not seen here. I have left one of the 512M Pi's running for 3.5 hours straight without any problems - this one was idling and was not overclocked. I then overclocked it to max "Turbo" mode, re-booted, and started a python script that burns 100% CPU. The /sys/class/thermal/thermal_zone0/temp reported 45 degrees C (45000 raw number) when I started the script and stabilized at 53 degrees C after a minute or so. I left it running for more than 20 minutes straight - no problems.

 

[1] http://www.raspberrypi.org/phpBB3/viewtopic.php?f=28&t=22281&p=215444

 

There has also been a report on a bad USB controller connection [2]. We can rule that out. The issue occurs with specific USB devices and cannot be triggered by mechanically exciting the USB connector. Plus, it is the same pattern on all 3 boards.

 

[2] http://www.element14.com/community/message/64061

 

Unfortunately this sounds like an RMA on all three boards. Please advise me on how to proceed and when I can expect a new batch of 512M Pi's where the USB interface is stable again.

 

  Kind regards

-- Jan Holst Jensen

  • Sign in to reply
  • Cancel
Parents
  • wallarug
    wallarug over 13 years ago

    Sounds like the "bad batch" from RS is

     

    BATCH NUMBER: E3912RSV13R1.0

     

    That is the vibe I am getting from the other forum.  Get people to check batch numbers.

     

    [1] http://www.raspberrypi.org/phpBB3/viewtopic.php?f=28&t=22281&p=215444

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • wallarug
    wallarug over 13 years ago

    Sounds like the "bad batch" from RS is

     

    BATCH NUMBER: E3912RSV13R1.0

     

    That is the vibe I am getting from the other forum.  Get people to check batch numbers.

     

    [1] http://www.raspberrypi.org/phpBB3/viewtopic.php?f=28&t=22281&p=215444

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to wallarug

    Fergus Byrne wrote:

     

    Sounds like the "bad batch" from RS is

     

    BATCH NUMBER: E3912RSV13R1.0

     

    That is the vibe I am getting from the other forum.  Get people to check batch numbers.

     

    [1] http://www.raspberrypi.org/phpBB3/viewtopic.php?f=28&t=22281&p=215444

     

    I can't find something on my boards that look like that kind of batch number. But there is a white label with "digital-clock"-like digits on the bottom side of the board that says "1241", which I assume could mean "batch 41, 2012" ? Above that label there are two lines of white text that say "KCE MC1" and "94V-0 F1". Right below the SD card connector there is a sticker that says "07/11".

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    > there is a white label with "digital-clock"-like digits on the bottom side of the board that says "1241", which I assume could mean "batch 41, 2012" ?

     

    It probably means week 41 of 2012.