Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum Creating Python 2.7 Class
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 16 replies
  • Subscribers 704 subscribers
  • Views 2697 views
  • Users 0 members are here
  • that
  • of
  • in
  • under
  • cmdmodule
  • the
  • instance
  • to
  • very
  • this
  • instead);
  • am
  • must
  • first
  • create
  • need
  • as
  • method
  • are
  • way
  • commands
  • raspberry_pi
  • hi
  • unbound
  • grouped
  • called
  • argument
  • send_when_different()
  • with
  • be
  • (got
  • quickly.;
  • typeerror:
  • attempting
  • instructions
  • a
  • class.
  • file
  • can
  • set
  • i
  • nothing
Related

Creating Python 2.7 Class

wallarug
wallarug over 14 years ago

Hi, I am attempting to create a set of instructions that are grouped in a file under a class.  This way, the commands that I need can be called very quickly.

 

I am having a problem, I keep getting the following error:

[ code ]

 

Traceback (most recent call last):

  File "<pyshell#7>", line 1, in <module>

    CMDmodule.send_when_different()

TypeError: unbound method send_when_different() must be called with CMDmodule instance as first argument (got nothing instead)

 

[ /code]

 

Does anyone know how I can get the groups of commands to work by me importing the module / class?

Attachments:
CMDmodule.py.zip
  • Sign in to reply
  • Cancel
Parents
  • mgt6910
    mgt6910 over 14 years ago

    Fergus, this link may point you in the right direction...

     

    http://stackoverflow.com/questions/4473184/unbound-method-f-must-be-called-with-fibo-instance-as-first-argument-got-cla

     

     

    p.s. why did  you use 512 tests to invert the motors instead of :

     

     

    def invert_mota(self):

         motor_a = 255 - motor_a

     

    def invert_motb(self):

         motor_b = 255 - motor_b

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to mgt6910

    >  p.s. why did  you use 512 tests to invert the motors instead of :  ...

     

    good point!

     

    One of the design goals for programming languages is that there should

    essentially never be a need for repetitive looking code.  So when you

    see something like that, you know there's probably a better way to do it.

     

    For example, using copy/paste to duplicate code is usually a bad idea.

    Instead, you should usually create a subprogram and call it multiple times.

    If you have multiple sequential calls to the same subprogram, you should

    instead use a loop.  If you have similar but not identical subprograms,

    you can combine them by adding parameters.  If you have similar

    algorithms applied to different data types, you can combine them

    using generics.  If you have similar classes, you can combine their

    common parts using inheritance from a common base class.

     

    In the case at hand, when you have a repetitive looking elsif chain,

    you can often simplify it using a switch statement.  If you still have a

    repetitive looking switch statement, you can often simplify it using

    a table lookup, either to look up a value or to look up a subprogram

    to call indirectly.  If you still have a repetitive looking table, you can

    often simplify it using a mathematical calculation.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to mgt6910

    >  p.s. why did  you use 512 tests to invert the motors instead of :  ...

     

    good point!

     

    One of the design goals for programming languages is that there should

    essentially never be a need for repetitive looking code.  So when you

    see something like that, you know there's probably a better way to do it.

     

    For example, using copy/paste to duplicate code is usually a bad idea.

    Instead, you should usually create a subprogram and call it multiple times.

    If you have multiple sequential calls to the same subprogram, you should

    instead use a loop.  If you have similar but not identical subprograms,

    you can combine them by adding parameters.  If you have similar

    algorithms applied to different data types, you can combine them

    using generics.  If you have similar classes, you can combine their

    common parts using inheritance from a common base class.

     

    In the case at hand, when you have a repetitive looking elsif chain,

    you can often simplify it using a switch statement.  If you still have a

    repetitive looking switch statement, you can often simplify it using

    a table lookup, either to look up a value or to look up a subprogram

    to call indirectly.  If you still have a repetitive looking table, you can

    often simplify it using a mathematical calculation.