Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Relay board for Raspberry Pi?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 19 replies
  • Subscribers 710 subscribers
  • Views 3868 views
  • Users 0 members are here
  • pi
  • raspberry_pi
  • adafruit
  • relay
Related

Relay board for Raspberry Pi?

alfredos
alfredos over 13 years ago

Hi,

 

I need to move about 10 relays off a Raspberry Pi for my home automation project. I can find easily ready made, inexpensive boards that will connect to anything at 5V, like an Arduino. But there doesn't seem to be much on offer for the Pi's 3V3 GPIO. My current best find is Adafruit's 3-to-5 and any 5V relay board off DX or so.

 

I am looking for a ready made board or ready to build kit, as compact as possible. Ideally powered off the 5V pin available on the Pi, but I can live with another P/S.

 

Any recommendations?

  • Sign in to reply
  • Cancel
Parents
  • mcb1
    mcb1 over 9 years ago

    You can drive the Opto-coupled boards with the 3v3 I/O of the RPi.

    In most cases they have a 1000ohm resistor and LED in series with the LED part of the opto-coupler.

     

    You simply add another 1k across the existing one, and they'll happily drive from the 3v3 RPi i/o pins.

    You'll need both 5v (for the relays) and 3v3 for the channel drive as these boards are active low (ie you make IN1 LOW to turn on the relay)

     

    image

     

    With 10 relays the other suggestion takes much less i/o pins.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • mcb1
    mcb1 over 9 years ago

    You can drive the Opto-coupled boards with the 3v3 I/O of the RPi.

    In most cases they have a 1000ohm resistor and LED in series with the LED part of the opto-coupler.

     

    You simply add another 1k across the existing one, and they'll happily drive from the 3v3 RPi i/o pins.

    You'll need both 5v (for the relays) and 3v3 for the channel drive as these boards are active low (ie you make IN1 LOW to turn on the relay)

     

    image

     

    With 10 relays the other suggestion takes much less i/o pins.

     

    Mark