Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Anyone one received raspberry pi rev B 512MB  Made in China and how about its Production Quality?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 20 replies
  • Subscribers 709 subscribers
  • Views 3859 views
  • Users 0 members are here
  • raspberry_pi
Related

Anyone one received raspberry pi rev B 512MB  Made in China and how about its Production Quality?

zidane1980
zidane1980 over 13 years ago

I received raspberry pi rev B 512MB Made in China last week,unlike the neat board made in the UK and I feel quite disappoint about it,

this is mine

and below is how it looks

image

the pcb was remarked as Made In China

image

 

And this! the p5 pin holes was filled with solder, which will make me a lot of trouble soldering pins

image

 

And so as the jtag pins...

image

 

Look this,a big tin ball on pin...I cannot imagine how they made it...

 

 

image

the same solder work on the usb ports

image

 

 

Just some complain,  I will not be pleasure to receive such a junk.

  • Sign in to reply
  • Cancel
  • shabaz
    shabaz over 13 years ago in reply to e14 Contributor

    Soldered holes is normal (or acceptable) if it is the long set of holes labelled P2/P3.

    As far as I am aware, hardly anyone will ever have access to JTAG tools to connect there.

    The factory may have been told to allow solder on that set of ports as part of the wave soldering screen,

    since it is not used by users.

    The small set near P1 (closest to the "Made in China" label ideally should not be covered in solder,

    but only affects you if you were planning to solder something there.

    For those that are planning to solder a connector there, the solder can be manually removed.

    Personally I would not return a device for that reason, but not everyone is familiar with solder removal

    methods, so possibly the procedure may be difficult for some if all 8 of those holes are plugged up.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago

    seems to be a heep more solder on the china ones compaired to the UK version, just finished soldering my Pi Cobbler(first ever solder project) and i too have blobs on pins image but i will say when my RPI arrived it made a huge differance to actually see something that was made in the UK rather than from china,

     

    long and the short of it, so glad my RPI is British image and i'm crap at soldering image

     

     

    EDIT: zidane1980 i notice that your "made in china) is a sticker, have you tried removing the "Sticker" to see what it says under it? image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    I have one that seems to have the same problem that Ron Niessen is experiencing.

    I'm in USA, and I received 2 units 3 days ago. One is just fine, but the other crashes after a short period of operation. (Between 1 and 10 minutes.)

    When it crashes, my HDMI display shows a "no signal" message, and all of the RPi indicator LEDs extinguish except for PWR. It takes a power cycle to bring it back to life.

    The crash seems to come more quickly if I'm running X.

    For the voltage measurements across TP1-TP2, the bad unit seems to settle at about 4.79, while the good one settles at about 4.83 after booting.

    While watching the DMM during boot, I did see measurements as low as 4.59 on the bad one, but never below 4.7 on the good one. However, these readings might not mean much because of the meter's sampling and averaging rates with respect to the rapidly changing measured value.

    When I use the other unit with the exact same connections, power supplies, and SD card, it has no such problem, and has run all night a couple of times.

    (Wheezy has some memory leaks somewhere, but that's a different issue.)

    I have not tried the frozen rhubarb, though. (Raspberry-Rhubarb Pi(e), anyone?)

    The vitals from the bad unit:

    serial 5b5e497a

    date: 1236

    revison: 000f

    bottom label: E4612RS2V13B1.0

    This one is also made in China.

     

    BTW, the good one is also made in China, date code 1238.

    I requested an RMA on the website yesterday, so I hope the exange will be easy.

     

    Edit: I don't see any obvious production quality issues on either of mine. On both units, 3 of the P5 holes are filled with solder, and all of the P2 holes are filled. But I don't know how this was specified for production.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    John Burt wrote:

     

    When I use the other unit with the exact same connections, power supplies, and SD card, it has no such problem, and has run all night a couple of times.

    Just a datapoint, for an older, original version, made in china board:

     

    root@raspberry-pi:~# uptime

    11:22:27 up 62 days, 16:19,  3 users,  load average: 0.16, 0.05, 0.06

     

    I'm not using the new turbo-mode firmware or kernel, but as it originated as Arch it's overclocked to 800Mhz anyway. TP1-TP2 is 5.00v as I'm supplying power via P1. I also have a load of I2C sensors and stuff hanging off it and it's not had a problem.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • comfortmd
    comfortmd over 13 years ago

    got one from china, has the P5 holes filled (the four holes closest to the outside edge).  my multimeter has gone walkabout so i can't check voltages, but it has crashed repeatedly when running xmbc, running temp 120-153 while it is on.  i do not know how much of a problem this is, but i hope someone would enlighten me if it is.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    I have exactly the same problem with a Pi that I ordered from Newark in late November. It is made in China, has some unpopulated component holes filled with solder. Otherwise it looks fine even under a microscope. I tested multiple power supplies, monitored them on a scope under load using advanced trigger etc, no problems there. When the Pi randomly crashes the screen goes blank, all the time the power LED is still lit. Sometimes the Flash LED is lit. I bypassed the polyfuse by connecting 5.00VDC between test points 1 and 2. Same behavior. Tried reflashing etc. I am going to return it now. Hopefully I can get a new one in a reasonable amount of time.

     

    AZ

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • andycrofts
    andycrofts over 13 years ago

    Bit miffed myself. got my Pi from "the Other Place", put sd card in, turned it over to put in the case, card fell out. Realised the card socket was faulty. Back to RS for replacement, after a month of waiting for warranty return, got another - also Chinese - one, exactly same problem.
    Nonetheless, try to fit it into RS white case. No joy, all connector holes misaligned, the SD hole looked like it'd been chewed out by rats*.
    Oh, well, I guess I'll find a REAL SD socket, and solder it in myself.
    I really wanted it to try on this project: http://www.ubioulu.fi/sites/default/files/UbiCity_Herneoja_090502.pdf
    They're using big 100 W+ Windows PC's inside, and with research, I reckon I could get all on a Pi. Time's running out, tourist season in a couple of months. Being unemployed, I reckon I've time to 'fiddle'....


    (works fine with SD held in with a rubber band and a clothes peg. looks funny, but it's a lovely machine!

     

    * I reckon the case manufacturers used my previous Engineering Managers method of manufacturing....
    "Measure it with a micrometer, mark it with chalk, then hew it out with a blunt axe"

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • element14Dave
    element14Dave over 13 years ago

    Just to let everyone know as of March 15, 2013 all of our Raspberry Pi's are being manufactured in the UK...here is a link to the story from the Inquirer .

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to element14Dave

    Dave,

      One of the interesting points in that article is that Element14 now has someone

    (Claire Doyle) with the title: "global head of Raspberry Pi at Element14", who is

    apparently replacing Mike Buffham (global head of EDE at Premier Farnell) as the

    main press point of contact for RPi issues.  Perhaps Ms. Doyle could be invited to

    participate occasionally in E14's RPi discussion group, given her interest in RPi.

     

    The article isn't clear as to whether the shutdown of E14's China RPi factories was

    accompanied by a corresponding increase in the production rate at the Wales factory.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to element14Dave

    Greetings,  I have a RevB board (made in the UK - smile) and the SD Card Socket broke on it.  What is the recommended replacement part so I can make it operational again?  And I'd be glad to upgrade the socket to a sturdier one.

     

    thanks,

    --joe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<