How easy is it to connect a Pi to a Laptop and use that Laptop's screen as the Pi's display unit ?
How easy is it to connect a Pi to a Laptop and use that Laptop's screen as the Pi's display unit ?
I've not tried it on a pi, but one reasonable way is to run an 'X Server' on your laptop.
There are a few X servers available for free, but some are flaky. Maybe try the Cygwin one.
Once the server is running (it sounds counter-intuitive, but the laptop client is actually
running the X server) then the pi will be able to communicate to the laptop's X Server
via the network connection.
If you meant to do just a 'screen capture' style of thing, then you could use the
composite analog video out with a 'capture card' type of thing, but this is not the same
experience as an X server.
If your use-case is to be able to see video-related content (e.g. images and video) from your
pi on your laptop, then I'd suggest some alternate method, for example video streaming over
the network.
If the use-case is to be able to write software for the pi, then you don't really need to see the
desktop of the pi. You could just write the code on your laptop, and use secure file transfer
and secure shell to transfer it to the pi and execute it.
You can also use VNC. I run my pi's headless, but on the odd occasion I want to see a screen I just start the vncserver.
I ssh'd and and did
sudo apt-get install tightvncserver
followed the prompts,
then did
tightvncserver
the first time you run it it will ask you to set a password - enter what you want, but remember it
it will respond with something like
New 'X' desktop is <your raspi hostname>:<display number>
then on your vncclient
tell it to connect to either
<your raspi hostname>:<display number>
if it says it can't find that, then just
<your raspi hostname>
but change the port to
5900 + <display number>
so if <display number> is 1
so the port would be 5901 not the default 5900
the password will be the password you entered when you started the server
I hope this makes sense to you
Mike
You can also use VNC. I run my pi's headless, but on the odd occasion I want to see a screen I just start the vncserver.
I ssh'd and and did
sudo apt-get install tightvncserver
followed the prompts,
then did
tightvncserver
the first time you run it it will ask you to set a password - enter what you want, but remember it
it will respond with something like
New 'X' desktop is <your raspi hostname>:<display number>
then on your vncclient
tell it to connect to either
<your raspi hostname>:<display number>
if it says it can't find that, then just
<your raspi hostname>
but change the port to
5900 + <display number>
so if <display number> is 1
so the port would be 5901 not the default 5900
the password will be the password you entered when you started the server
I hope this makes sense to you
Mike