Raspberry Pi Forum question about the Debian preloaded SD card
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 684 subscribers
  • Views 1330 views
  • Users 0 members are here
  • raspberry_pi
Related

question about the Debian preloaded SD card

ykwong
ykwong over 13 years ago

I recently bought a model B RaspPi and a Debian preloaded SD Card (4G) from Element14. 

Booting up is ok, though I have not really tried to use it long enough to see if it has any voltage drop or heat problem. 

 

My question is :

I do not want to damage (or alter the original state of) my one-and-only-one o/s preloaded SD card.  So I bought a blank 4G SD card and try to make a duplicate and from there I intend to use the duplicate only.  By the way, having a duplicate card is also handy when I decide to buy one more Rasp-Pi.

 

I found that if I use my duplicated SD Card, the bootup is not successful, it will not stop at the Linux prompt that allows me to start the X Window.  It stops midway in the bootup process and I have no choice but to switch the power off.

 

Obviously, I think my method of the card duplication was wrong. Here is how I duplicated the SD card.

I inserted the original in my Mac (which has a built-in SD card slot),

I copied all the files (these are not images file already as the card is bootable) from the original SD into a folder on my Mac harddisk.

Then I inserted the blank 4G SD card in my Mac, and copy those files back from the harddisk to the SD card.

 

I probably did it the wrong way or this method will never duplicate the card successfully.

 

What would be the correct way to do what I want to achieve?

 

I am grateful to any advice, information, comments....

  • Sign in to reply
  • Cancel
Parents
  • gdstew
    gdstew over 13 years ago

    Here is a version of the instructions for using dd  to write the image file using Linux that I modified to include reading the image. Note that BSD uses a

    different naming convention for block devices than Linux does but after substituting the BSD versions it should work. Also note that these image files

    can be => 2 GB in size.

     

    1.  Run df -h to see what devices are currently mounted

    2.  If your computer has a slot for SD cards, insert the card. If not, insert the card

         into an SD card reader, then connect the reader to your computer.

    3.  Run df -h again. The device that wasn't there last time is your SD card. The left

         column gives the device name of your SD card. It will be listed as something like

         "/dev/mmcblk0p1" or "/dev/sdd1". The last part ("p1" or "1" respectively) is the

         partition number, but you want to read and write to the whole SD card, not just one

         partition, so you need to remove that part from the name (getting for example

         "/dev/mmcblk0" or "/dev/sdd") as the device for the whole SD card. Note that the

         SD card can show up more than once in the output of df: in fact it will if you

         have previously written a Raspberry Pi image to this SD card, because the RPi SD

         images have more than one partition.

    4.  Now that you've noted what the device name is, you need to unmount it so that files

         can't be read or written to the SD card while you are copying over the SD image.

         So run the command below, replacing "/dev/sdd1" with whatever your SD card's

         device name is (including the partition number)

          * umount /dev/sdd1

          * If your SD card shows up more than once in the output of df due to having

             multiple partitions on the SD card, you should unmount all of these partitions.

    5.  In the terminal read the image to the card with this command, making sure you

         replace the input file if= argument "/dev/sdd" with the right device name and the

         output file of= argument with the path and name of your .img file. Make sure the

         device name is the name of the whole SD card as described above, not just a

         partition of it (for example, sdd, not sdds1 or sddp1, or mmcblk0 not mmcblk0p1)

          * dd bs=1M if=/dev/sdd of=RP_debian.img

          * Note that if you are not logged in as root you will need to prefix this with sudo

          * The dd command does not give any information of its progress and so may appear

             to have frozen. If your card reader has an LED it may blink during the read

             process, or you can run pkill -USR1 -n -x dd in another terminal (prefixed

             with sudo if you are not logged in as root).

    6.  To write the image to the card use this command, making sure you replace the input

         file if= argument with the path and name of your .img file, and the "/dev/sdd" in the

         output file of= argument with the right device name (this is very important: you will lose

         all data on the hard drive on your computer if you get the wrong device name). Make

         sure the device name is the name of the whole SD card as described above, not just

         a partition of it (for example, sdd, not sdds1 or sddp1, or mmcblk0 not mmcblk0p1)

          * dd bs=1M if=RP_debian.img of=/dev/sdd

          * Note that if you are not logged in as root you will need to prefix this with sudo

          * The dd command does not give any information of its progress and so may appear

             to have frozen. It could take more than five minutes to finish writing to the

             card. If your card reader has an LED it may blink during the write process, or

             you can run pkill -USR1 -n -x dd in another terminal (prefixed with sudo if you

             are not logged in as root).

    7.  As root run the command sync or if a normal user run sudo sync (this will ensure the

         write cache is flushed and that it is safe to unmount your SD card)

    8.  Remove SD card from card reader, insert it in the Raspberry Pi, and have fun

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • ykwong
    ykwong over 13 years ago in reply to gdstew

    Thanks Gary.
    I am going to copy and paste your instruction to an rtf file first and make a hardcopy so that I can cross-reference when I am trying out the dd approach.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • ykwong
    ykwong over 13 years ago in reply to gdstew

    Thanks Gary.
    I am going to copy and paste your instruction to an rtf file first and make a hardcopy so that I can cross-reference when I am trying out the dd approach.