I recently bought a model B RaspPi and a Debian preloaded SD Card (4G) from Element14.
Booting up is ok, though I have not really tried to use it long enough to see if it has any voltage drop or heat problem.
My question is :
I do not want to damage (or alter the original state of) my one-and-only-one o/s preloaded SD card. So I bought a blank 4G SD card and try to make a duplicate and from there I intend to use the duplicate only. By the way, having a duplicate card is also handy when I decide to buy one more Rasp-Pi.
I found that if I use my duplicated SD Card, the bootup is not successful, it will not stop at the Linux prompt that allows me to start the X Window. It stops midway in the bootup process and I have no choice but to switch the power off.
Obviously, I think my method of the card duplication was wrong. Here is how I duplicated the SD card.
I inserted the original in my Mac (which has a built-in SD card slot),
I copied all the files (these are not images file already as the card is bootable) from the original SD into a folder on my Mac harddisk.
Then I inserted the blank 4G SD card in my Mac, and copy those files back from the harddisk to the SD card.
I probably did it the wrong way or this method will never duplicate the card successfully.
What would be the correct way to do what I want to achieve?
I am grateful to any advice, information, comments....