Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi loses ethernet
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 28 replies
  • Subscribers 711 subscribers
  • Views 10368 views
  • Users 0 members are here
  • raspberry_pi
Related

Raspberry Pi loses ethernet

e14 Contributor
e14 Contributor over 13 years ago

Hello there.

After several attempts to search this forum and not having found a solution, I decided to create a new discussion.

 

My Raspberry is a headless setup with a disk (externally powered) that I use as a downloader (transmission) and a file server (samba).

Sometimes it works for days in a row, sometimes it gets stuck and does not even acquire an IP address.

 

When it does not have an IP address I cannot determine what is wrong.

I have it plugged in to my router, the lights on the board itself light up and the light of the router that says it is connected also lights up.

The router does not recognise the Pi (it is not shown at the DHCP client list) and the Pi cannot ping the router.

Also, the Pi sees if the cable is removed. (the lights turn off and dmesg says eth0 is unplugged).

 

/etc/network/interfaces has dhcp enabled (although when I try to convert it to static and reboot the Pi says it has an IP address but cannot even ping the router and the router does not find it)

/etc/resolv.conf also has my router IP

 

I am at a deadend. If anyone could help me I would really appreciate it.

 

PS. I also used my multimeter at the TP1 TP2 connectors and got a result of 4.99V.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 12 years ago

    Ok, I've now run my old RasPi with the SD card built on the new failing one and powered the old one by the new power supply, result - no ethernet dropout after running for about 4 hours (the new RasPi fails in about 4 mins).  I think I've now established to my satisfaction that there is something seriously wrong with my new RasPi and there is no other unit, power supply, SD card, ethernet router, ethernet cables etc etc that is the problem. 

    In both cases the only connection to either RasPi is an ethernet connection, no USB, no HDMI, absolutely nothing but the power supply.  So if anyone else gets the ethernet dropout problem one of the possible causes can be the RasPi itself.  Of course in some cases it could be the power supply or any of the other diagnosis mentioned in this thread but the RasPi being the problem is a possibility.  I hope that helps.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 12 years ago

    Ok, I've now run my old RasPi with the SD card built on the new failing one and powered the old one by the new power supply, result - no ethernet dropout after running for about 4 hours (the new RasPi fails in about 4 mins).  I think I've now established to my satisfaction that there is something seriously wrong with my new RasPi and there is no other unit, power supply, SD card, ethernet router, ethernet cables etc etc that is the problem. 

    In both cases the only connection to either RasPi is an ethernet connection, no USB, no HDMI, absolutely nothing but the power supply.  So if anyone else gets the ethernet dropout problem one of the possible causes can be the RasPi itself.  Of course in some cases it could be the power supply or any of the other diagnosis mentioned in this thread but the RasPi being the problem is a possibility.  I hope that helps.