Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi loses ethernet
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 28 replies
  • Subscribers 711 subscribers
  • Views 10368 views
  • Users 0 members are here
  • raspberry_pi
Related

Raspberry Pi loses ethernet

e14 Contributor
e14 Contributor over 13 years ago

Hello there.

After several attempts to search this forum and not having found a solution, I decided to create a new discussion.

 

My Raspberry is a headless setup with a disk (externally powered) that I use as a downloader (transmission) and a file server (samba).

Sometimes it works for days in a row, sometimes it gets stuck and does not even acquire an IP address.

 

When it does not have an IP address I cannot determine what is wrong.

I have it plugged in to my router, the lights on the board itself light up and the light of the router that says it is connected also lights up.

The router does not recognise the Pi (it is not shown at the DHCP client list) and the Pi cannot ping the router.

Also, the Pi sees if the cable is removed. (the lights turn off and dmesg says eth0 is unplugged).

 

/etc/network/interfaces has dhcp enabled (although when I try to convert it to static and reboot the Pi says it has an IP address but cannot even ping the router and the router does not find it)

/etc/resolv.conf also has my router IP

 

I am at a deadend. If anyone could help me I would really appreciate it.

 

PS. I also used my multimeter at the TP1 TP2 connectors and got a result of 4.99V.

  • Sign in to reply
  • Cancel
Parents
  • danringer
    danringer over 10 years ago

    I've had the same problem but only with wifi usb dongles, I've found the ethernet jack to be extremely stable. Try newest os and a higher output power supply.  Maybe a heat sink?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • danringer
    danringer over 10 years ago

    I've had the same problem but only with wifi usb dongles, I've found the ethernet jack to be extremely stable. Try newest os and a higher output power supply.  Maybe a heat sink?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to danringer

    A better USB cable may be the answer rather than a higher output power adapter, it is well known that bad usb cables are well known for causing issues with PI's