Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Possible to use Microsoft wireless keyboard?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 705 subscribers
  • Views 874 views
  • Users 0 members are here
  • raspberry_pi
Related

Possible to use Microsoft wireless keyboard?

e14 Contributor
e14 Contributor over 13 years ago

I booted up the Raspberry Pi and made it to the configuration screen but couldn't control anything by the keyboard. I was using a a wireless microsoft keyboard that was connected through a wireless hub.

 

Do I have to use a wired keyboard for setup? Or how can I get this one to work for my needs

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    Keyboards that work or not with the Pi can be somewhat of a mystery.  I have a pretty standard wired USB keyboard from a Dell desktop that used to work fine with the Pi, but after some regular updates it totally stopped working (still works on a Linux PC).

     

    The Pi seems to miss some key down or key up events for some keyboards which results in dropped or repeated keys (or missing mouse clicks from mice).  A fix for that is to force USB 1.1 by adding dwc_otg.speed=1 to the end of the one long line in /boot/cmdline.txt (make sure that line does not wordwrap).  Forcing USB 1.1 may reduce network speed and speed of USB flash or hard drives, but is still faster than my 6 mbps DSL internet.

     

    I had to do that for my older Logitech di Novo Edge wireless keyboard/mousepad, and that works as well for new Logitech K400 wireless keyboard/mousepad.  And a nice thing about the K400 is that I was also able (to use Windows) to associate a Logitech wireless mouse to its unifying receiver (quake3 is tough to play with a mousepad).  Either of those wireless keyboard dongles works along with a mini-WiFi directly on the Pi USB ports

     

    However, what should have been a nice little GearHead wireless keyboard/mousepad (KB3800TPW) that someone else reported as working, does not work at all for me.  It totally disrupts USB whether connected directly, or on a powered USB hub.  It works fine on a Linux desktop PC, just not on any of my 3 Raspberry Pi.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago

    Keyboards that work or not with the Pi can be somewhat of a mystery.  I have a pretty standard wired USB keyboard from a Dell desktop that used to work fine with the Pi, but after some regular updates it totally stopped working (still works on a Linux PC).

     

    The Pi seems to miss some key down or key up events for some keyboards which results in dropped or repeated keys (or missing mouse clicks from mice).  A fix for that is to force USB 1.1 by adding dwc_otg.speed=1 to the end of the one long line in /boot/cmdline.txt (make sure that line does not wordwrap).  Forcing USB 1.1 may reduce network speed and speed of USB flash or hard drives, but is still faster than my 6 mbps DSL internet.

     

    I had to do that for my older Logitech di Novo Edge wireless keyboard/mousepad, and that works as well for new Logitech K400 wireless keyboard/mousepad.  And a nice thing about the K400 is that I was also able (to use Windows) to associate a Logitech wireless mouse to its unifying receiver (quake3 is tough to play with a mousepad).  Either of those wireless keyboard dongles works along with a mini-WiFi directly on the Pi USB ports

     

    However, what should have been a nice little GearHead wireless keyboard/mousepad (KB3800TPW) that someone else reported as working, does not work at all for me.  It totally disrupts USB whether connected directly, or on a powered USB hub.  It works fine on a Linux desktop PC, just not on any of my 3 Raspberry Pi.