Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum My Christmas RPi is rockin, my Wi-Pi..not so much. What am I doing wrong....
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 14 replies
  • Subscribers 707 subscribers
  • Views 2298 views
  • Users 0 members are here
  • raspi-config
  • raspberry_pi
  • wipi
  • raspberry_pi_accessories
Related

My Christmas RPi is rockin, my Wi-Pi..not so much. What am I doing wrong....

e14 Contributor
e14 Contributor over 13 years ago

Because I know it's something I'm doing wrong.

 

I saw the Adafruit video of the Motorola Atrix lapdock being used with the RPi and I thought "gotta do that". So I made the cable and for the first time powered up my Christmas RPi and it worked perfectly. I had downloaded the Wheezy (2012-10-28) image off the RPi Foundation site and burned an SD card and it all worked bloody perfect.  Then I installed the Wi-Pi and ground to a halt as I tried to figure out why the WiPi refused to work. I followed the PDF instructions on the Element14 site and modified the 'interfaces' file and checked it a bunch of times but no go. The indicator light on the WiPi is not on and although it appears the OS is sensing the dongle it does not appear to be able to connect to the access point.

Here's what I appended in the interfaces file;

 

 

auto wlan0

iface wlan0 inet dhcp

wpa-ssid Le-Mars

wpa-psk #############   (this was the actual password)

 

 

Oct 28 22:59:47 raspberrypi kernel: [    3.283301] usb 1-1.2: new high-speed USB device number 4 using dwc_otg
Oct 28 22:59:47 raspberrypi kernel: [    3.411226] usb 1-1.2: New USB device found, idVendor=148f, idProduct=5370
Oct 28 22:59:47 raspberrypi kernel: [    3.423516] usb 1-1.2: New USB device strings: Mfr=1, Product=2, SerialNumber=3
Oct 28 22:59:47 raspberrypi kernel: [    3.437190] usb 1-1.2: Product: 802.11 n WLAN
Oct 28 22:59:47 raspberrypi kernel: [    3.446827] usb 1-1.2: Manufacturer: Ralink
Oct 28 22:59:47 raspberrypi kernel: [    3.456369] usb 1-1.2: SerialNumber: 1.0
Oct 28 22:59:47 raspberrypi kernel: [    3.563310] usb 1-1.3: new high-speed USB device number 5 using dwc_otg
Oct 28 22:59:47 raspberrypi kernel: [    3.693815] usb 1-1.3: New USB device found, idVendor=0424, idProduct=2517
Oct 28 22:59:47 raspberrypi kernel: [    3.715064] usb 1-1.3: New USB device strings: Mfr=0, Product=0, SerialNumber=0

The router is looking for 802.11g using WPA. It can output 'n' as well but my old Mac Mini gets extra stupid when 'n' packets are mixed into the stream.

this is a snippet of the bootup syslog which (I think) shows that the RPi is seeing the WiPi however later when it tries to do a DHCP it fails out completly.

 

I also measured the voltage between TP1 and TP2 and it showed 4.80v with the WiPi in and 4.85v with it out. The lapdock certainly appears to be delivering solid power to the RPi with the added benefit of battery backup power for 'free'.

 

I'm kinda stumped and I don't know where to go If anybody has got any ideas I would be extremely gratefull.

 

 

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    Hello Paul

     

    I too have invested in a WiPi and thought I'd got things working perfectly the other night.

     

    I've also implemented some VNC Software on my Pi and Windows7 Laptop, with the intention of being able to connect wirelessly once the Pi has booted up.

     

    Located the Pi elsewhere in the House this evening, plugged it in and it's not connecting to my Hub at all !!!!

     

    I don't have a Monitor readily available at that location so can't check what might be going wrong but wondered if you might have worked out if removing the entries in the Interfaces File really does enable it to connect properly at Bootup, once the initial setup in the Wireless Config has been done properly ?

     

    Regards

     

    Andy

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Hi Andy,

     

    all I can do is tell you what works for my RasPi running Raspbian 2012-12-16 Wheezy. WiFI Config writes to a file called wpa_supplicant.conf and once my Wifi parameters were written to this file my RasPi accessed my router from that moment on including subsequent reboots. The interfaces file appeared to have no effect on the WiPi and so I deleted the entries that the WiPi install instructions specified. Apparently this version Rasbian has the drivers for this dongle preloaded.

     

    Here is my copy of wpa_supplicant.conf as written/created by WiFi Config (BTW, I've overwritten the PSK with '*' (Yep, Debian keeps WiFi passkeys in plaintext. Very secure)).

     

    ctrl_interface=DIR=/var/run/wpa_supplicant GROUP=netdev

    update_config=1

     

    network={

         ssid="Le-Mars"

         psk="************"

         proto=WPA

         key_mgmt=WPA-PSK

         pairwise=TKIP

         group=TKIP WEP104 WEP40

         auth_alg=OPEN

    }

     

    network={

         ssid="Le-Mars"

         psk="************"

         proto=WPA

         key_mgmt=WPA-PSK

         pairwise=TKIP

         auth_alg=OPEN

    }

     

    All I know is that once this file was written, all my WiFi networking issues went away. Now bear in mind, I'm a noob and this file apparently can really screw up your install if it's syntax is even a teeny bit wrong. I strongly suggest you let WiFi config do the heavy lifting as far as writing this file is concerned unless your a hardcore Linux wrangler.

     

    BTW on the subject of portable monitors I got a Motorola Atrix lapdock, cables from Amazon and made up the mutant cable as shown by Adafruit (apparently this is unecissary on the latest RasPi). It works like a dream with the benefit that the RasPi is battery portable, although the Lego RasPi case stands out a bit at Starbucks image.

     

    regards,

     

    Paul.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Thanks very much for the feedback Paul.

     

    I think I caused myself a problem as it happens, as I noticed the WiPi Blue light wasn't on after a reboot and couldn't see the Pi via my Wireless Hub management console either.

     

    I'd plugged in a separate Wireless Dongle that I intend to use for a Wireless Sensor Network I intend to introduce and hadn't realised the Pi O/S would recognise it immediately at boot-up and introduce some Config changes to accommodate that additional Peripheral.

     

    Once I removed that and rebooted again the WiPi was recognised correctly by the Pi and the Pi appeared in my Wireless Hub management console.

    As I've also deployed UltraVNC to both the Pi and my Windows7 Laptop, I suspect something about VNC on the Pi has also been corrupted/reconfigured as I still cannot connect to the Pi from the Laptop.

     

    I will have to bring everything back downstairs tomorrow evening, connect the Pi to my LCD TV via the HDMI Port and check everything again to restore things I think.

     

    It's all good fun though and infact this aspect of trial and error will contribute positively to a Project I have planned for one of my Degree Modules - I'm currently getting ahead with things before my Module starts in late January and will be able to document my experiences retrospectively.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Thanks very much for the feedback Paul.

     

    I think I caused myself a problem as it happens, as I noticed the WiPi Blue light wasn't on after a reboot and couldn't see the Pi via my Wireless Hub management console either.

     

    I'd plugged in a separate Wireless Dongle that I intend to use for a Wireless Sensor Network I intend to introduce and hadn't realised the Pi O/S would recognise it immediately at boot-up and introduce some Config changes to accommodate that additional Peripheral.

     

    Once I removed that and rebooted again the WiPi was recognised correctly by the Pi and the Pi appeared in my Wireless Hub management console.

    As I've also deployed UltraVNC to both the Pi and my Windows7 Laptop, I suspect something about VNC on the Pi has also been corrupted/reconfigured as I still cannot connect to the Pi from the Laptop.

     

    I will have to bring everything back downstairs tomorrow evening, connect the Pi to my LCD TV via the HDMI Port and check everything again to restore things I think.

     

    It's all good fun though and infact this aspect of trial and error will contribute positively to a Project I have planned for one of my Degree Modules - I'm currently getting ahead with things before my Module starts in late January and will be able to document my experiences retrospectively.