Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum My Christmas RPi is rockin, my Wi-Pi..not so much. What am I doing wrong....
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 14 replies
  • Subscribers 707 subscribers
  • Views 2297 views
  • Users 0 members are here
  • raspi-config
  • raspberry_pi
  • wipi
  • raspberry_pi_accessories
Related

My Christmas RPi is rockin, my Wi-Pi..not so much. What am I doing wrong....

e14 Contributor
e14 Contributor over 13 years ago

Because I know it's something I'm doing wrong.

 

I saw the Adafruit video of the Motorola Atrix lapdock being used with the RPi and I thought "gotta do that". So I made the cable and for the first time powered up my Christmas RPi and it worked perfectly. I had downloaded the Wheezy (2012-10-28) image off the RPi Foundation site and burned an SD card and it all worked bloody perfect.  Then I installed the Wi-Pi and ground to a halt as I tried to figure out why the WiPi refused to work. I followed the PDF instructions on the Element14 site and modified the 'interfaces' file and checked it a bunch of times but no go. The indicator light on the WiPi is not on and although it appears the OS is sensing the dongle it does not appear to be able to connect to the access point.

Here's what I appended in the interfaces file;

 

 

auto wlan0

iface wlan0 inet dhcp

wpa-ssid Le-Mars

wpa-psk #############   (this was the actual password)

 

 

Oct 28 22:59:47 raspberrypi kernel: [    3.283301] usb 1-1.2: new high-speed USB device number 4 using dwc_otg
Oct 28 22:59:47 raspberrypi kernel: [    3.411226] usb 1-1.2: New USB device found, idVendor=148f, idProduct=5370
Oct 28 22:59:47 raspberrypi kernel: [    3.423516] usb 1-1.2: New USB device strings: Mfr=1, Product=2, SerialNumber=3
Oct 28 22:59:47 raspberrypi kernel: [    3.437190] usb 1-1.2: Product: 802.11 n WLAN
Oct 28 22:59:47 raspberrypi kernel: [    3.446827] usb 1-1.2: Manufacturer: Ralink
Oct 28 22:59:47 raspberrypi kernel: [    3.456369] usb 1-1.2: SerialNumber: 1.0
Oct 28 22:59:47 raspberrypi kernel: [    3.563310] usb 1-1.3: new high-speed USB device number 5 using dwc_otg
Oct 28 22:59:47 raspberrypi kernel: [    3.693815] usb 1-1.3: New USB device found, idVendor=0424, idProduct=2517
Oct 28 22:59:47 raspberrypi kernel: [    3.715064] usb 1-1.3: New USB device strings: Mfr=0, Product=0, SerialNumber=0

The router is looking for 802.11g using WPA. It can output 'n' as well but my old Mac Mini gets extra stupid when 'n' packets are mixed into the stream.

this is a snippet of the bootup syslog which (I think) shows that the RPi is seeing the WiPi however later when it tries to do a DHCP it fails out completly.

 

I also measured the voltage between TP1 and TP2 and it showed 4.80v with the WiPi in and 4.85v with it out. The lapdock certainly appears to be delivering solid power to the RPi with the added benefit of battery backup power for 'free'.

 

I'm kinda stumped and I don't know where to go If anybody has got any ideas I would be extremely gratefull.

 

 

  • Sign in to reply
  • Cancel
Parents
  • wallarug
    wallarug over 13 years ago

    auto wlan0

    iface wlan0 inet dhcp

    wpa-ssid Le-Mars

    wpa-psk #############   (this was the actual password)

    You need to use inverted commas like so:

    auto wlan0

    iface wlan0 inet dhcp

    wpa-ssid "Le-Mars"

    wpa-psk "#############"

    Hope this helps.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • wallarug
    wallarug over 13 years ago

    auto wlan0

    iface wlan0 inet dhcp

    wpa-ssid Le-Mars

    wpa-psk #############   (this was the actual password)

    You need to use inverted commas like so:

    auto wlan0

    iface wlan0 inet dhcp

    wpa-ssid "Le-Mars"

    wpa-psk "#############"

    Hope this helps.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to wallarug

    Thanks for the reply Fergus.

     

    I put double quotation marks around the ssid and the passkey as you suggested and saved and then rebooted. Unfortunatly there was no difference in the outcome. The RPi still didn't have access to the network. I checked the interfaces file to make sure that I had indeed saved the file correctly and it was as I had edited it. Then I had a thought, I'll go into Xwindows and see if I can access the WiPi via the application on the desktop. Sure enough I was able to do a scan of the local access points and I found mine. Then I selected it and typed in my passkey and 'bingo', network access and the little blue light on the WiPi was mine. The browsers worked and everything. Then I exited out of Xwindows and the network access persisted as demonstrated by pinging the router from the command line. So then I rebooted and sure enough, the WiPi initialized immediatly and I was linked to my access point. So I checked the interfaces file and it was exactly as I had left it before going into Xwindows. In fact just as a test I purposely broke the SSid and Psk entries in the Wlan0 section and rebooted. It made no difference. The RPi connected to my access point without a problem. Then I deleted the whole Wlan0 entry as shown in the install PDF. Obviously the RPi/Wheezy is not looking in the interfaces file for it's login information.

     

    So now I have two questions for the engineers at Element 14;

     

    1, what did the Xwindows WiFi application modify (because it wasn't the interfaces file) to enable the WiPi to work on the latest version of the RPi/Wheezy.

    2, Did anybody at Element14 actually tested the instructions PDF on the E14 website regarding the WiPi and the installation to the RPi because quite obviously they don't work, and don't get me started on the instructions that come in the E14 WiPi branded box.Those caused me to have to reflash my SD card because they wrecked the OS (not happy. Wasted an afternoon on this foolishness).

     

    I suspect that the instructions to install the WiPi on the current RPi are actually really simple.

     

    1, Use the latest version of Wheezy (if you don't you're on your own)

    2, Plug in the WiPi to the Raspberry Pi

    3, power up the RPi, log in and type 'startx'

    4, Doubleclick on 'WiFi Config'

    5, click on the Scan button

    6, Enter your passkey for your respective network security (probably WPA)

    7, click on the Close button.

    8, click on the Connect button.

    9, close the application.

     

    Thats it. You should see a blue light on the WiPi and you should be connected to your network.

     

    Trust me Element14, I really appreciate that the the WiPi is a staggeringly cheap product and offers excellent value for money. But the RPi is being sold to legions of noobs (even more nooby than me) and they are going to be frustrated as hell with this simple stuff. They will give up and stick the RPi in the drawer and you won't sell them tons more stuff for their little electric pal who's fun to be with.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 13 years ago in reply to e14 Contributor

    I'm glad you got it working.  Networking is often tricky and there are so many layers and protocols that sometimes it's hard to tell why something worked.  I'm speaking as someone who has implemented networking hardware and software -- but not wireless.

     

    At some point I may get a WiPi for my RasPi/Lapdock.  Quick question: is your WiPi plugged into a RasPi USB port or a Lapdock USB port?

     

    Thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to johnbeetem

    It's plugged directly into the RPi top USB slot, and it works perfectly. I read on another board that you don't want to plug the WiFi dongle into a hub and that it only works reliably if it's directly connected to the RPi. I have to say I am gobsmacked at how cool the Atrix lapdock works with the RPi. How it works out the correct screen res I do not know. It will be a bit of a giggle to take over the Lapdock/RPi and sit in Starbucks on battery power just like all the big kids do....

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 13 years ago in reply to e14 Contributor

    Paul Bryant wrote:

     

    ... How it works out the correct screen res I do not know...

    HDMI has an I2C link (signals SCL and SDA).  The HDMI generator asks the monitor what resolutions it supports and the monitor returns a list.  I think Lapdock only returns 1366 x 768.

     

    The only thing I had to do manually was to set "disable_overscan=1" in config.txt to use all the pixels.  If you have wide black bands around the used part of the screen you may want to try this.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to johnbeetem

    Ahh, so that's how. Nope, no big black bands. It figured it out all on it's own. Maybe it's because it's got a UK keyboard.....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Paul, et al:

       I struggled with this one for days and I thought I was home free after seeing Paul's 9 steps to WiPi WiFi bliss. Unfortunately the darn thing would try to connect a few times and then fail. I finally resorted to manual configuration by bypassing the WiFi Config app entirely:

     

    http://www.raspberrypi-tutorials.co.uk/set-raspberry-pi-wireless-network/  (starting mid-page at: $ sudo nano /etc/wpa.config)

     

    I had some issues typing in my WPA key, as I have some @ symbols included. Whenever I tried to type the @ symbol I got quotes ", but I soon figured out that trying to type the quotes " would give me @.

     

    That did the trick for me, but I was still intrigued (disappointed/ticked off) that the WiFi config app didn't work like it should. I came back to this thread and saw Paul's post about the wpa_supplicant.conf file, so I went back in to take a look at mine. I noticed that my psk= line had " where the @ should be. I was able to change it using my newly found key mapping workaround. I then put 2 and 2 together and realized that the WiFi config app hides the key when you type it in, so all you see is :*************. I realized that the WiFi config wasn't able to connect to my wireless network because it was recording the wrong password.

     

    I then found a post that shows you that the default mapping is for UK and they (my esteemed colleagues from across the pond) have the @ and " mappings reversed. Here's the link to remap your keyboard to US:

     

    http://raspberrypi.stackexchange.com/questions/1042/why-is-my-symbol-not-working  (don't forget to reboot to make the change stick!)

     

    I went back and reburned a fresh Wheezy image, changed the default keyboard to "us," rebooted, and then followed Paul's 9 steps. Worked like a charm.

     

    Thanks,

    BillyD

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Glad you got it working Bill.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

     

    Paul Bryant wrote:

     

    It's plugged directly into the RPi top USB slot, and it works perfectly. I read on another board that you don't want to plug the WiFi dongle into a hub and that it only works reliably if it's directly connected to the RPi. I have to say I am gobsmacked at how cool the Atrix lapdock works with the RPi. How it works out the correct screen res I do not know. It will be a bit of a giggle to take over the Lapdock/RPi and sit in Starbucks on battery power just like all the big kids do....

           Paul,

           I had my WiPi plugged into the USB port on the Pi and I was having problems, I plugged it into a powered hub (Belkin) and it works fine.  I checked the voltage (TP1-TP2) and it is 5.0. The Lapdock is the greatest!

     

           Bill, I think you have a German keyboard like I do.  It takes a little getting used to especially since it is marked like a US keyboard. Maybe someone knows how to change Debian from thinking it is German!



    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 13 years ago in reply to e14 Contributor

    George Golden wrote:

     

           Bill, I think you have a German keyboard like I do.  It takes a little getting used to especially since it is marked like a US keyboard. Maybe someone knows how to change Debian from thinking it is German!

    There are instructions for changing the default "gb" = Great Britain keyboard mapping to something else at the RasPi Troubleshooting Wiki.  The instructions are for Debian Squeeze, but may work with Wheezy.