Raspberry Pi Forum Pi-View HDMI VGA converter problem
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 686 subscribers
  • Views 4288 views
  • Users 0 members are here
  • pi
  • raspberry_pi
  • adapter
  • vga
Related

Pi-View HDMI VGA converter problem

Former Member
Former Member over 13 years ago

Hello all,

Please bear with me as I am new to this. I have run my RPi on my home TV using a HDMI to HDMI cable.

However for working in school, I have bought the Pi-View HDMI-VGA converter and when I connect this to a 50/60HZ monitor I get the screen message;

"Attention signal frequency is out of range

H: 67.5kHz V: 60.5 kHz

Please change signal timing"

 

The Pi is powered via USB (phone lead) through a second PC and I have a steady green LED.

If I power the Pi via a powered USB hub, then I see an intermittent messgae;

"Attention no signal

Please check input signal or connection"

 

Can anyone please advise where I may be going wrong?

Thanks in advance.

 

Simon

  • Sign in to reply
  • Cancel
Parents
  • wmsundell
    wmsundell over 12 years ago

    Ok, just a suggestion, I read somewhere in one of the Rpi or BBB forums that you need to use a "powered" HDMI to VGA adapter, if you use one that is from Element 14, it will draw power from the Rpi's power supply.  So from reading that msg I realized the problems I had when using that adapter.  I got a Dell Genesis monitor and hooked the HDMI directly to the HDMI to DVI adapter and the problems went away.  I have not found a "powered" HDMI to VGA adapter yet since I found this monitor.

    Bill

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • wmsundell
    wmsundell over 12 years ago

    Ok, just a suggestion, I read somewhere in one of the Rpi or BBB forums that you need to use a "powered" HDMI to VGA adapter, if you use one that is from Element 14, it will draw power from the Rpi's power supply.  So from reading that msg I realized the problems I had when using that adapter.  I got a Dell Genesis monitor and hooked the HDMI directly to the HDMI to DVI adapter and the problems went away.  I have not found a "powered" HDMI to VGA adapter yet since I found this monitor.

    Bill