Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Can we connect Raspberry pi to old CRT television as monitor?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 709 subscribers
  • Views 3307 views
  • Users 0 members are here
  • raspberry_pi
Related

Can we connect Raspberry pi to old CRT television as monitor?

rufzalta
rufzalta over 13 years ago

What are the other options i have to connect as monitor. I have a VGA monitor but doesnot have HDMI converter. I can get display out of my mobile Nokia N-70, Car dvd,calculators etc..

  • Sign in to reply
  • Cancel
Parents
  • guzunty
    guzunty over 13 years ago

    There is another option. If you already have a regular desktop computer and you are willing to do a bit of command line work to set it up, you can use ssh to work on the Pi.

     

    You don't even need a keyboard or a mouse. You do need the Pi to be running a network connection, but that is part of the setup.

     

    http://www.adafruit.com/blog/2012/12/20/tutorial-adafruits-raspberry-pi-lesson-6-using-ssh-raspberry_pi-raspberrypi/

     

    EDIT: Actually, I just checked and (unusually for AdaFruit) this link probably isn't the best. It is using a funky serial cable. I use a plain ethernet connection since I want access to the internet from the Pi (and I think most people would). A quick Google for 'ssh -X' didn't produce anything that stood out as a connect-the-dots tutorial, sorry.

     

    The windows that would normally appear on the Pi display appear on your computers desktop instead.

     

    It's not a solution for everyone, since you don't get that Raspberry Pi desktop environment to launch programs. Instead you launch a terminal window and start programs that way. This arguably a better way to get used to the operating system anyway, its the way the Pro's do it. Another advantage is that you don't have the extra keyboard, monitor and mouse cluttering up your surfaces.

     

    Like I said, not for everyone, but it's the way I do it.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to guzunty

    > There is another option. If you already have a regular desktop computer and you are willing to do a bit of command line work to set it up, you can use ssh to work on the Pi.

     

    This implies that you are limited to using the command line for remote access.

    But actually you can use "X forwarding" or VNC for remote access using a GUI.

    Using X forwarding gives you X11 on the RPi without the usual slowness because

    the rendering is not done on the RPi.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to guzunty

    > There is another option. If you already have a regular desktop computer and you are willing to do a bit of command line work to set it up, you can use ssh to work on the Pi.

     

    This implies that you are limited to using the command line for remote access.

    But actually you can use "X forwarding" or VNC for remote access using a GUI.

    Using X forwarding gives you X11 on the RPi without the usual slowness because

    the rendering is not done on the RPi.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • guzunty
    guzunty over 13 years ago in reply to e14 Contributor

    Yup, I never intended to imply this was a command line only solution. What I meant was, 'you do need to do some initial command line work to get it set up'. Not so much after that.

     

    Once working, you have windows on the computer monitor exactly as if you were sitting at the Pi except, as coder27 says, with less load on the Pi because the host renders the windows.

     

    'ssh -X' Wouldn't be without it image

     

    In fact if you go all the way and set up Bonjour, you can just use:

     

    ssh -X raspberrypi.local -l username