Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum PiFace Problems
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 78 replies
  • Subscribers 717 subscribers
  • Views 12286 views
  • Users 0 members are here
  • raspberry_pi
  • piface
  • raspberry_pi_accessories
Related

PiFace Problems

keithtowns
keithtowns over 13 years ago

Am I missing something? I have two PiFace and 3 Raspberry Pi. I followed the instructions the get the PiFace working but have yet to succeed. I have tried the image provided as well as updating an existing Raspian image to no avail. I have also tried all my Pi and the two PiFace in all the combinations. I almost gave up but also tried a different power supply and SD card. None of the above got the emulator to switch on the LEDs and I could not do it through Python. Any ideas? I've spent hours on this, please tell me I've missed something. Thanks.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    Keith, you are not alone. The 'documentation' with the piface is worse than useless. I particularly like the typo on page 2 of the 'instructions' (etc/ which should be /etc/) and that if the emulator fails (I can't get it to work – ends with 'segmentation fault') the 'instructions' that follow are, again, useless. I will get it working in the end, but no thanks to the fools at man.ac.uk. How difficult would it have been to provide basic instructions in the box? Good luck with it - I'll reply back when I've finished arm-wrestling with it and got it doing something (I have a job in mind).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    ... not sure if urls are allowed here - if they are, here's some documentation for piface ...

     

    https://docs.google.com/folder/d/0B-UAZ9CyJCLGQjJ3RDlqa2pqaDg/edit?pli=1

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mrbuzzcut
    mrbuzzcut over 13 years ago in reply to keithtowns

    Did you get any error messages in the terminal window when you ran the emulator?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • keithtowns
    keithtowns over 13 years ago in reply to mrbuzzcut

    Hi Jeff

     

    No errors, the emulator window opens and says piface detected but nothing works. In the terminal window the cursor waits and returns to root@raspberrypi:~# once the emulator has been closed.

     

    Cheers

     

    Keith

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mrbuzzcut
    mrbuzzcut over 13 years ago in reply to keithtowns

    PiFace detected...that's a start. Did you click the override button?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to keithtowns

    Keith, can you run the commands I listed in post #8 and tell me the output? If you can see the SPI device files (/dev/spidev0.0 and /dev/spidev0.1) and running the Python shell commands doesn't error then it's probably an error with your board.

     

    Also, try reading from the board:

     

    $ python

    >>> import piface.pfio as p

    >>> p.digital_read(0)

     

    This should return a 1 or 0 value depending on whether the switch was pressed. So you should run the digital_read() command twice, once while holding the first switch and once while not. The returned values should be different. If they are the same even when you have held down the switch then it's a hardware fault.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • keithtowns
    keithtowns over 13 years ago in reply to e14 Contributor

    Hello Thomas

     

    The commands returned the following:

     

    root@raspberrypi:~# ls -l /dev/spidev*

    crw-rw---T 1 root spiuser 153, 0 Jan  1  1970 /dev/spidev0.0

    crw-rw---T 1 root spiuser 153, 1 Jan  1  1970 /dev/spidev0.1

     

    However, the input was more revealing:

     

    root@raspberrypi:~# python

    Python 2.7.3 (default, Jan 13 2013, 11:20:46)

    [GCC 4.6.3] on linux2

    Type "help", "copyright", "credits" or "license" for more information.

    >>> import piface.pfio as p

    >>> p.digital_read(0)

    Traceback (most recent call last):

      File "<stdin>", line 1, in <module>

      File "/usr/local/lib/python2.7/dist-packages/piface/pfio.py", line 249, in digital_read

        current_pin_values = read_input()

      File "/usr/local/lib/python2.7/dist-packages/piface/pfio.py", line 300, in read_input

        port, data = read(INPUT_PORT)

      File "/usr/local/lib/python2.7/dist-packages/piface/pfio.py", line 329, in read

        operation, port, data = send([(READ_CMD, port, 0xff)])[0] # send is expecting and returns a list

      File "/usr/local/lib/python2.7/dist-packages/piface/pfio.py", line 342, in send

        raise InitError("The pfio module has not yet been initialised. Before send(), call init().")

    piface.pfio.InitError: The pfio module has not yet been initialised. Before send(), call init().

    >>>

     

     

    Thanks

     

    Keith

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to keithtowns

    Ah, my bad. You need to initialised the pfio first.

     

    $ python

    >>> import piface.pfio as p

    >>> p.init()

    >>> p.digital_read(0)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • keithtowns
    keithtowns over 13 years ago in reply to mrbuzzcut

    Hi Jeff

     

    Yes I did click on the override enable and then all on/off and individual pins but nothing......

     

    Thanks anyway

     

    Keith

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • keithtowns
    keithtowns over 13 years ago in reply to e14 Contributor

    Hi Thomas

     

    I tried the code below:

     

    root@raspberrypi:/home/pi# python

    Python 2.7.3 (default, Jan 13 2013, 11:20:46)

    [GCC 4.6.3] on linux2

    Type "help", "copyright", "credits" or "license" for more information.

    >>> import piface.pfio as p

    >>> p.init()

    >>> p.digital_read(0)

    1

    >>> p.digital_read(1)

    1

    >>> p.digital_read(0)

    1

    >>> p.digital_read(1)

    1

    >>>

     

    For the first two tries, no button was pressed. For the second two, I pressed all the buttons.

     

    Cheers

     

    Keith

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • keithtowns
    keithtowns over 13 years ago in reply to e14 Contributor

    Hi Thomas

     

    Just tried the same again with my other Piface board, exactly the same results.

     

    Cheers

     

    Keith

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to keithtowns

    Where are your jumpers on the board in the correct place? They should both be on 0. Here is a picture I just took of my PiFace for reference.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to keithtowns

    Where are your jumpers on the board in the correct place? They should both be on 0. Here is a picture I just took of my PiFace for reference.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • keithtowns
    keithtowns over 13 years ago in reply to e14 Contributor

    Hi Thomas

     

    THAT FIXED IT!

     

    Both PiFace came with the jumpers set in the other position - THANK YOU! (and why would they do that?)

     

    I believe that Scratch needs an updated version to work with PiFace, is there anywhere I can download it from using my current version of Raspian?

     

    Thanks

     

    Keith

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to keithtowns

    Ah-ha! That's brilliant news! The jumper switches tell PiFace what number it is. With both set to 0, you tell PiFace that it's board 0. By default the Python module addresses board 0 so that's why it wasn't working when you had it set to whatever-else.

     

    I don't think you need an updated version of Scratch, you just need to enable Mesh. Here are some old instructions (I'll be honest, they need improving image). If you have any trouble then start a new thread and I'll try to help when I can.

     

    Good luck, and have fun!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Hi Thomas,

     

    I just installed the new Python3 version of pifacedigitalio following the directions on github: https://github.com/piface/pifacedigitalio. I'm using the latest version of Raspbian (2013-02-09) with all of the latest updates installed (via apt) and the latest firmware (via hexxeh's rpi-update script).

     

    For some reason, my system is not setting up the permissions properly for the /dev/spidev* files. Output of 'ls -al /dev/spi*' is below:

     

    pi@raspberrypi ~ $ sudo ls -al /dev/spi*

    crw------- 1 root root 153, 0 Dec 31  1969 /dev/spidev0.0

    crw------- 1 root root 153, 1 Dec 31  1969 /dev/spidev0.1

     

    I'm getting ready to just add manual udev rules to set the permissions, but I wanted to check as to why they aren't being setup automatically. Does the new Python3 version of the Piface Python IO library setup not handle permission setup yet?

     

    Thanks,

    Andy

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Ah, so I haven't! I'll add this to the install script tomorrow, it must have slipped my mind since I was already working on a machine that had the permisions set up.

     

    For now, try running the spidev-setup script here.

     

    Thanks for the heads-up!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Yea, I just manully ran the old script and got it working. Thanks of the confirmation. With that sorted out, both the io library and emulater seem to be working properly.

     

    -Andy

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    I've updated the pifacedigitalio install script to update the spi permissions. Everything should work now, I might also add auto un-blacklisting the spi kernel module later.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Hi Thomas, I'm new to R-Pi and Pi-Face. I thus far have everything working quite well with your pifacedigitalio; but have an issue on the interrupts. Once I have called wait_for_input with loop=True I would like to be able to exit gracefully from the interrupt routine. Currently I try to set loop=false with one of the inputs but that does not work (I think for obvious reasons). Any help on how I can exit gracefully after receiving the interrupt I need?

     

    Thank you

    Sven

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Hi Sven,

    Currently the interrupt handler only supports looping forever or exiting after one interrupt. It should also handle a keyboard interrupt gracefully (Ctrl+C).

     

    For some reason I never thought of the use-case where you might want to exit the loop only from a certain interrupt. I've updated the code so that instead of using a loop variable to determine whether the loop should continue waiting for inputs, it decides based on the return value of the callback. If a callback returns True, wait_for_input keeps waiting for interrupts. If False, wait_for_input should return.

     

    I've updated this in a new branch called dev_interrupt_return but I haven't tested it yet (I'm in the middle of exams, I can test later in the week). The branch is here if you want to test the new version for me. Inspect the README for new interrupt instructions.

     

    How are you finding the interrupts on pifacedigitalio by the way? I tried to make it as simple as possible but I've not had much feedback! In particular, how is the spartan README? I was going for brief, but informative.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Hi Thomas,

     

    Firstly, apologies for disturbing your exams. I will most certainly test the new branch. At the moment the interrupts are doing the job I need them to do and when I hit input [1] I have simply put in a rather crude sys.exit(). It works for now. I kind of like the readme, it forces you to think about the situation.

     

    Interestingly, the solution you proposed with the boolean return from the callback is exactly what I tried but I could not quite get it to work.

     

    Thanks for your quick response, I'll let you know how it goes.

     

    Cheers

    Sven

     

    Edit:

    I got it working. I had to make some small changes to your code, I added the following in call_mapped_input_functions():

     

    if int_bit == 0:

        keep_waiting = True

        continue

     

    and I also added the following at the end of the function:

    return keep_waiting.

     

    These may not be the most elegant solutions but for now it is working. Thanks again for your help.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Sven, I never saw your edit before I updated the code. No worries, I've done a similar fix. It should work now.

     

    I've slightly changed the naming of things too: instead of 'into' I'm now using 'direction' because it's clearer. This also uses predefined direction variables: IN_EVENT_DIR_ON, IN_EVENT_DIR_OFF and IN_EVENT_DIR_BOTH.

     

    Check out the new instructions.

     

    Hope that helps.