Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum PiFace Problems
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 78 replies
  • Subscribers 717 subscribers
  • Views 12329 views
  • Users 0 members are here
  • raspberry_pi
  • piface
  • raspberry_pi_accessories
Related

PiFace Problems

keithtowns
keithtowns over 13 years ago

Am I missing something? I have two PiFace and 3 Raspberry Pi. I followed the instructions the get the PiFace working but have yet to succeed. I have tried the image provided as well as updating an existing Raspian image to no avail. I have also tried all my Pi and the two PiFace in all the combinations. I almost gave up but also tried a different power supply and SD card. None of the above got the emulator to switch on the LEDs and I could not do it through Python. Any ideas? I've spent hours on this, please tell me I've missed something. Thanks.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    Keith, you are not alone. The 'documentation' with the piface is worse than useless. I particularly like the typo on page 2 of the 'instructions' (etc/ which should be /etc/) and that if the emulator fails (I can't get it to work – ends with 'segmentation fault') the 'instructions' that follow are, again, useless. I will get it working in the end, but no thanks to the fools at man.ac.uk. How difficult would it have been to provide basic instructions in the box? Good luck with it - I'll reply back when I've finished arm-wrestling with it and got it doing something (I have a job in mind).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    ... not sure if urls are allowed here - if they are, here's some documentation for piface ...

     

    https://docs.google.com/folder/d/0B-UAZ9CyJCLGQjJ3RDlqa2pqaDg/edit?pli=1

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Sven, I never saw your edit before I updated the code. No worries, I've done a similar fix. It should work now.

     

    I've slightly changed the naming of things too: instead of 'into' I'm now using 'direction' because it's clearer. This also uses predefined direction variables: IN_EVENT_DIR_ON, IN_EVENT_DIR_OFF and IN_EVENT_DIR_BOTH.

     

    Check out the new instructions.

     

    Hope that helps.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • ogii
    ogii over 13 years ago in reply to keithtowns

    Hi, can I join the queue of disgruntled piface buyers (note not users) that has spent far too long trying to decode how to get this as yet useless board working?

     

    I've updated as per previous posts.

     

    My error message in response to an lxterminal command of piface/scripts/piface-emulator is

     

    Bash ........emulator: input output error.

     

    Any ideas please?

     

    Like previous poster the piface was bought to help a 10 year old interact with a model railway set up.

     

    At this moment I think rather than being customer ready this is more a geeks experiment that should not have reached production yet until all aspects of the set up instructions had been tested.

     

    It's certainly failing the sales of goods act at the moment.....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to ogii

    Are you using the most up to date software. We've moved over to Python 3, now. You can get it from https://github.com/piface

     

    > Bash ........emulator: input output error.

     

    That looks like an error with bash and not the emulator. I can't seem to replicate your problem and my Python 2 emulator works when I issue the commands:

     

    $ git clone https://github.com/thomasmacpherson/piface.git

    $ cd piface/python/

    $ sudo python setup.py install

    $ cd ../scripts/

    $ ./piface-emulator

     

    Can describe how you reach your problem in more detail, please?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 13 years ago in reply to e14 Contributor

    Thomas

    If you want a better image showing the default jumpers you can use my picture.

    http://www.element14.com/community/roadTestReviews/1452

    If you want the fullsized image, PM me with your email.

     

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Hello Thomas,
    I have the PiFace 2.1 with the latest version of pifacecommon and pifacedigitalio on the last raspbian running. Control of IO is not a problem. But the interrupts do not work with python. The sample code, for example, shows no function. But the interrupts works fine withe the Java lib Pi4J. Do you have any idea what could go wrong?

    best greetings Andreas

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    Hi, sorry for the delayed reply, I've been on holiday!

     

    Are you using the example code from here: http://piface.github.io/pifacedigitalio/example.html#interrupts? Did you reboot after installing? Can you show me the code you are trying to use?

     

    Pi4J is a Java library for accessing the GPIO pins, not PiFace (to my knowledge at least).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    Hey Thomas,
    thanks for your answer. I have reinstalled the distribution. I try the / usr/share/doch/python3-pifacedigitalio/examples/presslights.py program and also the example code on the webpage (ure link). Nothing works. But simple polling on a button works fine. So buttons and leds are working...

    To Pi4J, "With the Pi-Face Java API interface now available in the libraries Pi4J (Pi4J in version 0.0.5-SNAPSHOT and later)" Source: http://www.savagehomeautomation.com/projects/raspberry-pi-programming -pi-face-with-java-pi4j.html
    The API package comes with two examples for the piface PiFaceExample.java and PiFaceGpioExample.java. I compile and run the PiFaceExample
    (it use listener (interrupts)) and it ran as it should, so I think that the interrupts generally works?!

     

    I hope you have another ideas image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    That's great news about Java support for PiFace!

     

    Are you running the latest versions of the Python modules? Can you show me the output of the following commands:

     

    $ python3 -c "import pifacedigitalio.version as p; print(p.__version__)"

    $ python3 -c "import pifacecommon.version as p; print(p.__version__)"

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    Python3: 3.2.3 (Mar 1) GCC 4.6.3

    PiFacedigitalio: 2.0.3

    PiFaceCommon: 3.0.0

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    How about the outputs from the following commands:

     

    groups

    lsmod

    cat /etc/modprobe.d/raspi-blacklist.conf

    cat /lib/udev/rules.d/60-python3-pifacecommon.rules

     

    I can't seem to replicate the issue I'm afraid.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    How about the outputs from the following commands:

     

    groups

    lsmod

    cat /etc/modprobe.d/raspi-blacklist.conf

    cat /lib/udev/rules.d/60-python3-pifacecommon.rules

     

    I can't seem to replicate the issue I'm afraid.