Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum What would be the total GPIO pins available.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 711 subscribers
  • Views 2026 views
  • Users 0 members are here
  • raspberrypi
  • gpio_configuration
Related

What would be the total GPIO pins available.

finian826
finian826 over 13 years ago

Good day,

I am thinking of employing 1 or 2 Rpi's into my model train layout to remote manage my turnouts and other specialty items on my layout.

I know through GPIO-P1 I have 17 available GPIO pins. From some of my other reading I have discovered on the new model B's there was a P5 added that gives 4 more GPIO pins for usage, but it also says in the same document that those pins are used by the system. The available pins on P5 are GPIO28-GPIO31, but those are used as follows: GPIO28-31 are used by the board ID and are connected to resistors R3 to R10.

 

I know that some are also avabile via S5 which from my understanding will eventually be used for the upcoming camera board.

 

So if I read correctly, theorietically I could have 25 possible GPIO pins available or would it only be 21 if I take and use the 4 from S5.

 

Any input on this from others would be great.

 

Thanks

Terry

  • Sign in to reply
  • Cancel
Parents
  • guzunty
    guzunty over 13 years ago

    If you're looking to maximise your IO, please check out the board I designed:

     

    https://github.com/Guzunty/Pi/wiki

     

    The standard configuration offers up to 25 IO pins using only four of the Pi GPIO pins via the Pi SPI interface. It can be configured to provide a few more without much work and the other Pi pins can still be used for still more I/O if need be.

     

    You can also program it to use up to 8 of the outputs as zero CPU load pulse width modulated, which may be useful in a model railway configuration. PWM does require one additional Pi GPIO pin to provide a clock.

     

    It is also very easy on the budget, only £3.20 for the bare PCB. Total parts cost is under a tenner.

     

    Perhaps the best bit is that it protects your Pi GPIO from the higher voltages that are present in a model railway layout. If you should make a mistake and allow damaging voltages onto this board, the CPLD at the heart of it is socketed and can be replaced for less than £3.

     

    This board doesn't provide high current drives, but I'm assuming as a model railway enthusiast you'll have the downstream high current stuff already.

     

    HTH,

     

    DC.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bad_boy_y
    bad_boy_y over 13 years ago in reply to guzunty

    You can add lot of I/O whit arduino like Due see the roadtest.

    http://www.element14.com/community/roadTests/1144

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • bad_boy_y
    bad_boy_y over 13 years ago in reply to guzunty

    You can add lot of I/O whit arduino like Due see the roadtest.

    http://www.element14.com/community/roadTests/1144

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • guzunty
    guzunty over 13 years ago in reply to bad_boy_y

    Looks pretty good depending on its price. When is it going to be available though?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bad_boy_y
    bad_boy_y over 13 years ago in reply to guzunty

    Derek

     

    for the arduino due realy cheap see the link (not the green guy on Zelda)

     

    http://www.newark.com/arduino/a000062/eval-board-arduino-due/dp/47W2961