Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi + Webcam + Python + OpenCV = Weird Problems + No Solutions
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 705 subscribers
  • Views 2367 views
  • Users 0 members are here
  • raspberry_pi
Related

Raspberry Pi + Webcam + Python + OpenCV = Weird Problems + No Solutions

e14 Contributor
e14 Contributor over 13 years ago

Now,

 

EDIT: Main goal, capture an image, wait some time, capture another image, add the two images together and show it :END EDIT

 

I run the program and can see the webcam feed, I then press a key capturing an image as img1, then again but as img2, and again img3. Now when the final image displays (img2+img3) it just shows img3 added to itself, i.e. as though I coded Add(img3,img3,img1). I have also tried AddWeighted and AND functions.

 

I have tried and tried and cannot find the problem, is it the Add function that is not reading img2, or could img2 not be saved properly? or what is going on!!

 

Any help would be great,

 

Cheers,

 

Dan.

 

 

# Daniel Myers
# cvTest.py
# 18 Feb 13

 

from cv import *

 

SIZE=(HEIGHT,WIDTH)=(640,480) # Image capture size
CAMERA_INDEX=-1 # -1 means any camera attached

 

def TakePic(cam):
    NamedWindow('cvTest',CV_WINDOW_AUTOSIZE)
    while True:
        img=QueryFrame(cam)
        ShowImage('cvTest',img)
        k=WaitKey(2)
        if k>=0:
            return img

 

cam=CaptureFromCAM(CAMERA_INDEX) # Initializes capturing a video from a camera
SetCaptureProperty(cam,CV_CAP_PROP_FRAME_WIDTH,WIDTH) # Set the capture image width
SetCaptureProperty(cam,CV_CAP_PROP_FRAME_HEIGHT,HEIGHT) # Set the capture image height

 

img1=TakePic(cam)
ShowImage('img1',img1)

 

img2=TakePic(cam)
ShowImage('img2',img2)

 

img3=TakePic(cam)
ShowImage('img3',img3)

 

AddWeighted(img2,0.4,img3,0.6,20,img1)
ShowImage('img2+img3',img1)

 

k=WaitKey(100000)
DestroyAllWindows()
del(cam)

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago

    Update,

     

    Had a stroke of genius, I changed the end of the code to be as follows:

     

    img3=TakePic(cam)
    ShowImage('img3',img3)

     

    #AddWeighted(img2,0.4,img3,0.6,20,img1)
    ShowImage('img1 again',img1)

     

    k=WaitKey(100000)
    DestroyAllWindows()
    del(cam)

     

    So now it doesnt do the AddWeighted, it is just meant to show img1 again, however when I run this it shows img3, so for some unknow reason you can only ever access the last image created... (unless someone thinks otherwise)

     

    Anyone have any idea how to get around this?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago

    Wrote two functions (below). I capture an image, convert to mat, capture an image, convert to mat, add the two mats, convert to image and show..... now this works, it shows overlapped images however this is awful coding and terribly slow, but proves the Add function works, and the theory is there there is jsut something wrong with the IplImage's

     

    def Img2Mat(img):
         width=img.width
         height=img.height
         depth=img.depth
         mat=CreateMat(height,width,depth)
         for w in range(0,width):
              for h in range(0,height):
                   value=Get2D(img,h,w)
                   Set2D(mat,h,w,value)

         return mat

    def Mat2Img(mat):
         width=mat.cols
         height=mat.rows
         size=(width,height)
         img=CreateImage(size,8,3)
         for w in range(0,width):
               for h in range(0,height):
                    value=Get2D(mat,h,w)
                    Set2D(img,h,w,value)
         return img

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Daniel,

      I think your assignments to img1, img2, and img3 are just copying pointers,

    not the full images, so all the pointers end up pointing to the last image taken

    by TakePic. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Ah I thought I had escaped the clutches of Pointers moving from C to Python, but then python openCV is C underneath yeah?

     

    Anyway I'll try looking into making sure everything is pointing in the right direction tomorrow.

     

    Thanks heaps for your help.

     

    Dan.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Guido explains here:

     

    http://www.python.org/doc/essays/ppt/acm-ws/sld039.htm

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    coder27 you legend, you have fixed all my problem and I wish to send you flowers.... or maybe thanks is just enough?

     

    Here is the easy fix,

     

    cam=CaptureFromCAM(-1)

     

    img=QueryFrame(cam)

    img1=CloneImage(img)

     

    img=QueryFrame(cam)

    img2=CloneImage(img)

     

    img=Add(img1,img2,img)

    img3=CloneImage(img)

     

    Cheers everyone,

     

    Dan.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    hello Dan

     

    we write python code

     

    import improc

     

    from improc import*

     

    camera= Camera (320,240)

    viewer = Viewer (640,480,"pic.")

    img= camera.grabImage()

     

    viewer.displayImage (img)

     

    for x in range  (0, img.width) :

     

               for y in range(0, img.height) :

        

                          red, green, blue = img [x, y]

     

    if red > green  and  red >blue :

     

       img [x, y]  = 255, 0, 0

     

    elif green > red and green > blue :

     

    img[x, y] =0, 255, 0

     

    else

     

    img[x, y] = 0, 0, 255

     

    viewer.displayImage (img)

     

    waitTime (1000)

     

     

    we take the image  viewer,but we want to  save image on raspberry pi

     

    how can i do this ? what does it comment ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Hi osman,

     

    Sorry but I'm not familar with the python package improc. Is it a standard package or did you create it? I'm assuming you want to save "img" as a JPEG, PNG or other format?

     

    I could do this in openCV but not sure about improc sorry.

     

    I would use:

     

    #Start Example 1

     

    from cv import *

     

    #All your capture and image processing here

     

    SaveImage("img.png",img)

     

    #End Example 1

     

     

    This will work using PIL, if you don't have the Python Image Library, use the command:

     

         sudo apt-get install python-imaging

     

    Or if you have PIP:

     

        sudo pip install PIL

     

    Anyway here is the code

     

    #Start Example 2

     

    import improc

    from improc import *

    from PIL import Image #Importing the PIL package

     

    camera=Camera(320,240)

    viewer=Viewer(640,480,"pic.")

    img=camera.grabImage()

     

    viewer.displayImage(img)

     

    img2=Image.new('RGB',(320,240),(0,0,0)) #Creates a blank PIL Image

    pixels=img2.load() #Create the pixel map

     

    for x in range (0,img.width):

        for y in range(0,img.height):

            red,green,blue=img [x, y]

            if red>green and red>blue:

                img[x,y]=(255,0,0)

                pixels[x,y]=(255,0,0)

            elif green>red and green>blue:

                img[x,y]=(0,255,0)

                pixels[x,y]=(0,255,0)

            else

                img[x,y]=(0,0,255)

                pixels[x,y]=(0,0,255)

     

    viewer.displayImage(img)

     

    waitTime(1000)

     

    img2.save('img2.png') #Save the img as a PNG file

     

    #End Example 2

     

    Note I just change the pixels variable, I am pretty sure that pixels points to the pixel values of img2 therefore if you change pixels, img2 changes.

     

    Any issues let me know

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Daniel thanks for codes

     

    but i want to know how can i compile this code and runn i could not find these thinks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Hi Osman,

     

    I still don't know what the improc libaray is so wouldnt be able to say how to compile or run.

     

     

     

    Assuming you don't have OpenCV which is what I use to do my image processing on the Raspberry Pi in Python, you can follow my steps below (but it takes 5 hours)

     

    or there is this guide which I haven't done before

    http://www.technolabsz.com/2013/03/how-to-easily-install-opencv-on.html

     

     

    Once that is installed you can use this code:

     

    #START EXAMPLE CODE

    from cv import *

     

    SIZE=(HEIGHT,WIDTH)=(320,240) # Image capture size
    CAMERA_INDEX=-1 # -1 means any camera attached

     

    cam=CaptureFromCAM(CAMERA_INDEX) # Initializes capturing a video from a camera

    SetCaptureProperty(cam,CV_CAP_PROP_FRAME_WIDTH,WIDTH) # Set the capture image width

    SetCaptureProperty(cam,CV_CAP_PROP_FRAME_HEIGHT,HEIGHT) # Set the capture image height


    NamedWindow('image_before',CV_WINDOW_AUTOSIZE) #Create the before window

    NamedWindow('image_after',CV_WINDOW_AUTOSIZE) #Create the after window

     

     

    img1=QueryFrame(cam) #capture the frame from the camera

    img2=CloneImage(img1) #Copy the image to be edited

     

    W,H=GetSize(img1)

     

    for x in range (0,W):

        for y in range(0,H):     

            red,green,blue=get2D(img1,x,y)

            if red>green and red>blue:

                Set2D(img2,x,y,(255,0,0) )

            elif green>red and green>blue:

                Set2D(img2,x,y,(0,255,0) )

            else

                Set2D(img2,x,y,(0,0,255) )

     

    SaveImage('img2.png',img2)

     

    ShowImage('image_before',img1) #Show before image

    ShowImage('image_after',img2) #Show after image

     

    k=WaitKey(100000) #keep the images up
    DestroyAllWindows() #clean up
    del(cam) #clean up
    #END EXAMPLE CODE

     

     

    Cheers,

     

    Dan.

     

     

     

     

     

     

     

     

     

    1 Install OpenCV for Python TAKES APPROX 5 HOURS!!!

     

      1.1 Install the dependant packages using the command:

     

              $sudo apt-get -y install build-essential cmake cmake-qt-gui pkg-config libpng12-0 libpng12-dev libpng++-dev libpng3 libpnglite-dev zlib1g-dbg zlib1g zlib1g-dev pngtools libtiff4-dev libtiff4 libtiffxx0c2 libtiff-tools

     

            and some more:

     

              $sudo apt-get -y install libjpeg8 libjpeg8-dev libjpeg8-dbg libjpeg-progs ffmpeg libavcodec-dev libavcodec53 libavformat53 libavformat-dev libgstreamer0.10-0-dbg libgstreamer0.10-0 libgstreamer0.10-dev libxine1-ffmpeg libxine-dev libxine1-bin libunicap2 libunicap2-dev libdc1394-22-dev libdc1394-22 libdc1394-utils swig libv4l-0 libv4l-dev python-numpy libpython2.6 python-dev python2.6-dev libgtk2.0-dev pkg-config

     

      1.2 Get the source for OpenCV using the command:

     

              $wget http://sourceforge.net/projects/opencvlibrary/files/opencv-unix/2.4.3/OpenCV-2.4.3.tar.bz2

     

      1.3 Extract the archive using the command:

     

              $tar -xvjpf OpenCV-2.4.3.tar.bz2

     

      1.4 Remove the file (space saving)using the command:

     

              $rm OpenCV-2.4.3.tar.bz2

     

      1.5 Open the directory using the command:

     

              $cd OpenCV-2.4.3

     

      1.6 Make a new directory using the command:

     

              $mkdir build

     

            and open it:

     

              $cd build

     

      1.7 Configure the build using the command:

     

              $cmake -D CMAKE_BUILD_TYPE=RELEASE -D CMAKE_INSTALL_PREFIX=/usr/local -D BUILD_PYTHON_SUPPORT=ON -D BUILD_EXAMPLES=ON ..

     

      1.8 Now install (TAKES 5 HOURS!!!! have a coffee) using the commands:

     

              $make

     

            and then:

     

              $sudo make install

     

      1.9 Open and configure the OpenCV files using the command:

     

              $sudo nano /etc/ld.so.conf.d/opencv.conf

     

            then add the following line to the end (fle may be empty, its all good):

     

              /usr/local/lib

     

      1.10 Open and edit the system bashrc file using the command:

     

               $sudo nano /etc/bash.bashrc

     

             and add to the end of the file these lines:

     

               PKG_CONFIG_PATH=$PKG_CONFIG_PATH:/usr/local/lib/pkgconfig export

               PKG_CONFIG_PATH

     

      1.11 Reference:

     

               http://mitchtech.net/raspberry-pi-opencv/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>