Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum RPi + GSM/3G module + SIM card
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 705 subscribers
  • Views 2820 views
  • Users 0 members are here
Related

RPi + GSM/3G module + SIM card

e14 Contributor
e14 Contributor over 13 years ago

Hello, everybody!

 

I am new to RaspberryPI, just got mine recently, and all I did was setup Raspbian and browse the web with it.

 

Now I plan on developing a GSM app, to be used along with a various number of applications (imagination is the limit).

However, I am not exactly tech-savvy in the "do it yourself" department, and I need some help.

 

I want to attach a SIM card to RPi.

The objective is to create a general purpose application which should do the following:

1. listen for incoming SMS text messages (which can contain application-specific commands)

2. parse the incoming commands and send some packets (XML/RPC requests) to some server (accessible by IP address in the same LAN, in a VPN or public IP address)

3. reply to sender with a templatable SMS text message.

 

I need to be pointed in the right direction, or any good direction, esecially related to:

1. attaching a SIM card to RaspberryPi.

I surfed the web, and the only solution I found was RPi with an Arduino board on top, and a GSM/3G module on top of that.

Is there a GSM/3G module out there, which can be directly attached to RPi? I prefer a module capable of operating in 850/900/1800/1900MHz and also 3G / WCDMA2100.

I could use not only advice, but also some links to where to buy the pieces from.

 

2. coding the application.

I can manage developing most of the application on my own, but I could use some assistance or tutorials on how to interact with the GSM module.

I don't like the idea of working with an Arduino in the middle, and I couldn't find any tutorials to match my requirements.

 

Any help is most welcome, as I may continue my research baed on your advice/links/tutorials.

 

Also, if somewhere in the great jungle we call internet, you know someone who might need such an application, I intend to make my application available for purchase.

So I am also open to investments, and develop this application under a shared licence agreement which can be discussed privately.

 

Best regards to all !

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    shabaz over 13 years ago

    SMS is really dated. An alternative method would be to use a 3G USB stick, and just use IP.

    If you're in an area with no 3G, then perhaps SMS is a better alternative.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to shabaz

    I agree with you, a 3G USB stick is definitely a cheaper solution, but it is not the object of my project.

    The 3G solution (which is actually basic networking) will be integrated anyway, for testing purposes, until the SMS module is complete.

     

    However, you can still add some value to your reply image

    Do you have any idea what hardware should I use for SMS ? Also, can you by any chance point to me any tutorials for SMS receiving/sending ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 13 years ago in reply to e14 Contributor

    I believe most GSM modules just rely on normal AT commands (perhaps an extension). For example, see here which

    explains the commands required to send an SMS for one device.

    Personally to me it just doesn't make sense these days - M2M is increasingly IP for good reason.

    You could try to find a module with a serial interface, and use that since the Raspberry Pi has a serial interface.

    You could check out something like this module (I did not read the datasheet).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 13 years ago in reply to e14 Contributor

    I believe most GSM modules just rely on normal AT commands (perhaps an extension). For example, see here which

    explains the commands required to send an SMS for one device.

    Personally to me it just doesn't make sense these days - M2M is increasingly IP for good reason.

    You could try to find a module with a serial interface, and use that since the Raspberry Pi has a serial interface.

    You could check out something like this module (I did not read the datasheet).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to shabaz

    Thank you very much.

     

    Although I was trying to avoid the Arduino, it may prove to be the easiet starting point for me, at least from the learning point of view.

    That Sierra module you shown me seems pretty capable, and it's probably worth those 60 pounds + VAT, since it looks like it does a bunch of useful things.

     

    To give you a hint about why I prefer SMS over IP / 3G wireless, the main reason is, as you partially pointed out, 3G coverage and 3G provider reliability. I could use the GoogleMarket over 3G, for example, but that's not exactly the purpose of my project. Another reason is the easy billing: my app is (hopefully image ) ment to be used by a paying user, and I can't assume he is smart or that has a smartphone. So a contract with a phone company solves the problem of receiving payments for micro-transactions via SMS (although their cut of my profit would be rather big).

     

    Anyway... thanks for the advice, I hope I can put it to good use soon image

    Best regards!

     

    PS: I am still open to suggestions from other users, maybe there are also other solutions to chose from.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 13 years ago in reply to e14 Contributor

    To be honest, even with no 3G, GPRS may be a better option. SMS should be absolute last case (at least for M2M). I suppose it does depend on billing options etc but I'm no expert on that unfortunately :-(