Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum RPi + GSM/3G module + SIM card
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 705 subscribers
  • Views 2821 views
  • Users 0 members are here
Related

RPi + GSM/3G module + SIM card

e14 Contributor
e14 Contributor over 13 years ago

Hello, everybody!

 

I am new to RaspberryPI, just got mine recently, and all I did was setup Raspbian and browse the web with it.

 

Now I plan on developing a GSM app, to be used along with a various number of applications (imagination is the limit).

However, I am not exactly tech-savvy in the "do it yourself" department, and I need some help.

 

I want to attach a SIM card to RPi.

The objective is to create a general purpose application which should do the following:

1. listen for incoming SMS text messages (which can contain application-specific commands)

2. parse the incoming commands and send some packets (XML/RPC requests) to some server (accessible by IP address in the same LAN, in a VPN or public IP address)

3. reply to sender with a templatable SMS text message.

 

I need to be pointed in the right direction, or any good direction, esecially related to:

1. attaching a SIM card to RaspberryPi.

I surfed the web, and the only solution I found was RPi with an Arduino board on top, and a GSM/3G module on top of that.

Is there a GSM/3G module out there, which can be directly attached to RPi? I prefer a module capable of operating in 850/900/1800/1900MHz and also 3G / WCDMA2100.

I could use not only advice, but also some links to where to buy the pieces from.

 

2. coding the application.

I can manage developing most of the application on my own, but I could use some assistance or tutorials on how to interact with the GSM module.

I don't like the idea of working with an Arduino in the middle, and I couldn't find any tutorials to match my requirements.

 

Any help is most welcome, as I may continue my research baed on your advice/links/tutorials.

 

Also, if somewhere in the great jungle we call internet, you know someone who might need such an application, I intend to make my application available for purchase.

So I am also open to investments, and develop this application under a shared licence agreement which can be discussed privately.

 

Best regards to all !

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    Most 3g modems can do both gprs and sms.

    They indeed rely on the an extended AT command set.

    You can use an usb stick 3g modem or you can use one with a serial port like the Siemens TC35i

    The Pi is still having issues with usb 2 serial devices. It wouldn't suprise me that a 3g modem appears as such a device to the Pi.

    I am currently testing with a Huawei usb stick, and it's not working stable. The Pi reboots without any trail in the logfiles.

    The TP1 - TP2 voltage is 4.98V, so I assume that's not the problem. I will try a self powered hub to see if it works better with it.

    You can find the Siemens manual with the AT commands on the web.

    External 3g modems like that Siemens usually need an extra 12V supply. An usb 3g can work without it.

    Mine shows up as 3 serial ports and a cd rom device with the windows drivers. Some usb device wait for a command like an eject and only switch from cd rom mode to modem mode afterwards.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Hmmm...

    I didn't think of sending SMSs using a 3G dongle.

    Good idea, Luc Cool, thanks!

     

    I have 4 or 5 USB 3G sticks laying around (most of them Huawei and ZTE), and also an externally powered USB hub, so I guess I could try one out, especially since my 3G provider gives free SMSs between its subscribers image

     

    Still, I think I'd rather use a Pi-compatible GSM/3G module for its power consumption and stability.

    I don;t really trust these 3G dongles. I used 2 of them with a tablet, and with one of them the temperature of the tablet would rise pretty much after 1-2h, and with the other, the stick would heat up in about 30-45 min. So I don't want to chose this as a final solution just yet.

     

    I am still open to suggestions.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    I just figured out that the Pi was likely rebooting due to rf interference from the Huawei stick to the Pi.

    I placed an usb cable between the Pi and the stick so that I could locate the stick away from the Pi, and things started to work.

    I did solder a polyfuse over the one alrerady on the board. This increases the TP1 - TP2 voltage with 0.1 - 0.2V

    External modems like the Siemens, Wavecom and Telit ones use an external antenna. Their reception will likely be better due to that.

    They usually also sell OEM modules of their product range. Wathever solution you choose, the way to program them is very similar.

    There can be minor differences in the AT command set. Sending sms is pretty easy. Receiving them usually involves polling a number of reception slots to see if they contain a message.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    I just figured out that the Pi was likely rebooting due to rf interference from the Huawei stick to the Pi.

    I placed an usb cable between the Pi and the stick so that I could locate the stick away from the Pi, and things started to work.

    I did solder a polyfuse over the one alrerady on the board. This increases the TP1 - TP2 voltage with 0.1 - 0.2V

    External modems like the Siemens, Wavecom and Telit ones use an external antenna. Their reception will likely be better due to that.

    They usually also sell OEM modules of their product range. Wathever solution you choose, the way to program them is very similar.

    There can be minor differences in the AT command set. Sending sms is pretty easy. Receiving them usually involves polling a number of reception slots to see if they contain a message.