Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum RT3070 wireless adapter adjust tx power??
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 27 replies
  • Subscribers 709 subscribers
  • Views 8560 views
  • Users 0 members are here
Related

RT3070 wireless adapter adjust tx power??

wallarug
wallarug over 13 years ago

I seem to be unable to adjust the tx power above 20dbm.  I have tried: 'iwconfig wlan0 txpower 22' but this does not change the txpower.

 

I have also disabled the power-management.

 

The adapter claims that it can hit 5800mW of power which aquates to about 37dBm.

 

Does anyone know how I can get the txpower up? (I can put it down, just not up)

 

root@raspberrypi:~# lsusb

Bus 001 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub

Bus 001 Device 002: ID 0424:9512 Standard Microsystems Corp.

Bus 001 Device 003: ID 0424:ec00 Standard Microsystems Corp.

Bus 001 Device 004: ID 148f:3070 Ralink Technology, Corp. RT2870/RT3070 Wireless Adapter

root@raspberrypi:~# iwconfig wlan0 txpower 30

Error for wireless request "Set Tx Power" (8B26) :

    SET failed on device wlan0 ; Invalid argument.

root@raspberrypi:~#

  • Sign in to reply
  • Cancel
Parents
  • wallarug
    wallarug over 13 years ago

    adding to this, how can I tell if my card supports AP mode?  I tried iw list but this is what I got:

     

    root@CMDoverwatch:~# iw list

    Wiphy phy0

            Band 1:

                    Capabilities: 0x172

                            HT20/HT40

                            Static SM Power Save

                            RX Greenfield

                            RX HT20 SGI

                            RX HT40 SGI

                            RX STBC 1-stream

                            Max AMSDU length: 3839 bytes

                            No DSSS/CCK HT40

                    Maximum RX AMPDU length 65535 bytes (exponent: 0x003)

                    Minimum RX AMPDU time spacing: 2 usec (0x04)

                    HT RX MCS rate indexes supported: 0-7, 32

                    TX unequal modulation not supported

                    HT TX Max spatial streams: 1

                    HT TX MCS rate indexes supported may differ

                    Frequencies:

                            * 2412 MHz [1] (20.0 dBm)

                            * 2417 MHz [2] (20.0 dBm)

                            * 2422 MHz [3] (20.0 dBm)

                            * 2427 MHz [4] (20.0 dBm)

                            * 2432 MHz [5] (20.0 dBm)

                            * 2437 MHz [6] (20.0 dBm)

                            * 2442 MHz [7] (20.0 dBm)

                            * 2447 MHz [8] (20.0 dBm)

                            * 2452 MHz [9] (20.0 dBm)

                            * 2457 MHz [10] (20.0 dBm)

                            * 2462 MHz [11] (20.0 dBm)

                            * 2467 MHz [12] (20.0 dBm) (passive scanning, no IBSS)

                            * 2472 MHz [13] (20.0 dBm) (passive scanning, no IBSS)

                            * 2484 MHz [14] (20.0 dBm) (passive scanning, no IBSS)

                    Bitrates (non-HT):

                            * 1.0 Mbps

                            * 2.0 Mbps (short preamble supported)

                            * 5.5 Mbps (short preamble supported)

                            * 11.0 Mbps (short preamble supported)

                            * 6.0 Mbps

                            * 9.0 Mbps

                            * 12.0 Mbps

                            * 18.0 Mbps

                            * 24.0 Mbps

                            * 36.0 Mbps

                            * 48.0 Mbps

                            * 54.0 Mbps

            max # scan SSIDs: 4

            max scan IEs length: 2257 bytes

            Coverage class: 0 (up to 0m)

            Supported Ciphers:

                    * WEP40 (00-0f-ac:1)

                    * WEP104 (00-0f-ac:5)

                    * TKIP (00-0f-ac:2)

                    * CCMP (00-0f-ac:4)

            Available Antennas: TX 0 RX 0

            Supported interface modes:

                     * IBSS

                     * managed

                     * AP

                     * AP/VLAN

                     * WDS

                     * monitor

                     * mesh point

            software interface modes (can always be added):

                     * AP/VLAN

                     * monitor

            interface combinations are not supported

            Supported commands:

                     * new_interface

                     * set_interface

                     * new_key

                     * new_beacon

                     * new_station

                     * new_mpath

                     * set_mesh_params

                     * set_bss

                     * authenticate

                     * associate

                     * deauthenticate

                     * disassociate

                     * join_ibss

                     * join_mesh

                     * remain_on_channel

                     * set_tx_bitrate_mask

                     * action

                     * frame_wait_cancel

                     * set_wiphy_netns

                     * set_channel

                     * set_wds_peer

                     * connect

                     * disconnect

            Supported TX frame types:

                     * IBSS: 0x00 0x10 0x20 0x30 0x40 0x50 0x60 0x70 0x80 0x90 0xa0 0xb0 0xc0 0xd0 0xe0 0xf0

                     * managed: 0x00 0x10 0x20 0x30 0x40 0x50 0x60 0x70 0x80 0x90 0xa0 0xb0 0xc0 0xd0 0xe0 0xf0

                     * AP: 0x00 0x10 0x20 0x30 0x40 0x50 0x60 0x70 0x80 0x90 0xa0 0xb0 0xc0 0xd0 0xe0 0xf0

                     * AP/VLAN: 0x00 0x10 0x20 0x30 0x40 0x50 0x60 0x70 0x80 0x90 0xa0 0xb0 0xc0 0xd0 0xe0 0xf0

                     * mesh point: 0x00 0x10 0x20 0x30 0x40 0x50 0x60 0x70 0x80 0x90 0xa0 0xb0 0xc0 0xd0 0xe0 0xf0

                     * P2P-client: 0x00 0x10 0x20 0x30 0x40 0x50 0x60 0x70 0x80 0x90 0xa0 0xb0 0xc0 0xd0 0xe0 0xf0

                     * P2P-GO: 0x00 0x10 0x20 0x30 0x40 0x50 0x60 0x70 0x80 0x90 0xa0 0xb0 0xc0 0xd0 0xe0 0xf0

            Supported RX frame types:

                     * IBSS: 0xd0

                     * managed: 0x40 0xd0

                     * AP: 0x00 0x20 0x40 0xa0 0xb0 0xc0 0xd0

                     * AP/VLAN: 0x00 0x20 0x40 0xa0 0xb0 0xc0 0xd0

                     * mesh point: 0xb0 0xc0 0xd0

                     * P2P-client: 0x40 0xd0

                     * P2P-GO: 0x00 0x20 0x40 0xa0 0xb0 0xc0 0xd0

     

    Any ideas?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • wallarug
    wallarug over 13 years ago

    adding to this, how can I tell if my card supports AP mode?  I tried iw list but this is what I got:

     

    root@CMDoverwatch:~# iw list

    Wiphy phy0

            Band 1:

                    Capabilities: 0x172

                            HT20/HT40

                            Static SM Power Save

                            RX Greenfield

                            RX HT20 SGI

                            RX HT40 SGI

                            RX STBC 1-stream

                            Max AMSDU length: 3839 bytes

                            No DSSS/CCK HT40

                    Maximum RX AMPDU length 65535 bytes (exponent: 0x003)

                    Minimum RX AMPDU time spacing: 2 usec (0x04)

                    HT RX MCS rate indexes supported: 0-7, 32

                    TX unequal modulation not supported

                    HT TX Max spatial streams: 1

                    HT TX MCS rate indexes supported may differ

                    Frequencies:

                            * 2412 MHz [1] (20.0 dBm)

                            * 2417 MHz [2] (20.0 dBm)

                            * 2422 MHz [3] (20.0 dBm)

                            * 2427 MHz [4] (20.0 dBm)

                            * 2432 MHz [5] (20.0 dBm)

                            * 2437 MHz [6] (20.0 dBm)

                            * 2442 MHz [7] (20.0 dBm)

                            * 2447 MHz [8] (20.0 dBm)

                            * 2452 MHz [9] (20.0 dBm)

                            * 2457 MHz [10] (20.0 dBm)

                            * 2462 MHz [11] (20.0 dBm)

                            * 2467 MHz [12] (20.0 dBm) (passive scanning, no IBSS)

                            * 2472 MHz [13] (20.0 dBm) (passive scanning, no IBSS)

                            * 2484 MHz [14] (20.0 dBm) (passive scanning, no IBSS)

                    Bitrates (non-HT):

                            * 1.0 Mbps

                            * 2.0 Mbps (short preamble supported)

                            * 5.5 Mbps (short preamble supported)

                            * 11.0 Mbps (short preamble supported)

                            * 6.0 Mbps

                            * 9.0 Mbps

                            * 12.0 Mbps

                            * 18.0 Mbps

                            * 24.0 Mbps

                            * 36.0 Mbps

                            * 48.0 Mbps

                            * 54.0 Mbps

            max # scan SSIDs: 4

            max scan IEs length: 2257 bytes

            Coverage class: 0 (up to 0m)

            Supported Ciphers:

                    * WEP40 (00-0f-ac:1)

                    * WEP104 (00-0f-ac:5)

                    * TKIP (00-0f-ac:2)

                    * CCMP (00-0f-ac:4)

            Available Antennas: TX 0 RX 0

            Supported interface modes:

                     * IBSS

                     * managed

                     * AP

                     * AP/VLAN

                     * WDS

                     * monitor

                     * mesh point

            software interface modes (can always be added):

                     * AP/VLAN

                     * monitor

            interface combinations are not supported

            Supported commands:

                     * new_interface

                     * set_interface

                     * new_key

                     * new_beacon

                     * new_station

                     * new_mpath

                     * set_mesh_params

                     * set_bss

                     * authenticate

                     * associate

                     * deauthenticate

                     * disassociate

                     * join_ibss

                     * join_mesh

                     * remain_on_channel

                     * set_tx_bitrate_mask

                     * action

                     * frame_wait_cancel

                     * set_wiphy_netns

                     * set_channel

                     * set_wds_peer

                     * connect

                     * disconnect

            Supported TX frame types:

                     * IBSS: 0x00 0x10 0x20 0x30 0x40 0x50 0x60 0x70 0x80 0x90 0xa0 0xb0 0xc0 0xd0 0xe0 0xf0

                     * managed: 0x00 0x10 0x20 0x30 0x40 0x50 0x60 0x70 0x80 0x90 0xa0 0xb0 0xc0 0xd0 0xe0 0xf0

                     * AP: 0x00 0x10 0x20 0x30 0x40 0x50 0x60 0x70 0x80 0x90 0xa0 0xb0 0xc0 0xd0 0xe0 0xf0

                     * AP/VLAN: 0x00 0x10 0x20 0x30 0x40 0x50 0x60 0x70 0x80 0x90 0xa0 0xb0 0xc0 0xd0 0xe0 0xf0

                     * mesh point: 0x00 0x10 0x20 0x30 0x40 0x50 0x60 0x70 0x80 0x90 0xa0 0xb0 0xc0 0xd0 0xe0 0xf0

                     * P2P-client: 0x00 0x10 0x20 0x30 0x40 0x50 0x60 0x70 0x80 0x90 0xa0 0xb0 0xc0 0xd0 0xe0 0xf0

                     * P2P-GO: 0x00 0x10 0x20 0x30 0x40 0x50 0x60 0x70 0x80 0x90 0xa0 0xb0 0xc0 0xd0 0xe0 0xf0

            Supported RX frame types:

                     * IBSS: 0xd0

                     * managed: 0x40 0xd0

                     * AP: 0x00 0x20 0x40 0xa0 0xb0 0xc0 0xd0

                     * AP/VLAN: 0x00 0x20 0x40 0xa0 0xb0 0xc0 0xd0

                     * mesh point: 0xb0 0xc0 0xd0

                     * P2P-client: 0x40 0xd0

                     * P2P-GO: 0x00 0x20 0x40 0xa0 0xb0 0xc0 0xd0

     

    Any ideas?