Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Difficulties using NTP with a GPS + Raspberry Pi (HELP!)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 707 subscribers
  • Views 2854 views
  • Users 0 members are here
  • raspberry_pi
Related

Difficulties using NTP with a GPS + Raspberry Pi (HELP!)

vk3pb
vk3pb over 13 years ago

Hi all

 

I have been asking around for help on other forums with this problem but noone has come up with a solution thus far. I hope that someone out there can help.

 

I am trying to get my model B pi to work with a bu-353 GPS. I have achieved some success but I can't get ntp to automatically fetch the time on boot.

 

I followed the instructions here

 

http://blog.retep.org/2012/06/18/getting-gps-to-work-on-a-raspberry-pi/

 

but found that I needed to make a few modifications to get cgps working

 

Here's what I did

 

sudo apt-get install gpsd gpsd-clients python-gps

 

I then ran

 

sudo dpkg-reconfigure /etc/gpsd

 

to set gpsd to automatically boot. I added -n in the options but didn't put in  /dev/ttyUSB0 as the port but rather left it to automatically find the USB plug.

 

I then manually edited GPSD and added in

 

chmod a+rw /dev/ttyUSB0

 

The reason for these two tweaks is that the gps was not loading up properly and cgps -s just waited a few seconds and went back to the command line. The tweaks seem to have fixed that.

 

Now if I start my pi and then put in the comamnd line

 

cgps -s

 

I can see what the gps is seeing, location information sats etc all in text format. If I run xgps I can see a graphical version of this. This works every time although can take a coupel of seconds to get a fix.

 

So far so good.

 

Per the web page I now proceed to try and set up ntp

 

sudo apt-get install ntp

Installation is probably unnecessary as ntp is already installed.

 

Now I go to the /etc directory and sudo nano ntp.conf and add in the following lines

 

# gps ntp
server 127.127.28.0 minpoll 4
fudge  127.127.28.0 time1 0.183 refid NMEA
server 127.127.28.1 minpoll 4 prefer
fudge  127.127.28.1 refid PPS

 

and then type

 

sudo service ntp restart

 

Ntp restarts. cgps-s continues to work ok but my time does not update like it should. Although I can get a fix on satellites and can see the time in cgps it doesn;t get picked up by NTP like it should.

 

How can I get NTP to load up the time from satellites at boot properly with the above setup? I would be grateful for some help as I am a beginner at Linux and I think a lot of people out there would like to know how to set up a cheap gps like this with the Pi.

 

Thanking you

  

Peter

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    While most of what you've done looks ok-ish, you're really not going to want to use PPS with a USB device. The reason for this is that the PPS signal needs to be reasonably accurate otherwise ntp will mark it as a falseticker and ignore it as a time source. The original idea for PPS is that it comes in on DTR or another line on a real RS232 port, however your USB device isn't a 'real' anything, it's just emulating a serial port and USB has it's own latency issues making an emulated PPS signal not quite the same.. (forgetting for a moment that the RPi brings it's own usb issues)

     

    You may get better results by removing the two lines with 127.127.28.1 and only use the NEMA stream although you can't expect much accuracy this way.

     

    Another reason it may appear not to work is that ntp will take some time to sync with a particular source, possibly many minutes. With only NEMA data it'll be trying to sync with the start of the message, if that's subject to jitter it could take a lot longer.

     

    Also ntp will usually refuse to sync with a timesource that's more than 1000 seconds different from the local clock, so it may never sync.  As the RPi has no RTC then it's likely to be very much more than 1000 seconds out on boot, so in a situation like that you need something to read the stream from the gps and set the clock reasonably close, ntp can then handle getting you a more accurate sync assuming it's possible with a usb device.

     

    There are other ways to do this, you can use a gps that has a real rs232 interface and wire up a PPS signal to a gpio pin. The kernel has a pps-gpio driver that's suitable, but this may require a fair bit of knowledge of how to compile a kernel with appropriate platform (or devicetree) data to identify the gpio being used for pps.

     

    It really depends on what your goal is. Do you just want to set a date and reasonably close time on boot ?  Or do you want what ntp and PPS is really designed for, a clock with (potentially) microsecond or better accuracy to be used as an ntp server for other systems on your network ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago

    While most of what you've done looks ok-ish, you're really not going to want to use PPS with a USB device. The reason for this is that the PPS signal needs to be reasonably accurate otherwise ntp will mark it as a falseticker and ignore it as a time source. The original idea for PPS is that it comes in on DTR or another line on a real RS232 port, however your USB device isn't a 'real' anything, it's just emulating a serial port and USB has it's own latency issues making an emulated PPS signal not quite the same.. (forgetting for a moment that the RPi brings it's own usb issues)

     

    You may get better results by removing the two lines with 127.127.28.1 and only use the NEMA stream although you can't expect much accuracy this way.

     

    Another reason it may appear not to work is that ntp will take some time to sync with a particular source, possibly many minutes. With only NEMA data it'll be trying to sync with the start of the message, if that's subject to jitter it could take a lot longer.

     

    Also ntp will usually refuse to sync with a timesource that's more than 1000 seconds different from the local clock, so it may never sync.  As the RPi has no RTC then it's likely to be very much more than 1000 seconds out on boot, so in a situation like that you need something to read the stream from the gps and set the clock reasonably close, ntp can then handle getting you a more accurate sync assuming it's possible with a usb device.

     

    There are other ways to do this, you can use a gps that has a real rs232 interface and wire up a PPS signal to a gpio pin. The kernel has a pps-gpio driver that's suitable, but this may require a fair bit of knowledge of how to compile a kernel with appropriate platform (or devicetree) data to identify the gpio being used for pps.

     

    It really depends on what your goal is. Do you just want to set a date and reasonably close time on boot ?  Or do you want what ntp and PPS is really designed for, a clock with (potentially) microsecond or better accuracy to be used as an ntp server for other systems on your network ?